|
| class | Camera |
| | This class is the main interface with the camera and the SDK features, such as: video, depth, tracking, mapping, and more. More...
|
| |
| class | ZEDCommon |
| |
| struct | Matrix3x3 |
| | Holds a 3x3 matrix that can be marshaled between the wrapper and C# scripts. More...
|
| |
| struct | Resolution |
| | Holds a camera resolution as two pointers (for height and width) for easy passing back and forth to the ZED wrapper. More...
|
| |
| struct | Rect |
| | Rect structure to define a rectangle or a ROI in pixels Use to set ROI target for AEC/AGC More...
|
| |
| struct | CameraConfiguration |
| | Structure containing information about the camera sensor More...
|
| |
| struct | CameraInformation |
| | Structure containing information of a single camera (serial number, model, input type, etc.) More...
|
| |
| class | PositionalTrackingParameters |
| | Parameters for positional tracking initialization. More...
|
| |
| struct | Pose |
| | Pose structure with data on timing and validity in addition to position and rotation. More...
|
| |
| struct | ImuData |
| | Full IMU data structure. More...
|
| |
| struct | BarometerData |
| |
| struct | MagnetometerData |
| |
| struct | TemperatureSensorData |
| |
| struct | SensorsData |
| |
| struct | SensorParameters |
| | Structure containing information about a single sensor available in the current device More...
|
| |
| struct | SensorsConfiguration |
| | Structure containing information about all the sensors available in the current device More...
|
| |
| class | RuntimeParameters |
| | Runtime parameters used by the ZEDCamera.Grab() function, and its Camera::grab() counterpart in the SDK. More...
|
| |
| struct | CameraParameters |
| | Calibration information for an individual sensor on the ZED (left or right). More...
|
| |
| struct | CalibrationParameters |
| | Holds calibration information about the current ZED's hardware, including per-sensor calibration and offsets between the two sensors. More...
|
| |
| class | InitParameters |
| | Struct containing all parameters passed to the SDK when initializing the ZED. These parameters will be fixed for the whole execution life time of the camera. More...
|
| |
| struct | RecordingParameters |
| | Sets the recording parameters. More...
|
| |
| struct | StreamingParameters |
| | Sets the streaming parameters. More...
|
| |
| struct | DeviceProperties |
| | Device properties More...
|
| |
| struct | StreamingProperties |
| | Streaming device properties More...
|
| |
| struct | RecordingStatus |
| | Container for information about the current SVO recording process. More...
|
| |
| class | SpatialMappingParameters |
| | Sets the spatial mapping parameters. More...
|
| |
| class | Mesh |
| | A mesh contains the geometric (and optionally texture) data of the scene captured by spatial mapping. More...
|
| |
| class | FusedPointCloud |
| | A fused point cloud contains both geometric and color data of the scene captured by spatial mapping. More...
|
| |
| struct | Chunk |
| | Represents a sub-mesh, it contains local vertices and triangles. More...
|
| |
| struct | PlaneData |
| | Structure that defines a new plane, holding information directly from the ZED SDK. Data within is relative to the camera; More...
|
| |
| struct | BatchParameters |
| | sets batch trajectory parameters The default constructor sets all parameters to their default settings. Parameters can be user adjusted. More...
|
| |
| struct | AI_Model_status |
| | Contains AI model status. More...
|
| |
| struct | ObjectDetectionParameters |
| | Sets the object detection parameters. More...
|
| |
| struct | ObjectDetectionRuntimeParameters |
| | Sets the object detection runtime parameters. More...
|
| |
| struct | ObjectData |
| | Object data structure directly from the SDK. Represents a single object detection. More...
|
| |
| struct | CustomBoxObjectData |
| | Container to store the externally detected objects. The objects can be ingested using IngestCustomBoxObjects() function to extract 3D information and tracking over time. More...
|
| |
| struct | Objects |
| | Object Scene data directly from the ZED SDK. Represents all detections given during a single image frame. Contains the number of object in the scene and the objectData structure for each object. Since the data is transmitted from C++ to C#, the size of the structure must be constant. Therefore, there is a limitation of 200 (MAX_OBJECT constant) objects in the image. More...
|
| |
| class | ObjectsBatch |
| | Contains batched data of a detected object More...
|
| |
| struct | char2 |
| | Represents a 2D vector of uchars for use on both the CPU and GPU. More...
|
| |
| struct | char3 |
| | Represents a 3D vector of uchars for use on both the CPU and GPU. More...
|
| |
| struct | char4 |
| | Represents a 4D vector of uchars for use on both the CPU and GPU. More...
|
| |
| struct | float2 |
| | Represents a 2D vector of floats for use on both the CPU and GPU. More...
|
| |
| struct | float3 |
| | Represents a 3D vector of floats for use on both the CPU and GPU. More...
|
| |
| struct | float4 |
| | Represents a 4D vector of floats for use on both the CPU and GPU. More...
|
| |
| class | Mat |
| | Mirrors the sl::Mat class used in the ZED C++ SDK to store images. Can be used to retrieve individual images from GPU or CPU memory: see Camera.RetrieveImage() and Camera.RetrieveMeasure(). More...
|
| |
|
| enum class | Constant |
| | Constant for plugin. Should not be changed More...
|
| |
| enum class | ERROR_CODE |
| | List of error codes in the ZED SDK. More...
|
| |
| enum class | COORDINATE_SYSTEM |
| | List of available coordinate systems. More...
|
| |
| enum class | POSITIONAL_TRACKING_STATE |
| | Possible states of the ZED's Tracking system. More...
|
| |
| enum class | REFERENCE_FRAME |
| | Reference frame (world or camera) for tracking and depth sensing. More...
|
| |
| enum class | SENSOR_WORLD |
| | Defines the world type that the SDK can use to initialize the Positionnal Tracking module More...
|
| |
| enum class | TRACKING_FRAME |
| | Part of the ZED (left/right sensor, center) that's considered its center for tracking purposes. More...
|
| |
| enum class | HEADING_STATE |
| |
| enum class | SENSOR_TYPE |
| | List of the available onboard sensors More...
|
| |
| enum class | SENSORS_UNIT |
| | List of the available onboard sensors measurement units More...
|
| |
| enum class | DEPTH_MODE |
| | Lists available depth computation modes. Each mode offers better accuracy than the mode before it, but at a performance cost. More...
|
| |
| enum class | SENSING_MODE |
| | Lists available sensing modes - whether to produce the original depth map (STANDARD) or one with smoothing and other effects added to fill gaps and roughness (FILL). More...
|
| |
| enum class | MEASURE |
| | Lists available measure types retrieved from the camera, used for creating precise measurement maps (Measure-type textures). Based on the MEASURE enum in the ZED C++ SDK. For more info, see: https://www.stereolabs.com/docs/api_3.X/group__Depth__group.html#ga798a8eed10c573d759ef7e5a5bcd545d More...
|
| |
| enum class | INPUT_TYPE |
| | Lists available input type in SDK. More...
|
| |
| enum class | CAMERA_STATE |
| | List of possible camera state More...
|
| |
| enum class | RESOLUTION |
| | Represents the available resolution options. More...
|
| |
| enum class | FLIP_MODE |
| | brief Lists available compression modes for SVO recording. More...
|
| |
| enum class | MODEL |
| | Types of compatible ZED cameras. More...
|
| |
| enum class | VIEW |
| | Lists available view types retrieved from the camera, used for creating human-viewable (Image-type) textures. More...
|
| |
| enum class | VIDEO_SETTINGS |
| | Lists available camera settings for the ZED camera (contrast, hue, saturation, gain, etc.) More...
|
| |
| enum class | TIME_REFERENCE |
| | Categories indicating when a timestamp is captured. More...
|
| |
| enum class | SVO_COMPRESSION_MODE |
| | SVO compression modes. More...
|
| |
| enum class | STREAMING_CODEC |
| | Streaming codecs More...
|
| |
| enum class | SIDE |
| | defines left,right,both to distinguish between left and right or both sides More...
|
| |
| enum class | MAPPING_RESOLUTION |
| | Spatial mapping depth resolution presets. More...
|
| |
| enum class | MAPPING_RANGE |
| | Spatial mapping depth range presets. More...
|
| |
| enum class | SPATIAL_MAP_TYPE |
| | Spatial Mapping type (default is mesh) More...
|
| |
| enum class | MESH_FILE_FORMAT |
| | Mesh formats that can be saved/loaded with spatial mapping. More...
|
| |
| enum class | MESH_FILTER |
| | Presets for filtering meshes scannedw ith spatial mapping. Higher values reduce total face count by more. More...
|
| |
| enum class | SPATIAL_MAPPING_STATE |
| | Possible states of the ZED's Spatial Mapping system. More...
|
| |
| enum class | UNIT |
| | Units used by the SDK for measurements and tracking. More...
|
| |
| enum class | PLANE_TYPE |
| | Type of the plane, determined by its orientation and whether detected by ZEDPlaneDetectionManager's DetectFloorPlane() or DetectPlaneAtHit(). More...
|
| |
| enum class | AREA_EXPORT_STATE |
| | Possible states of the ZED's spatial memory area export, for saving 3D features used by the tracking system to relocalize the camera. This is used when saving a mesh generated by spatial mapping when Save Mesh is enabled - a .area file is saved as well. More...
|
| |
| enum class | BODY_FORMAT |
| | Lists of supported skeleton body model More...
|
| |
| enum class | OBJECT_CLASS |
| | Lists available object class More...
|
| |
| enum class | OBJECT_SUBCLASS |
| | Lists available object subclass. More...
|
| |
| enum class | OBJECT_TRACKING_STATE |
| | Tracking state of an individual object. More...
|
| |
| enum class | OBJECT_ACTION_STATE |
| | Lists available object action state. More...
|
| |
| enum class | DETECTION_MODEL |
| | List available models for detection More...
|
| |
| enum class | AI_MODELS |
| |
| enum class | OBJECT_FILTERING_MODE |
| | Lists of supported bounding box preprocessing More...
|
| |
| enum class | BODY_PARTS |
| | semantic and order of human body keypoints. More...
|
| |
| enum class | BODY_PARTS_POSE_34 |
| | ssemantic of human body parts and order keypoints for BODY_FORMAT.POSE_34. More...
|
| |
| enum class | MAT_TYPE |
| | Type of mat, indicating the data type and the number of channels it holds. Proper mat type depends on the image type. See sl.VIEW and sl.MEASURE (in ZEDCommon.cs) More...
|
| |
| enum class | COPY_TYPE |
| | Categories for copying data within or between the CPU (processor) memory and GPU (graphics card) memory. More...
|
| |
| enum class | MEM |
| | Which memory to store an image/mat: CPU/processor memory or GPU (graphics card) memory. More...
|
| |