Classes | |
class | PositionalTrackingParameters |
Parameters for positional tracking initialization. More... | |
struct | Pose |
Pose structure with data on timing and validity in addition to position and rotation. More... | |
Enumerations | |
enum class | POSITIONAL_TRACKING_STATE |
Possible states of the ZED's Tracking system. More... | |
enum class | REFERENCE_FRAME |
Reference frame (world or camera) for tracking and depth sensing. More... | |
enum class | TRACKING_FRAME |
Part of the ZED (left/right sensor, center) that's considered its center for tracking purposes. More... | |
|
strong |
Possible states of the ZED's Tracking system.
Enumerator | |
---|---|
SEARCHING | Tracking is searching for a match from the database to relocate to a previously known position. |
OK | Tracking is operating normally; tracking data should be correct. |
OFF | Tracking is not enabled. |
FPS_TOO_LOW | Effective FPS is too low to give proper results for motion tracking. Consider using PERFORMANCES parameters (DEPTH_MODE_PERFORMANCE, low camera resolution (VGA, HD720)) |
SEARCHING_FLOOR_PLANE | The camera is searching for the floor plane to locate itself related to it, the REFERENCE_FRAME.WORLD will be set afterward. |
|
strong |
|
strong |