sl Namespace Reference

Classes

class  Camera
 This class serves as the primary interface between the camera and the various features provided by the SDK. More...
 
class  ZEDCommon
 
struct  Matrix3x3
 Structure representing a generic 3*3 matrix. More...
 
struct  Resolution
 Structure containing the width and height of an image. More...
 
struct  Rect
 Structure defining a 2D rectangle with top-left corner coordinates and width/height in pixels. More...
 
struct  CameraConfiguration
 Structure containing information about the camera sensor. More...
 
struct  CameraInformation
 Structure containing information of a single camera (serial number, model, input type, etc.) More...
 
class  PositionalTrackingParameters
 Class containing a set of parameters for the positional tracking module initialization. More...
 
struct  Pose
 Structure containing positional tracking data giving the position and orientation of the camera in 3D space. More...
 
struct  RegionOfInterestParameters
 Structure containing a set of parameters for the region of interest. More...
 
struct  PositionalTrackingStatus
 Lists the different status of positional tracking. More...
 
struct  ImuData
 Structure containing data from the IMU sensor. More...
 
struct  BarometerData
 Structure containing data from the barometer sensor. More...
 
struct  MagnetometerData
 Structure containing data from the magnetometer sensor. More...
 
struct  TemperatureSensorData
 Structure containing data from the temperature sensors. More...
 
struct  SensorsData
 Structure containing all sensors data (except image sensors) to be used for positional tracking or environment study. More...
 
struct  SensorParameters
 Structure containing information about a single sensor available in the current device. More...
 
struct  SensorsConfiguration
 Structure containing information about all the sensors available in the current device. More...
 
class  RuntimeParameters
 Class containing parameters that defines the behavior of sl.Camera.Grab(). More...
 
struct  CameraParameters
 Structure containing the intrinsic parameters of a camera. More...
 
struct  CalibrationParameters
 Structure containing intrinsic and extrinsic parameters of the camera (translation and rotation). More...
 
struct  SVOData
 Structure containing data that can be stored in and retrieved from SVOs. That information will be ingested with sl.Camera.ingestDataIntoSVO and retrieved with sl.Camera.retrieveSVOData. More...
 
struct  VoxelMeasureParameters
 Parameters controlling voxel decimation in Camera.RetrieveVoxelMeasure. More...
 
class  InitParameters
 Class containing the options used to initialize the sl.Camera object. More...
 
struct  RecordingParameters
 Structure containing the options used to record. More...
 
struct  StreamingParameters
 Structure containing the options used to stream with the ZED SDK. More...
 
struct  DeviceProperties
 Structure containing information about the properties of a camera. More...
 
struct  StreamingProperties
 Structure containing information about the properties of a streaming device. More...
 
struct  HealthStatus
 Structure containing the self-diagnostic results of the camera (image, depth, sensor health). Retrieved via Camera.GetHealthStatus. More...
 
struct  RecordingStatus
 Structure containing information about the status of the recording. More...
 
struct  EncodedStreamPacket
 Single encoded video packet retrieved from a camera source. More...
 
struct  EncodedStreamInfo
 Describes one encoded video source exposed by the camera. More...
 
struct  InputType
 Structure defining the input type used in the ZED SDK. More...
 
class  PlaneDetectionParameters
 Class containing a set of parameters for the plane detection functionality. More...
 
class  SpatialMappingParameters
 Class containing a set of parameters for the spatial mapping module. More...
 
class  Mesh
 Class representing a mesh and containing the geometric (and optionally texture) data of the scene captured by the spatial mapping module. More...
 
class  FusedPointCloud
 A fused point cloud contains both geometric and color data of the scene captured by spatial mapping. More...
 
struct  Chunk
 Class representing a sub-mesh containing local vertices and triangles. More...
 
struct  PlaneData
 Structure representing a plane defined by a point and a normal, or a plane equation. More...
 
struct  BatchParameters
 Structure containing a set of parameters for batch object detection. More...
 
struct  AI_Model_status
 Structure containing AI model status. More...
 
struct  ObjectDetectionParameters
 Structure containing a set of parameters for the object detection module. More...
 
struct  ObjectTrackingParameters
 Structure containing a set of parameters for the object tracking module. More...
 
struct  ObjectDetectionRuntimeParameters
 Structure containing a set of runtime parameters for the object detection module. More...
 
struct  CustomObjectDetectionProperties
 Structure containing a set of runtime properties of a certain class ID for the object detection module using a custom model. More...
 
struct  CustomObjectDetectionRuntimeParameters
 
struct  BodyTrackingParameters
 Structure containing a set of parameters for the body tracking module. More...
 
struct  BodyTrackingRuntimeParameters
 Structure containing a set of runtime parameters for the body tracking module. More...
 
struct  ObjectData
 Structure containing data of a detected object such as its boundingBox, label, id and its 3D position. More...
 
struct  CustomBoxObjectData
 Structure that store externally detected objects. More...
 
struct  CustomMaskObjectData
 Structure that store external 2D mask. More...
 
struct  Objects
 Structure containing the results of the object detection module. It contains the number of object in the scene (numObject) and the objectData structure for each object. More...
 
struct  CovarMatrix
 Full covariance matrix for position (3x3). Only 6 values are necessary [p0, p1, p2] [p1, p3, p4] [p2, p4, p5] More...
 
struct  BodyData
 Structure containing data of a detected body/person such as its headBoundingBox, id and its 3D position. More...
 
struct  Bodies
 Structure containing the results of the body tracking module. More...
 
class  ObjectsBatch
 Class containing batched data of a detected objects from the object detection module. More...
 
struct  SynchronizationParameter
 Configuration parameters for data synchronization. More...
 
struct  InitFusionParameters
 Holds the options used to initialize the Fusion object. More...
 
struct  CommunicationParameters
 Holds the communication parameter to configure the connection between senders and receiver More...
 
struct  FusionConfiguration
 Stores the Fusion configuration, can be read from /write to a Json file. More...
 
struct  BodyTrackingFusionParameters
 Holds the options used to initialize the body tracking module of the Fusion. More...
 
struct  BodyTrackingFusionRuntimeParameters
 Holds the options used to change the behavior of the body tracking module at runtime. More...
 
struct  CameraIdentifier
 Used to identify a specific camera in the Fusion API More...
 
struct  CameraMetrics
 Holds the metrics of a sender in the fusion process. More...
 
struct  FusionMetrics
 Holds the metrics of the fusion process. More...
 
struct  FusedPositionalTrackingStatus
 Class containing the overall position fusion status More...
 
struct  Landmark
 Represents a 3d landmark. More...
 
struct  Landmark2D
 Represents a 2d landmark. More...
 
struct  GNSSData
 Structure containing GNSS data to be used for positional tracking as prior. More...
 
struct  GeoPose
 Holds Geo reference position. More...
 
struct  ECEF
 Represents a world position in ECEF format. More...
 
struct  ENU
 Represents a world position in ENU format. More...
 
struct  LatLng
 Represents a world position in LatLng format. More...
 
struct  UTM
 Represents a world position in UTM format. More...
 
class  GNSSCalibrationParameters
 Holds the options used for calibrating GNSS / VIO. More...
 
class  PositionalTrackingFusionParameters
 Holds the options used for initializing the positional tracking fusion module. More...
 
class  Fusion
 Holds Fusion process data and functions More...
 
struct  char2
 Represents a 2D vector of uchars for use on both the CPU and GPU. More...
 
struct  char3
 Represents a 3D vector of uchars for use on both the CPU and GPU. More...
 
struct  char4
 Represents a 4D vector of uchars for use on both the CPU and GPU. More...
 
struct  float2
 Represents a 2D vector of floats for use on both the CPU and GPU. More...
 
struct  float3
 Represents a 3D vector of floats for use on both the CPU and GPU. More...
 
struct  float4
 Represents a 4D vector of floats for use on both the CPU and GPU. More...
 
class  Mat
 Class representing 1 to 4-channel matrix of float or uchar, stored on CPU and/or GPU side. More...
 

Enumerations

enum class  Constant
 Constant for plugin. Should not be changed More...
 
enum class  POSITION_TYPE
 Lists the types of possible position outputs. More...
 
enum class  ERROR_CODE
 List of error codes in the ZED SDK. More...
 
enum class  COORDINATE_SYSTEM
 Lists available coordinates systems for positional tracking and 3D measures. More...
 
enum class  MODULE
 Lists available modules. More...
 
enum class  POSITIONAL_TRACKING_STATE
 Lists the different states of positional tracking. More...
 
enum class  ODOMETRY_STATUS
 Report the status of current odom tracking. More...
 
enum class  SPATIAL_MEMORY_STATUS
 Report the status of current map tracking. More...
 
enum class  POSITIONAL_TRACKING_FUSION_STATUS
 Report the status of the positional tracking fusion. More...
 
enum class  POSITIONAL_TRACKING_MODE
 Lists the mode of positional tracking that can be used. More...
 
enum class  COMPUTE_PREFERENCE
 Lists how much GPU a module is allowed to use. More...
 
enum class  REFERENCE_FRAME
 Lists possible types of position matrix used to store camera path and pose. More...
 
enum class  HEADING_STATE
 Lists the different states of the magnetic heading. More...
 
enum class  SENSOR_TYPE
 Lists available sensor types. More...
 
enum class  SENSORS_UNIT
 Lists available measurement units of onboard sensors. More...
 
enum class  DEPTH_MODE
 Lists available depth computation modes. More...
 
enum class  DEPTH_PRECISION
 Lists the precisions available for neural depth inference. More...
 
enum class  CUSTOM_DEPTH_FORMAT
 Lists the content type of the map ingested with Camera.IngestCustomDepth(). More...
 
enum class  CUSTOM_CONFIDENCE_CONVENTION
 Lists the value convention of the confidence map optionally ingested with Camera.IngestCustomDepth(). More...
 
enum class  MEASURE
 Lists retrievable measures. More...
 
enum class  VOXELIZATION_MODE
 Controls how voxel size adapts with depth. More...
 
enum class  REGION_OF_INTEREST_AUTO_DETECTION_STATE
 Lists the different states of region of interest auto detection. More...
 
enum class  INPUT_TYPE
 Lists available input types in the ZED SDK. More...
 
enum class  BUS_TYPE
 Lists available LIVE input type in the ZED SDK. More...
 
enum class  CAMERA_STATE
 Lists possible camera states. More...
 
enum class  RESOLUTION
 Lists available resolutions. More...
 
enum class  FLIP_MODE
 Lists possible flip modes of the camera. More...
 
enum class  MODEL
 Lists ZED camera model. SL_MODEL in C wrapper. More...
 
enum class  VIEW
 Lists available views. More...
 
enum class  VIDEO_SETTINGS
 Lists available camera settings for the camera (contrast, hue, saturation, gain, ...). More...
 
enum class  TIME_REFERENCE
 Lists possible time references for timestamps or data. More...
 
enum class  TIMESTAMP_CLOCK
 Lists available clock sources for SDK timestamps. More...
 
enum class  SVO_COMPRESSION_MODE
 Lists available compression modes for SVO recording. More...
 
enum class  SVO_ENCODING_PRESET
 Lists available encoding presets for SVO recording. Controls the speed/quality tradeoff of the GPU hardware encoder. More...
 
enum class  STREAMING_CODEC
 Lists the different encoding types for image streaming. More...
 
enum class  ENCODED_STREAM_SOURCE
 Identifies which of the camera's encoded video paths to read from. More...
 
enum class  SIDE
 Lists possible sides on which to get data from. More...
 
enum class  AREA_EXPORTING_STATE
 Lists the different states of spatial memory area export. More...
 
enum class  MAPPING_RESOLUTION
 Lists the spatial mapping resolution presets. More...
 
enum class  MAPPING_RANGE
 Lists the spatial mapping depth range presets. More...
 
enum class  SPATIAL_MAP_TYPE
 Lists the types of spatial maps that can be created. More...
 
enum class  MESH_FILE_FORMAT
 Lists available mesh file formats. More...
 
enum class  MESH_FILTER
 Lists available mesh filtering intensities. More...
 
enum class  SPATIAL_MAPPING_STATE
 Lists the different states of spatial mapping. More...
 
enum class  UNIT
 Lists available units for measures. More...
 
enum class  LENS_DISTORTION_MODEL
 Lists the lens distortion models used to describe a camera's optics. More...
 
enum class  PLANE_TYPE
 Lists the available plane types detected based on its orientation and whether detected by sl.Camera.FindFloorPlane() or sl.Camera.FindPlaneAtHit(). More...
 
enum class  AREA_EXPORT_STATE
 Possible states of the ZED's spatial memory area export, for saving 3D features used by the tracking system to relocalize the camera. This is used when saving a mesh generated by spatial mapping when Save Mesh is enabled - a .area file is saved as well. More...
 
enum class  BODY_FORMAT
 Lists supported skeleton body models. More...
 
enum class  BODY_KEYPOINTS_SELECTION
 Lists supported models for skeleton keypoints selection. More...
 
enum class  OBJECT_ACCELERATION_PRESET
 Lists of supported presets for maximum acceleration allowed for a given tracked object. More...
 
enum class  OBJECT_CLASS
 Lists available object classes. More...
 
enum class  OBJECT_SUBCLASS
 List available object subclasses. More...
 
enum class  OBJECT_TRACKING_STATE
 Lists the different states of object tracking. More...
 
enum class  OBJECT_ACTION_STATE
 Lists the different states of an object's actions. More...
 
enum class  OBJECT_DETECTION_MODEL
 Lists available models for the object detection module. More...
 
enum class  BODY_TRACKING_MODEL
 Lists available models for the body tracking module. More...
 
enum class  BODY_TRACKING_MODEL_GEN
 Lists the generations of neural network available for the body tracking module. More...
 
enum class  AI_MODELS
 Lists available AI models. More...
 
enum class  OBJECT_FILTERING_MODE
 Lists supported bounding box preprocessing. More...
 
enum class  INFERENCE_PRECISION
 Lists supported bounding box preprocessing. More...
 
enum class  BODY_18_PARTS
 Semantic of human body parts and order of sl.BodyData.keypoints for sl.BODY_FORMAT.BODY_18. More...
 
enum class  BODY_34_PARTS
 Semantic of human body parts and order of sl.BodyData.keypoints for sl.BODY_FORMAT.BODY_34. More...
 
enum class  BODY_38_PARTS
 Semantic of human body parts and order of sl.BodyData.keypoints for sl.BODY_FORMAT.BODY_38. More...
 
enum class  FUSION_ERROR_CODE
 Lists the types of error that can be raised by the Fusion. More...
 
enum class  SENDER_ERROR_CODE
 Lists the types of error that can be raised during the Fusion by senders. More...
 
enum class  COMM_TYPE
 Lists the different types of communications available for Fusion module. More...
 
enum class  GNSS_FUSION_STATUS
 Lists the different states of the GNSS fusion. More...
 
enum class  GNSS_STATUS
 
enum class  GNSS_MODE
 Gnss mode More...
 
enum class  FUSION_REFERENCE_FRAME
 Reference frame used for the positional tracking. More...
 
enum class  MAT_TYPE
 Lists available sl.Mat formats. More...
 
enum class  COPY_TYPE
 Lists available copy operation on sl.Mat. More...
 
enum class  MEM
 Lists available memory type. More...
 

Enumeration Type Documentation

◆ Constant

enum Constant
strong

Constant for plugin. Should not be changed

Enumerator
MAX_OBJECTS 
MAX_SUBMESH 

Maximum number of chunks. It's best to get relatively few chunks and to update them quickly.

MAX_BATCH_SIZE 

Max size of trajectory data (number of frames stored)

MAX_CAMERA_PLUGIN 

Maximum number of cameras that can be instantiated at the same time. Used to initialize arrays of cameras (ex: GetDeviceList()).

MAX_FUSED_CAMERAS 

Maximum number of camera that can be fused by the Fusion API.

ENCODED_STREAM_SOURCE_COUNT 

Number of encoded video sources a camera can expose. Used to size the array passed to GetEncodedStreamsInfo().

◆ MODULE

enum MODULE
strong

Lists available modules.

Enumerator
ALL 

All modules

DEPTH 

Depth module

POSITIONAL_TRACKING 

Positional tracking module

OBJECT_DETECTION 

Object Detection module

BODY_TRACKING 

Body Tracking module

SPATIAL_MAPPING 

Spatial mapping module

LAST 

◆ HEADING_STATE

enum HEADING_STATE
strong

Lists the different states of the magnetic heading.

Enumerator
GOOD 

The heading is reliable and not affected by iron interferences.

OK 

The heading is reliable, but affected by slight iron interferences.

NOT_GOOD 

The heading is not reliable because affected by strong iron interferences.

NOT_CALIBRATED 

The magnetometer has not been calibrated.

MAG_NOT_AVAILABLE 

The magnetometer sensor is not available.

◆ SIDE

enum SIDE
strong

Lists possible sides on which to get data from.

Enumerator
LEFT 

Left side only.

RIGHT 

Right side only.

BOTH 

Left and right side.

◆ AI_MODELS

enum AI_MODELS
strong

Lists available AI models.

Enumerator
MULTI_CLASS_DETECTION 

Related to sl.OBJECT_DETECTION_MODEL.MULTI_CLASS_BOX_FAST

MULTI_CLASS_MEDIUM_DETECTION 

Related to sl.OBJECT_DETECTION_MODEL.MULTI_CLASS_BOX_MEDIUM

MULTI_CLASS_ACCURATE_DETECTION 

Related to sl.OBJECT_DETECTION_MODEL.MULTI_CLASS_BOX_ACCURATE

HUMAN_BODY_FAST_DETECTION 

Related to sl.BODY_TRACKING_MODEL.HUMAN_BODY_FAST

HUMAN_BODY_MEDIUM_DETECTION 

Related to sl.BODY_TRACKING_MODEL.HUMAN_BODY_MEDIUM

HUMAN_BODY_ACCURATE_DETECTION 

Related to sl.BODY_TRACKING_MODEL.HUMAN_BODY_ACCURATE

HUMAN_BODY_38_FAST_DETECTION 

Related to sl.BODY_TRACKING_MODEL.HUMAN_BODY_FAST

HUMAN_BODY_38_MEDIUM_DETECTION 

Related to sl.BODY_TRACKING_MODEL.HUMAN_BODY_MEDIUM

HUMAN_BODY_38_ACCURATE_DETECTION 

Related to sl.BODY_TRACKING_MODEL.HUMAN_BODY_ACCURATE

PERSON_HEAD_DETECTION 

Related to sl.OBJECT_DETECTION_MODEL.PERSON_HEAD_BOX_FAST

PERSON_HEAD_ACCURATE_DETECTION 

Related to sl.OBJECT_DETECTION_MODEL.PERSON_HEAD_BOX_ACCURATE

REID_ASSOCIATION 

Related to sl.BatchParameters.enable

NEURAL_LIGHT_DEPTH 

Related to sl.DEPTH_MODE.NEURAL_LIGHT

NEURAL_DEPTH 

Related to sl.DEPTH_MODE.NEURAL

NEURAL_PLUS_DEPTH 

Related to sl.DEPTH_MODE.NEURAL_PLUS

NEURAL_DEPTH_INT8 

Related to sl.DEPTH_MODE.NEURAL with sl.DEPTH_PRECISION.INT8. Separate artifact and engine from NEURAL_DEPTH: optimizing one does not optimize the other.

◆ OBJECT_FILTERING_MODE

enum OBJECT_FILTERING_MODE
strong

Lists supported bounding box preprocessing.

Enumerator
NONE 

The ZED SDK will not apply any preprocessing to the detected objects.

NMS3D 

The ZED SDK will remove objects that are in the same 3D position as an already tracked object (independent of class id).

NMS3D_PER_CLASS 

The ZED SDK will remove objects that are in the same 3D position as an already tracked object of the same class id.

◆ INFERENCE_PRECISION

enum INFERENCE_PRECISION
strong

Lists supported bounding box preprocessing.

Enumerator
FP32 
FP16 
INT8 

◆ GNSS_STATUS

enum GNSS_STATUS
strong
Enumerator
UNKNOWN 

No GNSS fix data is available.

SINGLE 

Single Point Positioning.

DGNSS 

Differential GNSS.

RTK_FIX 

Real-Time Kinematic (RTK) GNSS fix in fixed mode.

RTK_FLOAT 

Real-Time Kinematic (RTK) GNSS fix in float mode.

PPS 

Precise Positioning Service.

◆ GNSS_MODE

enum GNSS_MODE
strong

Gnss mode

Enumerator
UNKNOWN 

No GNSS fix data is available.

NO_FIX 

No GNSS fix is available.

FIX_2D 

2D GNSS fix, providing latitude and longitude coordinates but without altitude information.

FIX_3D 

3D GNSS fix, providing latitude, longitude, and altitude coordinates.