Classes | |
| struct | ImuData |
| Structure containing data from the IMU sensor. More... | |
| struct | BarometerData |
| Structure containing data from the barometer sensor. More... | |
| struct | MagnetometerData |
| Structure containing data from the magnetometer sensor. More... | |
| struct | TemperatureSensorData |
| Structure containing data from the temperature sensors. More... | |
| struct | SensorsData |
| Structure containing all sensors data (except image sensors) to be used for positional tracking or environment study. More... | |
| struct | SensorParameters |
| Structure containing information about a single sensor available in the current device. More... | |
| struct | SensorsConfiguration |
| Structure containing information about all the sensors available in the current device. More... | |
| class | GNSS_STATUS |
| Class representing the fix quality of GNSS signal. More... | |
Enumerations | |
| enum class | HEADING_STATE |
| Lists the different states of the magnetic heading. More... | |
| enum class | SENSOR_TYPE |
| Lists available sensor types. More... | |
| enum class | SENSORS_UNIT |
| Lists available measurement units of onboard sensors. More... | |
|
strong |
Lists the different states of the magnetic heading.
|
strong |
Lists available sensor types.
|
strong |
Lists available measurement units of onboard sensors.
| Enumerator | |
|---|---|
| M_SEC_2 | m/s² (acceleration) |
| DEG_SEC | deg/s (angular velocity) |
| U_T | μT (magnetic field) |
| HPA | hPa (atmospheric pressure) |
| CELSIUS | °C (temperature) |
| HERTZ | Hz (frequency) |