Depth Sensing Module

Classes

class  RuntimeParameters
 Class containing parameters that defines the behavior of sl.Camera.Grab(). More...
 
struct  CameraParameters
 Structure containing the intrinsic parameters of a camera. More...
 
struct  CalibrationParameters
 Structure containing intrinsic and extrinsic parameters of the camera (translation and rotation). More...
 
struct  SVOData
 Structure containing data that can be stored in and retrieved from SVOs. That information will be ingested with sl.Camera.ingestDataIntoSVO and retrieved with sl.Camera.retrieveSVOData. More...
 

Enumerations

enum class  DEPTH_MODE
 Lists available depth computation modes. More...
 
enum class  MEASURE
 Lists retrievable measures. More...
 
enum class  REGION_OF_INTEREST_AUTO_DETECTION_STATE
 Lists the different states of region of interest auto detection. More...
 

Enumeration Type Documentation

◆ DEPTH_MODE

enum DEPTH_MODE
strong

Lists available depth computation modes.

Note
For more info, read about the ZED SDK C++ enum it mirrors: DEPTH_MODE
Enumerator
NONE 

No depth map computation.
Only rectified stereo images will be available.

PERFORMANCE 

Computation mode optimized for speed.

QUALITY 

Computation mode designed for challenging areas with untextured surfaces.

ULTRA 

Computation mode that favors edges and sharpness.
Requires more GPU memory and computation power.

NEURAL_LIGHT 

End to End Neural disparity estimation.
Requires AI module.

NEURAL 

End to End Neural disparity estimation.
Requires AI module.

NEURAL_PLUS 

More accurate Neural disparity estimation.
Requires AI module.

◆ MEASURE

enum MEASURE
strong

Lists retrievable measures.

Note
For more info, read about the ZED SDK C++ enum it mirrors: MEASURE
Enumerator
DISPARITY 

Disparity map. Each pixel contains 1 float.
Type: sl.MAT_TYPE.MAT_32F_C1

DEPTH 

Depth map in sl.UNIT defined in sl.InitParameters.coordinateUnits. Each pixel contains 1 float.
Type: sl.MAT_TYPE.MAT_32F_C1

CONFIDENCE 

Certainty/confidence of the depth map. Each pixel contains 1 float.
Type: sl.MAT_TYPE.MAT_32F_C1

XYZ 

Point cloud. Each pixel contains 4 float (X, Y, Z, not used).
Type: sl.MAT_TYPE.MAT_32F_C4

XYZRGBA 

Colored point cloud. Each pixel contains 4 float (X, Y, Z, color).
The color should to be read as an unsigned char[4] representing the RGBA color.
Type: sl.MAT_TYPE.MAT_32F_C4

XYZBGRA 

Colored point cloud. Each pixel contains 4 float (X, Y, Z, color).
The color should to be read as an unsigned char[4] representing the BGRA color.
Type: sl.MAT_TYPE.MAT_32F_C4

XYZARGB 

Colored point cloud. Each pixel contains 4 float (X, Y, Z, color).
The color should to be read as an unsigned char[4] representing the ARGB color.
Type: sl.MAT_TYPE.MAT_32F_C4

XYZABGR 

Colored point cloud. Each pixel contains 4 float (X, Y, Z, color).
The color should to be read as an unsigned char[4] representing the ABGR color.
Type: sl.MAT_TYPE.MAT_32F_C4

NORMALS 

Normal vectors map. Each pixel contains 4 float (X, Y, Z, 0).
Type: sl.MAT_TYPE.MAT_32F_C4

DISPARITY_RIGHT 

Disparity map for right sensor. Each pixel contains 1 float.
Type: sl.MAT_TYPE.MAT_32F_C1

DEPTH_RIGHT 

Depth map for right sensor. Each pixel contains 1 float.
Type: sl.MAT_TYPE.MAT_32F_C1

XYZ_RIGHT 

Point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, not used).
Type: sl.MAT_TYPE.MAT_32F_C4

XYZRGBA_RIGHT 

Colored point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, color). The color needs to be read as an unsigned char[4] representing the RGBA color.
Type: sl.MAT_TYPE.MAT_32F_C4

XYZBGRA_RIGHT 

Colored point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, color). The color needs to be read as an unsigned char[4] representing the BGRA color.
Type: sl.MAT_TYPE.MAT_32F_C4

XYZARGB_RIGHT 

Colored point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, color). The color needs to be read as an unsigned char[4] representing the ARGB color.
Type: sl.MAT_TYPE.MAT_32F_C4

XYZABGR_RIGHT 

Colored point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, color). The color needs to be read as an unsigned char[4] representing the ABGR color.
Type: sl.MAT_TYPE.MAT_32F_C4

NORMALS_RIGHT 

Normal vectors map for right view. Each pixel contains 4 float (X, Y, Z, 0).
Type: sl.MAT_TYPE.MAT_32F_C4

DEPTH_U16_MM 

Depth map in millimeter whatever the sl.UNIT defined in sl.InitParameters.coordinateUnits.
Invalid values are set to 0 and depth values are clamped at 65000.
Each pixel contains 1 unsigned short.
Type: sl.MAT_TYPE.MAT_16U_C1.

DEPTH_U16_MM_RIGHT 

Depth map in millimeter for right sensor. Each pixel contains 1 unsigned short.
Type: sl.MAT_TYPE.MAT_16U_C1.

◆ REGION_OF_INTEREST_AUTO_DETECTION_STATE

Lists the different states of region of interest auto detection.

Enumerator
RUNNING 

The region of interest auto detection is initializing.

READY 

The region of interest mask is ready, if auto_apply was enabled, the region of interest mask is being used.

NOT_ENABLED 

The region of interest auto detection is not enabled.