All Classes Namespaces Functions Variables Enumerations Enumerator Properties Modules Pages
Positional Tracking Module

Classes

class  PositionalTrackingParameters
 Class containing a set of parameters for the positional tracking module initialization. More...
 
struct  Pose
 Structure containing positional tracking data giving the position and orientation of the camera in 3D space. More...
 
struct  RegionOfInterestParameters
 Structure containing a set of parameters for the region of interest. More...
 
struct  PositionalTrackingStatus
 Lists the different status of positional tracking. More...
 

Enumerations

enum class  POSITIONAL_TRACKING_STATE
 Lists the different states of positional tracking. More...
 
enum class  ODOMETRY_STATUS
 Report the status of current odom tracking. More...
 
enum class  SPATIAL_MEMORY_STATUS
 Report the status of current map tracking. More...
 
enum class  POSITIONAL_TRACKING_FUSION_STATUS
 Report the status of the positional tracking fusion. More...
 
enum class  POSITIONAL_TRACKING_MODE
 Lists the mode of positional tracking that can be used. More...
 
enum class  REFERENCE_FRAME
 Lists possible types of position matrix used to store camera path and pose. More...
 
enum class  TRACKING_FRAME
 Part of the ZED (left/right sensor, center) that's considered its center for tracking purposes. More...
 

Enumeration Type Documentation

◆ POSITIONAL_TRACKING_STATE

Lists the different states of positional tracking.

Enumerator
SEARCHING 

\warn DEPRECATED: This state is no longer in use.

OK 

The positional tracking is working normally.

OFF 

The positional tracking is not enabled.

FPS_TOO_LOW 

The effective FPS is too low to give proper results for motion tracking.
Consider using performance parameters (sl.DEPTH_MODE.PERFORMANCE, low camera resolution (sl.RESOLUTION.VGA / sl.RESOLUTION.HDSVGA or sl.RESOLUTION.HD720).

SEARCHING_FLOOR_PLANE 

The camera is searching for the floor plane to locate itself with respect to it.
The sl.REFERENCE_FRAME.WORLD will be set afterward.

UNAVAILABLE 

The tracking module was unable to perform tracking from the previous frame to the current frame.

◆ ODOMETRY_STATUS

enum ODOMETRY_STATUS
strong

Report the status of current odom tracking.

Enumerator
OK 

The positional tracking module successfully tracked from the previous frame to the current frame.

UNAVAILABLE 

The positional tracking module failed to track from the previous frame to the current frame.

◆ SPATIAL_MEMORY_STATUS

enum SPATIAL_MEMORY_STATUS
strong

Report the status of current map tracking.

Enumerator
OK 

The positional tracking module is operating normally.

LOOP_CLOSED 

The positional tracking module detected a loop and corrected its position.

SEARCHING 

The positional tracking module is searching for recognizable areas in the global map to relocate.

OFF 

Spatial memory is disabled.

◆ POSITIONAL_TRACKING_FUSION_STATUS

Report the status of the positional tracking fusion.

Enumerator
VISUAL_INERTIAL 
VISUAL 
INERTIAL 
GNSS 
VISUAL_INERTIAL_GNSS 
VISUAL_GNSS 
INERTIAL_GNSS 
UNAVAILABLE 

◆ POSITIONAL_TRACKING_MODE

Lists the mode of positional tracking that can be used.

Enumerator
GEN_1 

Default mode. Best compromise in performance and accuracy.

GEN_2 

Next generation of positional tracking, allow better accuracy.

◆ REFERENCE_FRAME

enum REFERENCE_FRAME
strong

Lists possible types of position matrix used to store camera path and pose.

Enumerator
WORLD 

The transform of sl.Pose will contain the motion with reference to the world frame (previously called sl.PATH).

CAMERA 

The transform of sl.Pose will contain the motion with reference to the previous camera frame (previously called sl.POSE).

◆ TRACKING_FRAME

enum TRACKING_FRAME
strong

Part of the ZED (left/right sensor, center) that's considered its center for tracking purposes.

Enumerator
LEFT_EYE 

Camera's center is at the left sensor.

CENTER_EYE 

Camera's center is in the camera's physical center, between the sensors.

RIGHT_EYE 

Camera's center is at the right sensor.