Classes | |
| class | CommunicationParameters |
| Holds the communication parameter to configure the connection between senders and receiver. More... | |
| class | ECEF |
| Represents a world position in ECEF format. More... | |
| class | LatLng |
| Represents a world position in LatLng format. More... | |
| class | UTM |
| Represents a world position in UTM format. More... | |
| class | ENU |
| Represents a world position in ENU format. More... | |
| class | GeoConverter |
| Purely static class for Geo functions. More... | |
| class | GeoPose |
| Holds geographic reference position information. More... | |
| class | GNSSCalibrationParameters |
| Holds the options used for calibrating GNSS / VIO. More... | |
| class | CameraIdentifier |
| Used to identify a specific camera in the Fusion API. More... | |
| class | FusionConfiguration |
| Useful struct to store the Fusion configuration, can be read from /write to a JSON file. More... | |
| class | InitFusionParameters |
| Holds the options used to initialize the Fusion object. More... | |
| class | BodyTrackingFusionParameters |
| Holds the options used to initialize the body tracking module of the Fusion. More... | |
| class | BodyTrackingFusionRuntimeParameters |
| Holds the options used to change the behavior of the body tracking module at runtime. More... | |
| class | ObjectDetectionFusionParameters |
| Holds the options used to initialize the object detection module of the Fusion. More... | |
| class | PositionalTrackingFusionParameters |
| Holds the options used for initializing the positional tracking fusion module. More... | |
| class | SpatialMappingFusionParameters |
| Sets the spatial mapping parameters. More... | |
| class | CameraMetrics |
| Holds the metrics of a sender in the fusion process. More... | |
| class | FusionMetrics |
| Holds the metrics of the fusion process. More... | |
| class | Fusion |
| Holds Fusion process data and functions. More... | |
Enumerations | |
| enum class | POSITION_TYPE |
| Lists the types of possible position outputs. More... | |
| enum class | FUSION_REFERENCE_FRAME |
| Enum to define the reference frame of the fusion SDK. More... | |
| enum class | FUSION_ERROR_CODE |
| Lists the types of error that can be raised by the Fusion. More... | |
| enum class | SENDER_ERROR_CODE |
| Lists the types of error that can be raised during the Fusion by senders. More... | |
Functions | |
| FusionConfiguration | readFusionConfigurationFile (const std::string &json_config_filename, const int serial_number, const sl::COORDINATE_SYSTEM coord_sys, const sl::UNIT unit) |
| Read a configuration JSON file to configure a fusion process. More... | |
| std::vector< FusionConfiguration > | readFusionConfigurationFile (const std::string &json_config_filename, const sl::COORDINATE_SYSTEM coord_sys, const sl::UNIT unit) |
| Read a Configuration JSON file to configure a fusion process. More... | |
| std::vector< FusionConfiguration > | readFusionConfiguration (const std::string &fusion_configuration, const sl::COORDINATE_SYSTEM coord_sys, const sl::UNIT unit) |
| Read a Configuration JSON string to configure a fusion process. More... | |
| void | writeConfigurationFile (const std::string &json_config_filename, std::vector< FusionConfiguration > &configuration, const sl::COORDINATE_SYSTEM coord_sys, const sl::UNIT unit) |
| Write a Configuration JSON file to configure a fusion process. More... | |
Fusion | |
| ERROR_CODE | stopPublishing () |
| Set this camera as normal camera (without data providing). Stop to send camera data to fusion. More... | |
| CommunicationParameters | getCommunicationParameters () |
| Returns the CommunicationParameters used. It corresponds to the structure given as argument to the startPublishing() method. More... | |
|
strong |
|
strong |
|
strong |
Lists the types of error that can be raised by the Fusion.
| Enumerator | |
|---|---|
| FUSION_INCONSISTENT_FPS | Significant differences observed between sender's FPS. Fusion quality will be affected. |
| FUSION_FPS_TOO_LOW | Fusion FPS is too low because at least one sender has an FPS lower than 10 FPS. Fusion quality will be affected. |
| INVALID_TIMESTAMP | You have attempted to ingest GNSSData into the Fusion system with an invalid timestamp. It is essential to ensure that the timestamp of your GNSSData is set correctly. This issue may arise from a unit error in the ingested timestamp, such as providing the timestamp in microseconds instead of nanoseconds. |
| INVALID_COVARIANCE | This is a warning message notifying you about an issue encountered while ingesting GNSSData into the Fusion system. The problem lies in the very low covariance value provided. To ensure stability and prevent potential issues, the system will automatically clamp this covariance value. |
| NO_NEW_DATA_AVAILABLE | All data from all sources has been consumed. No new data is available for processing. |
| SUCCESS | Standard code indicating successful behavior. |
| GNSS_DATA_NEED_FIX | This is a warning message indicating an issue with the ingestGNSSData function call. The problem lies in the gnss_status field of |
| GNSS_DATA_COVARIANCE_MUST_VARY | It appears that you have made multiple calls to the ingestGNSSData function using the same GNSSData covariance. This warning is intended to prevent users from repeatedly ingesting a fixed or manually crafted covariance. |
| BODY_FORMAT_MISMATCH | Senders are using different body formats. Please use the same body format. |
| MODULE_NOT_ENABLED | The following module is not enabled. Please enable it to proceed. |
| SOURCE_MISMATCH | Some sources are provided by SVO and others by LIVE stream. |
| CONNECTION_TIMED_OUT | Connection timed out. Unable to reach the sender. Verify the sender's IP address and port. |
| MEMORY_ALREADY_USED | Intra-process shared memory allocation issue. Multiple connections to the same data. Check memory usage. |
| INVALID_IP_ADDRESS | The provided IP address format is incorrect. Please provide a valid IP address in the format 'a.b.c.d'. |
| FAILURE | Standard code indicating unsuccessful behavior. |
|
strong |
Lists the types of error that can be raised during the Fusion by senders.
| Enumerator | |
|---|---|
| GRAB_ERROR | |
| INCONSISTENT_FPS | |
| FPS_TOO_LOW | The frame rate of the sender is lower than 10 FPS. Check sender's settings and performance. |
| SUCCESS | |
| DISCONNECTED | |
| ERROR_CODE stopPublishing | ( | ) |
Set this camera as normal camera (without data providing).
Stop to send camera data to fusion.
| CommunicationParameters getCommunicationParameters | ( | ) |
Returns the CommunicationParameters used.
It corresponds to the structure given as argument to the startPublishing() method.
| FusionConfiguration sl::readFusionConfigurationFile | ( | const std::string & | json_config_filename, |
| const int | serial_number, | ||
| const sl::COORDINATE_SYSTEM | coord_sys, | ||
| const sl::UNIT | unit | ||
| ) |
Read a configuration JSON file to configure a fusion process.
| json_config_filename | : The name of the JSON file containing the configuration. |
| serial_number | : The serial number of the ZED Camera you want to retrieve. |
| coord_sys | : The COORDINATE_SYSTEM in which you want the World Pose to be in. |
| unit | : The UNIT in which you want the World Pose to be in. |
| std::vector<FusionConfiguration> sl::readFusionConfigurationFile | ( | const std::string & | json_config_filename, |
| const sl::COORDINATE_SYSTEM | coord_sys, | ||
| const sl::UNIT | unit | ||
| ) |
Read a Configuration JSON file to configure a fusion process.
| json_config_filename | : The name of the JSON file containing the configuration. |
| coord_sys | : The COORDINATE_SYSTEM in which you want the World Pose to be in. |
| unit | : The UNIT in which you want the World Pose to be in. |
| std::vector<FusionConfiguration> sl::readFusionConfiguration | ( | const std::string & | fusion_configuration, |
| const sl::COORDINATE_SYSTEM | coord_sys, | ||
| const sl::UNIT | unit | ||
| ) |
Read a Configuration JSON string to configure a fusion process.
| fusion_configuration | : The string containing the configuration (it will be parsed as JSON). |
| coord_sys | : Defines the COORDINATE_SYSTEM of the Fusion World Pose. |
| unit | : Defines the UNIT of the Fusion World Pose. |
| void sl::writeConfigurationFile | ( | const std::string & | json_config_filename, |
| std::vector< FusionConfiguration > & | configuration, | ||
| const sl::COORDINATE_SYSTEM | coord_sys, | ||
| const sl::UNIT | unit | ||
| ) |
Write a Configuration JSON file to configure a fusion process.
| json_config_filename | : The name of the JSON that will contain the information. |
| configuration | A vector of FusionConfiguration listing all the camera configurations. |
| coord_sys | : The COORDINATE_SYSTEM in which the World Pose is. |
| unit | : The UNIT in which the World Pose is. |