Core Module

Classes

struct  Timestamp
 Structure representing timestamps with utilities. More...
 
struct  SensorsData
 Structure containing all sensors data (except image sensors) to be used for positional tracking or environment study. More...
 
struct  SensorsData::BarometerData
 Structure containing data from the barometer sensor. More...
 
struct  SensorsData::TemperatureData
 Structure containing data from the temperature sensors. More...
 
struct  SensorsData::MagnetometerData
 Structure containing data from the magnetometer sensor. More...
 
struct  SensorsData::IMUData
 Structure containing data from the IMU sensor. More...
 
struct  CameraOneConfiguration
 Structure containing information about the camera sensor. More...
 
struct  CameraOneInformation
 Structure containing information of a single camera (serial number, model, input type, etc.). More...
 
class  String
 Class defining a string. More...
 
struct  Resolution
 Structure containing the width and height of an image. More...
 
class  Rect
 Class defining a 2D rectangle with top-left corner coordinates and width/height in pixels. More...
 
class  Matrix3f
 Class representing a generic 3*3 matrix. More...
 
class  Matrix4f
 Class representing a generic 4*4 matrix. More...
 
class  Vector2< T >
 Class representing a 2-dimensional vector for both CPU and GPU. More...
 
class  Vector3< T >
 Class representing a 3-dimensional vector for both CPU and GPU. More...
 
class  Vector4< T >
 Class representing a 4-dimensional vector for both CPU and GPU. More...
 
class  Mat
 Class representing 1 to 4-channel matrix of float or uchar, stored on CPU and/or GPU side. More...
 
struct  TensorParameters
 Structure to define the input options for deep learning inference. More...
 
class  Tensor
 Class representing a multi-dimensional array (Tensor), typically used for deep learning inference. More...
 
struct  SensorParameters
 Structure containing information about a single sensor available in the current device. More...
 
struct  SensorsConfiguration
 Structure containing information about all the sensors available in the current device. More...
 
struct  CameraConfiguration
 Structure containing information about the camera sensor. More...
 
struct  CameraInformation
 Structure containing information of a single camera (serial number, model, input type, etc.). More...
 

Enumerations

enum class  SENSORS_ERROR_CODE
 Lists error codes in the Sensors SDK. More...
 
enum class  UNIT
 Lists available units for measures. More...
 
enum class  COORDINATE_SYSTEM
 Lists available coordinates systems for positional tracking and 3D measures. More...
 
enum class  ERROR_CODE
 Lists error codes in the ZED SDK. More...
 
enum class  COMPUTE_PREFERENCE
 Lists how much GPU a module is allowed to use. More...
 
enum class  LENS_DISTORTION_MODEL
 Lists the lens distortion models used to describe a camera's optics. More...
 
enum class  SENSOR_TYPE
 Lists available sensor types. More...
 
enum class  SENSORS_UNIT
 Lists available measurement units of onboard sensors. More...
 
enum class  MEM
 Lists available memory type. More...
 
enum class  COPY_TYPE
 Lists available copy operation on sl::Mat. More...
 
enum class  MAT_TYPE
 Lists available sl::Mat formats. More...
 
enum class  CAMERA_MOTION_STATE
 Lists different states of the camera motion. More...
 
enum class  MODULE
 Lists available modules. More...
 

Functions

int getZEDSDKRuntimeVersion (int &major, int &minor, int &patch)
 Returns the ZED SDK version currently installed on the computer. More...
 
const void getZEDSDKBuildVersion (int &major, int &minor, int &patch)
 Returns the ZED SDK version which the current program has been compiled with. More...
 
String toVerbose (const ERROR_CODE &errorCode)
 Provide a concise sl::ERROR_CODE string. More...
 
bool isCameraOne (const sl::MODEL)
 Check the type of a camera model. More...
 
void sleep_ms (int time)
 Blocks the execution of the current thread for time milliseconds. More...
 
void sleep_us (int time)
 Blocks the execution of the current thread for time microseconds. More...
 

Enumeration Type Documentation

◆ SENSORS_ERROR_CODE

enum SENSORS_ERROR_CODE
strong

Lists error codes in the Sensors SDK.

Enumerator
STALE_DATA 

In pipelined mode with DROP_STALE sync policy, the retrieved data is too old relative to the sync timestamp. The frame was not returned to avoid using outdated information.

GNSS_DATA_NEED_FIX 

This is a warning message indicating an issue with the ingestGNSSData function call. The problem lies in the gnss_status field of the GNSSData parameter, which is currently set to UNKNOWN. To enhance the accuracy of the VPS (Visual Positioning System), it is essential to provide an appropriate value for this field. To rectify this issue, please consider setting the gnss_status field to a valid value that reflects the status of your GNSS sensor. If your GNSS sensor is unable to output a status, it is recommended to set the gnss_status field to sl::GNSS_STATUS::SINGLE.

INVALID_COVARIANCE 

This is a warning message notifying you about an issue encountered while ingesting GNSSData into the Fusion system. The problem lies in the very low covariance value provided. To ensure stability and prevent potential issues, the system will automatically clamp this covariance value.

INVALID_TIMESTAMP 

You have attempted to ingest GNSSData into the Fusion system with an invalid timestamp. It is essential to ensure that the timestamp of your GNSSData is set correctly. This issue may arise from a unit error in the ingested timestamp, such as providing the timestamp in microseconds instead of nanoseconds.

CONFIGURATION_FALLBACK 

The operation could not proceed with the target configuration but did success with a fallback.

MOTION_SENSORS_DATA_REQUIRED 

The input data does not contains the high frequency motion sensors data (IMU), this is usually because it requires newer SVO/Streaming. In order to work this modules needs inertial data present in it input.

CORRUPTED_FRAME 

The image is corrupted with invalid colors (green/purple images). This indicates a serious hardware or driver issue.

SENSOR_REBOOTING 

The sensor is currently rebooting.

SUCCESS 

Standard code for successful behavior.

FAILURE 

Standard code for unsuccessful behavior.

NO_GPU_COMPATIBLE 

No GPU found or CUDA capability of the device is not supported.

NOT_ENOUGH_GPU_MEMORY 

Not enough GPU memory for this depth mode, try a different mode (such as PERFORMANCE), or increase the minimum depth value (see InitParameters::depth_minimum_distance).

SENSOR_NOT_DETECTED 

No sensor was detected.

MOTION_SENSORS_NOT_INITIALIZED 

The MCU that controls the motion sensors module (IMU) has an invalid serial number. You can try to recover it by launching the ZED Diagnostic tool from the command line with the option -r.

MOTION_SENSORS_NOT_AVAILABLE 

A camera with motion sensors is detected but the motion sensors (IMU, barometer, ...) cannot be opened. Only the MODEL::ZED does not have motion sensors. Unplug/replug is required.

INVALID_RESOLUTION 

In case of invalid resolution parameter, such as an upsize beyond the original image size in Camera::retrieveImage.

LOW_USB_BANDWIDTH 

Insufficient bandwidth for the correct use of the camera. This issue can occur when you use multiple cameras or a USB 2.0 port.

CALIBRATION_FILE_NOT_AVAILABLE 

The calibration file of the camera is not found on the host machine. Use ZED Explorer or ZED Calibration to download the factory calibration file.

INVALID_CALIBRATION_FILE 

The calibration file is not valid. Try to download the factory calibration file or recalibrate your camera using ZED Calibration.

INVALID_SVO_FILE 

The provided SVO file is not valid.

SVO_RECORDING_ERROR 

An error occurred while trying to record an SVO (not enough free storage, invalid file, ...).

SVO_UNSUPPORTED_COMPRESSION 

An SVO related error, occurs when NVIDIA based compression cannot be loaded.

END_OF_SVOFILE_REACHED 

SVO end of file has been reached.
No frame will be available until the SVO position is reset.

INVALID_COORDINATE_SYSTEM 

The requested coordinate system is not available.

INVALID_FIRMWARE 

The firmware of the camera is out of date. Update to the latest version.

INVALID_FUNCTION_PARAMETERS 

Invalid parameters have been given for the function.

CUDA_ERROR 

A CUDA error has been detected in the process, in Camera.grab() or Camera.retrieveXXX() only. Activate verbose in Camera.open() for more info.

SENSOR_NOT_INITIALIZED 

The sensor is not initialized. Probably a missing call to open the sensor.

NVIDIA_DRIVER_OUT_OF_DATE 

Your NVIDIA driver is too old and not compatible with your current CUDA version.

INVALID_FUNCTION_CALL 

The call of the function is not valid in the current context. Could be a missing call of Camera.open().

CORRUPTED_SDK_INSTALLATION 

The ZED SDK was not able to load its dependencies or some assets are missing. Reinstall the ZED SDK or check for missing dependencies (TensorRT).

INCOMPATIBLE_SDK_VERSION 

The installed ZED SDK is incompatible with the one used to compile the program.

INVALID_AREA_FILE 

The given area file does not exist. Check the path.

INCOMPATIBLE_AREA_FILE 

The area file does not contain enough data to be used or the DEPTH_MODE used during the creation of the area file is different from the one currently set.

SENSOR_FAILED_TO_SETUP 

Failed to open the sensor at the proper resolution. Try another resolution or make sure that the UVC driver is properly installed.

SENSOR_DETECTION_ISSUE 

Your sensor can not be opened. Try replugging it to another port or flipping the USB-C connector (if there is one).

CANNOT_START_SENSOR_STREAM 

Cannot start the sensor stream. Make sure your sensor is not already used by another process or blocked by firewall or antivirus.

NO_GPU_DETECTED 

No GPU found. CUDA is unable to list it. Can be a driver/reboot issue.

PLANE_NOT_FOUND 

Plane not found. Either no plane is detected in the scene, at the location or corresponding to the floor, or the floor plane doesn't match the prior given.

MODULE_NOT_COMPATIBLE_WITH_SENSOR 

The module you try to use is not compatible with your sensor MODEL.

Note
MODEL::ZED does not have an IMU and does not support the AI modules.
MOTION_SENSORS_REQUIRED 

The module needs the sensors to be enabled (see InitParameters::sensors_required).

MODULE_NOT_COMPATIBLE_WITH_CUDA_VERSION 

The module needs a newer version of CUDA.

DRIVER_FAILURE 

The drivers initialization has failed. When using gmsl cameras, try restarting with sudo systemctl restart zed_x_daemon.service

CAMERA_EXCEEDS_BANDWIDTH 

The camera configuration exceeds available PHY CSI bandwidth (GMSL). Reduce resolution/FPS or adjust hardware configuration.

◆ UNIT

enum UNIT
strong

Lists available units for measures.

Enumerator
MILLIMETER 

International System (1/1000 meters)

CENTIMETER 

International System (1/100 meters)

METER 

International System (1 meter)

INCH 

Imperial Unit (1/12 feet)

FOOT 

Imperial Unit (1 foot)

◆ COORDINATE_SYSTEM

enum COORDINATE_SYSTEM
strong

Lists available coordinates systems for positional tracking and 3D measures.

Enumerator
IMAGE 

Standard coordinates system in computer vision.
Used in OpenCV: see here.

LEFT_HANDED_Y_UP 

Left-handed with Y up and Z forward.
Used in Unity with DirectX.

RIGHT_HANDED_Y_UP 

Right-handed with Y pointing up and Z backward.
Used in OpenGL.

RIGHT_HANDED_Z_UP 

Right-handed with Z pointing up and Y forward.
Used in 3DSMax.

LEFT_HANDED_Z_UP 

Left-handed with Z axis pointing up and X forward.
Used in Unreal Engine.

RIGHT_HANDED_Z_UP_X_FWD 

Right-handed with Z pointing up and X forward.
Used in ROS (REP 103).

◆ ERROR_CODE

enum ERROR_CODE
strong

Lists error codes in the ZED SDK.

Enumerator
SENSOR_CONFIGURATION_CHANGED 

The sensor's configuration (mode, multicast, etc.) was changed externally while streaming. If auto_recovery_on_config_change is enabled, the SDK will automatically reconnect. This warning code is returned once after successful recovery.

POTENTIAL_CALIBRATION_ISSUE 

The camera has a potential calibration issue

CONFIGURATION_FALLBACK 

The operation could not proceed with the target configuration but did success with a fallback.

SENSORS_DATA_REQUIRED 

The input data does not contains the high frequency sensors data, this is usually because it requires newer SVO/Streaming. In order to work this modules needs inertial data present in it input.

CORRUPTED_FRAME 

The image is corrupted with invalid colors (green/purple images). This indicates a serious hardware or driver issue. Check camera connection and drivers.

CAMERA_REBOOTING 

The camera is currently rebooting.

SUCCESS 

Standard code for successful behavior.

FAILURE 

Standard code for unsuccessful behavior.

NO_GPU_COMPATIBLE 

No GPU found or CUDA capability of the device is not supported.

NOT_ENOUGH_GPU_MEMORY 

Not enough GPU memory for this depth mode, try a different mode (such as PERFORMANCE), or increase the minimum depth value (see InitParameters::depth_minimum_distance).

CAMERA_NOT_DETECTED 

No camera was detected.

SENSORS_NOT_INITIALIZED 

The MCU that controls the sensors module has an invalid serial number. You can try to recover it by launching the ZED Diagnostic tool from the command line with the option -r.

SENSORS_NOT_AVAILABLE 

A camera with sensor is detected but the sensors (IMU, barometer, ...) cannot be opened. Only the MODEL::ZED does not has sensors. Unplug/replug is required.

INVALID_RESOLUTION 

In case of invalid resolution parameter, such as an upsize beyond the original image size in Camera::retrieveImage.

LOW_USB_BANDWIDTH 

Insufficient bandwidth for the correct use of the camera. This issue can occur when you use multiple cameras or a USB 2.0 port.

CALIBRATION_FILE_NOT_AVAILABLE 

The calibration file of the camera is not found on the host machine. Use ZED Explorer or ZED Calibration to download the factory calibration file.

INVALID_CALIBRATION_FILE 

The calibration file is not valid. Try to download the factory calibration file or recalibrate your camera using ZED Calibration.

INVALID_SVO_FILE 

The provided SVO file is not valid.

SVO_RECORDING_ERROR 

An error occurred while trying to record an SVO (not enough free storage, invalid file, ...).

SVO_UNSUPPORTED_COMPRESSION 

An SVO related error, occurs when NVIDIA based compression cannot be loaded.

END_OF_SVOFILE_REACHED 

SVO end of file has been reached.
No frame will be available until the SVO position is reset.

INVALID_COORDINATE_SYSTEM 

The requested coordinate system is not available.

INVALID_FIRMWARE 

The firmware of the camera is out of date. Update to the latest version.

INVALID_FUNCTION_PARAMETERS 

Invalid parameters have been given for the function.

CUDA_ERROR 

A CUDA error has been detected in the process, in Camera.grab() or Camera.retrieveXXX() only. Activate verbose in Camera.open() for more info.

CAMERA_NOT_INITIALIZED 

The ZED SDK is not initialized. Probably a missing call to Camera.open().

NVIDIA_DRIVER_OUT_OF_DATE 

Your NVIDIA driver is too old and not compatible with your current CUDA version.

INVALID_FUNCTION_CALL 

The call of the function is not valid in the current context. Could be a missing call of Camera.open().

CORRUPTED_SDK_INSTALLATION 

The ZED SDK was not able to load its dependencies or some assets are missing. Reinstall the ZED SDK or check for missing dependencies (TensorRT).

INCOMPATIBLE_SDK_VERSION 

The installed ZED SDK is incompatible with the one used to compile the program.

INVALID_AREA_FILE 

The given area file does not exist. Check the path.

INCOMPATIBLE_AREA_FILE 

The area file does not contain enough data to be used or the DEPTH_MODE used during the creation of the area file is different from the one currently set.

CAMERA_FAILED_TO_SETUP 

Failed to open the camera at the proper resolution. Try another resolution or make sure that the UVC driver is properly installed.

CAMERA_DETECTION_ISSUE 

Your camera can not be opened. Try replugging it to another port or flipping the USB-C connector (if there is one).

CANNOT_START_CAMERA_STREAM 

Cannot start the camera stream. Make sure your camera is not already used by another process or blocked by firewall or antivirus.

NO_GPU_DETECTED 

No GPU found. CUDA is unable to list it. Can be a driver/reboot issue.

PLANE_NOT_FOUND 

Plane not found. Either no plane is detected in the scene, at the location or corresponding to the floor, or the floor plane doesn't match the prior given.

MODULE_NOT_COMPATIBLE_WITH_CAMERA 

The module you try to use is not compatible with your camera MODEL.

Note
MODEL::ZED does not has an IMU and does not support the AI modules.
MOTION_SENSORS_REQUIRED 

The module needs the sensors to be enabled (see InitParameters::sensors_required).

MODULE_NOT_COMPATIBLE_WITH_CUDA_VERSION 

The module needs a newer version of CUDA.

DRIVER_FAILURE 

The drivers initialization has failed. When using gmsl cameras, try restarting with sudo systemctl restart zed_x_daemon.service

CAMERA_EXCEEDS_BANDWIDTH 

The camera configuration exceeds available PHY CSI bandwidth (GMSL). Reduce resolution/FPS or adjust hardware configuration.

◆ COMPUTE_PREFERENCE

enum COMPUTE_PREFERENCE
strong

Lists how much GPU a module is allowed to use.

Note
The selected mode sets a floor that cannot be avoided: for example POSITIONAL_TRACKING_MODE::GEN_1 computes depth and therefore always uses the GPU. This preference only controls the work that is optional on top of that floor.
Enumerator
AUTO 

Default. Let the SDK choose. For positional tracking, POSITIONAL_TRACKING_MODE::GEN_3 runs on the CPU and POSITIONAL_TRACKING_MODE::GEN_1 uses the GPU, since it computes depth.

PREFER_CPU 

Use no more GPU than the selected mode requires, leaving the GPU free for your own workloads. Tracking is slower than with GPU acceleration.

PREFER_GPU 

Use GPU acceleration wherever it is available, which makes tracking faster and lowers the per-frame time of sl::Camera::grab(). Falls back to the CPU by itself if the GPU cannot be used.

◆ LENS_DISTORTION_MODEL

enum LENS_DISTORTION_MODEL
strong

Lists the lens distortion models used to describe a camera's optics.

Note
The value is tied to the rectification state of the sl::CameraParameters it belongs to: raw/unrectified parameters are always RAD_TAN or FISHEYE, rectified parameters are always PINHOLE. Code working on raw parameters may treat "not FISHEYE" as RAD_TAN, but must not assume that on parameters that could be rectified.
Enumerator
RAD_TAN 

Radial-tangential (Brown-Conrady) distortion. Used by raw/unrectified parameters.

FISHEYE 

Fisheye distortion. Used by raw/unrectified parameters.

PINHOLE 

Pinhole model, no distortion. Used by rectified parameters.

◆ SENSOR_TYPE

enum SENSOR_TYPE
strong

Lists available sensor types.

Note
Sensors are not available on sl::MODEL::ZED.
Enumerator
ACCELEROMETER 

Three-axis accelerometer sensor to measure the inertial accelerations.

GYROSCOPE 

Three-axis gyroscope sensor to measure the angular velocities.

MAGNETOMETER 

Three-axis magnetometer sensor to measure the orientation of the device with respect to the Earth's magnetic field.

BAROMETER 

Barometer sensor to measure the atmospheric pressure.

◆ SENSORS_UNIT

enum SENSORS_UNIT
strong

Lists available measurement units of onboard sensors.

Note
Sensors are not available on sl::MODEL::ZED.
Enumerator
M_SEC_2 

m/s² (acceleration)

DEG_SEC 

deg/s (angular velocity)

U_T 

μT (magnetic field)

HPA 

hPa (atmospheric pressure)

CELSIUS 

°C (temperature)

HERTZ 

Hz (frequency)

◆ MEM

enum MEM
strong

Lists available memory type.

Enumerator
CPU 

Data will be stored on the CPU (processor side).

GPU 

Data will be stored on the GPU (graphic card side).

BOTH 

Data will be stored on the GPU and CPU.

LAST 

◆ COPY_TYPE

enum COPY_TYPE
strong

Lists available copy operation on sl::Mat.

Enumerator
CPU_CPU 

Copy data from CPU to CPU.

CPU_GPU 

Copy data from CPU to GPU.

GPU_GPU 

Copy data from GPU to GPU.

GPU_CPU 

Copy data from GPU to CPU.

◆ MAT_TYPE

enum MAT_TYPE
strong

Lists available sl::Mat formats.

Note
sl::Mat type depends on image or measure type.
For the dependencies, see sl::VIEW and sl::MEASURE.
Enumerator
F32_C1 

1-channel matrix of float

F32_C2 

2-channel matrix of float

F32_C3 

3-channel matrix of float

F32_C4 

4-channel matrix of float

U8_C1 

1-channel matrix of unsigned char

U8_C2 

2-channel matrix of unsigned char

U8_C3 

3-channel matrix of unsigned char

U8_C4 

4-channel matrix of unsigned char

U16_C1 

1-channel matrix of unsigned short

S8_C4 

4-channel matrix of signed char

NV12 

YUV 4:2:0 semi-planar data Y UVUVUV

◆ CAMERA_MOTION_STATE

enum CAMERA_MOTION_STATE
strong

Lists different states of the camera motion.

Enumerator
STATIC 

The camera is static.

MOVING 

The camera is moving.

FALLING 

The camera is falling.

◆ MODULE

enum MODULE
strong

Lists available modules.

Enumerator
ALL 

All modules

DEPTH 
POSITIONAL_TRACKING 
OBJECT_DETECTION 
BODY_TRACKING 
SPATIAL_MAPPING 
LAST 

Function Documentation

◆ getZEDSDKRuntimeVersion()

int getZEDSDKRuntimeVersion ( int &  major,
int &  minor,
int &  patch 
)

Returns the ZED SDK version currently installed on the computer.

Parameters
[out]major: Major variable to be filled.
[out]minor: Minor variable to be filled.
[out]patch: Patch variable to be filled.
Returns
-1 if the ZED SDK was not found
-2 if the ZED SDK version wasn't found
0 if success

◆ getZEDSDKBuildVersion()

const void getZEDSDKBuildVersion ( int &  major,
int &  minor,
int &  patch 
)
inline

Returns the ZED SDK version which the current program has been compiled with.

Parameters
[out]major: Major variable to be filled.
[out]minor: Minor variable to be filled.
[out]patch: Patch variable to be filled.

◆ toVerbose()

String sl::toVerbose ( const ERROR_CODE errorCode)

Provide a concise sl::ERROR_CODE string.

Returns
A concise sl::ERROR_CODE string for the user.

◆ isCameraOne()

bool sl::isCameraOne ( const sl::MODEL  )

Check the type of a camera model.

Returns
true if the specified camera model is a monocular camera

◆ sleep_ms()

void sl::sleep_ms ( int  time)
inline

Blocks the execution of the current thread for time milliseconds.

Parameters
time: Number of milliseconds to wait.

◆ sleep_us()

void sl::sleep_us ( int  time)
inline

Blocks the execution of the current thread for time microseconds.

Parameters
time: Number of microseconds to wait.