Classes | |
| class | PositionalTrackingParameters |
| Parameters for positional tracking initialization. More... | |
| class | Rotation |
| Designed to contain rotation data of the positional tracking. It inherits from the generic Matrix3f. More... | |
| class | Translation |
| Designed to contain translation data of the positional tracking. More... | |
| class | Orientation |
| Designed to contain orientation (quaternion) data of the positional tracking. More... | |
| class | Transform |
| Designed to contain translation and rotation data of the positional tracking. More... | |
| class | Pose |
| Contains positional tracking data which gives the position and orientation of the ZED in 3D space. More... | |
Enumerations | |
| enum class | POSITIONAL_TRACKING_STATE |
| Lists the different states of positional tracking. More... | |
| enum class | REFERENCE_FRAME |
| Defines which type of position matrix is used to store camera path and pose. More... | |
|
strong |
Lists the different states of positional tracking.
| Enumerator | |
|---|---|
| SEARCHING | The camera is searching for a previously known position to locate itself. |
| OK | Positional tracking is working normally. |
| OFF | Positional tracking is not enabled. |
| FPS_TOO_LOW | Effective FPS is too low to give proper results for motion tracking. Consider using PERFORMANCES parameters (DEPTH_MODE_PERFORMANCE, low camera resolution (VGA,HD720)) |
| SEARCHING_FLOOR_PLANE | The camera is searching for the floor plane to locate itself related to it, the REFERENCE_FRAME::WORLD will be set afterward. |
|
strong |
Defines which type of position matrix is used to store camera path and pose.
| Enumerator | |
|---|---|
| WORLD | The transform of sl::Pose will contains the motion with reference to the world frame (previously called PATH). |
| CAMERA | The transform of sl::Pose will contains the motion with reference to the previous camera frame (previously called POSE). |