Classes | |
| class | COMM_TYPE |
| Lists the different types of communications available for Fusion module. More... | |
| class | FUSION_ERROR_CODE |
| Lists the types of error that can be raised by the Fusion. More... | |
| class | SENDER_ERROR_CODE |
| Lists the types of error that can be raised during the Fusion by senders. More... | |
| class | POSITION_TYPE |
| Lists the types of possible position outputs. More... | |
| class | FUSION_REFERENCE_FRAME |
| Enum to define the reference frame of the fusion SDK. More... | |
| class | CommunicationParameters |
| Holds the communication parameter to configure the connection between senders and receiver. More... | |
| class | FusionConfiguration |
| Useful struct to store the Fusion configuration, can be read from /write to a JSON file. More... | |
| class | GNSSCalibrationParameters |
| Holds the options used for calibrating GNSS / VIO. More... | |
| class | PositionalTrackingFusionParameters |
| Holds the options used for initializing the positional tracking fusion module. More... | |
| class | BodyTrackingFusionParameters |
| Holds the options used to initialize the body tracking module of the Fusion. More... | |
| class | BodyTrackingFusionRuntimeParameters |
| Holds the options used to change the behavior of the body tracking module at runtime. More... | |
| class | ObjectDetectionFusionParameters |
| Holds the options used to initialize the object detection module of the Fusion. More... | |
| class | CameraMetrics |
| Holds the metrics of a sender in the fusion process. More... | |
| class | FusionMetrics |
| Holds the metrics of the fusion process. More... | |
| class | CameraIdentifier |
| Used to identify a specific camera in the Fusion API. More... | |
| class | ECEF |
| Represents a world position in ECEF format. More... | |
| class | LatLng |
| Represents a world position in LatLng format. More... | |
| class | UTM |
| Represents a world position in UTM format. More... | |
| class | ENU |
| Represent a world position in ENU format. More... | |
| class | GeoConverter |
| Purely static class for Geo functions. More... | |
| class | GeoPose |
| Holds Geo reference position. More... | |
| class | InitFusionParameters |
| Holds the options used to initialize the Fusion object. More... | |
| class | Fusion |
| Holds Fusion process data and functions. More... | |
Functions | |
| FusionConfiguration | read_fusion_configuration_file_from_serial (self, str json_config_filename, int serial_number, COORDINATE_SYSTEM coord_system, UNIT unit) |
| Read a configuration JSON file to configure a fusion process. More... | |
| list[FusionConfiguration] | read_fusion_configuration_file (str json_config_filename, COORDINATE_SYSTEM coord_system, UNIT unit) |
| Read a Configuration JSON file to configure a fusion process. More... | |
| list[FusionConfiguration] | read_fusion_configuration_json (dict fusion_configuration, COORDINATE_SYSTEM coord_system, UNIT unit) |
| Read a Configuration JSON to configure a fusion process. More... | |
| def | write_configuration_file (str json_config_filename, list fusion_configurations, COORDINATE_SYSTEM coord_sys, UNIT unit) |
| Write a Configuration JSON file to configure a fusion process. More... | |
| FusionConfiguration pyzed.sl.read_fusion_configuration_file_from_serial | ( | self, | |
| str | json_config_filename, | ||
| int | serial_number, | ||
| COORDINATE_SYSTEM | coord_system, | ||
| UNIT | unit | ||
| ) |
Read a configuration JSON file to configure a fusion process.
| json_config_filename | : The name of the JSON file containing the configuration. |
| serial_number | : The serial number of the ZED Camera you want to retrieve. |
| coord_system | : The COORDINATE_SYSTEM in which you want the World Pose to be in. |
| unit | : The UNIT in which you want the World Pose to be in. |
Referenced by FusionConfiguration.override_gravity().
| list[FusionConfiguration] pyzed.sl.read_fusion_configuration_file | ( | str | json_config_filename, |
| COORDINATE_SYSTEM | coord_system, | ||
| UNIT | unit | ||
| ) |
Read a Configuration JSON file to configure a fusion process.
| json_config_filename | : The name of the JSON file containing the configuration. |
| coord_sys | : The COORDINATE_SYSTEM in which you want the World Pose to be in. |
| unit | : The UNIT in which you want the World Pose to be in. |
Referenced by FusionConfiguration.override_gravity().
| list[FusionConfiguration] pyzed.sl.read_fusion_configuration_json | ( | dict | fusion_configuration, |
| COORDINATE_SYSTEM | coord_system, | ||
| UNIT | unit | ||
| ) |
Read a Configuration JSON to configure a fusion process.
| fusion_configuration | : The JSON containing the configuration. |
| coord_sys | : The COORDINATE_SYSTEM in which you want the World Pose to be in. |
| unit | : The UNIT in which you want the World Pose to be in. |
Referenced by FusionConfiguration.override_gravity().
| def pyzed.sl.write_configuration_file | ( | str | json_config_filename, |
| list | fusion_configurations, | ||
| COORDINATE_SYSTEM | coord_sys, | ||
| UNIT | unit | ||
| ) |
Write a Configuration JSON file to configure a fusion process.
| json_config_filename | : The name of the JSON that will contain the information. |
| conf | A list of FusionConfiguration listing all the camera configurations. |
| coord_sys | : The COORDINATE_SYSTEM in which the World Pose is. |
| unit | : The UNIT in which the World Pose is. |
Referenced by FusionConfiguration.override_gravity().