Structure containing information of a single camera (serial number, model, input type, etc.) More...
Data Fields | |
unsigned int | serial_number |
enum SL_MODEL | camera_model |
enum SL_INPUT_TYPE | input_type |
struct SL_CameraConfiguration | camera_configuration |
struct SL_SensorsConfiguration | sensors_configuration |
Structure containing information of a single camera (serial number, model, input type, etc.)
That information about the camera will be returned by sl_get_camera_information().
unsigned int SL_CameraInformation::serial_number |
< The serial number of the camera.
The model of the camera (ZED, ZED-M or ZED2).
enum SL_MODEL SL_CameraInformation::camera_model |
Input type used in SDK.
enum SL_INPUT_TYPE SL_CameraInformation::input_type |
Camera configuration as defined in CameraConfiguration.
struct SL_CameraConfiguration SL_CameraInformation::camera_configuration |
Device Sensors configuration as defined in SensorsConfiguration.