Classes | |
| class | ObjectData |
| Class containing data of a detected object such as its bounding_box, label, id and its 3D position. More... | |
| class | CustomBoxObjectData |
| Class that store externally detected objects. More... | |
| class | CustomMaskObjectData |
| Class that store externally detected objects with mask. More... | |
| class | Objects |
| Class containing the results of the object detection module. More... | |
| class | ObjectsBatch |
| Class containing batched data of a detected objects from the object detection module. More... | |
| class | AI_Model_status |
| Structure containing AI model status. More... | |
| class | BatchParameters |
| Structure containing a set of parameters for batch object detection. More... | |
| class | ObjectDetectionParameters |
| Structure containing a set of parameters for the object detection module. More... | |
| class | ObjectTrackingParameters |
| Structure containing a set of parameters for the object tracking module. More... | |
| class | ObjectDetectionRuntimeParameters |
| Structure containing a set of runtime parameters for the object detection module. More... | |
| class | CustomObjectDetectionProperties |
| Structure containing a set of runtime properties of a certain class ID for the object detection module using a custom model. More... | |
| class | CustomObjectDetectionRuntimeParameters |
| Structure containing a set of runtime parameters for the object detection module using your own model ran by the SDK. More... | |
Enumerations | |
| enum class | OBJECT_DETECTION_MODEL |
| Lists available models for the object detection module. More... | |
| enum class | AI_MODELS |
| Lists available AI models. More... | |
| enum class | OBJECT_CLASS |
| Lists available object classes. More... | |
| enum class | OBJECT_SUBCLASS |
| List available object subclasses. More... | |
| enum class | OBJECT_TRACKING_STATE |
| Lists the different states of object tracking. More... | |
| enum class | OBJECT_ACTION_STATE |
| Lists the different states of an object's actions. More... | |
| enum class | OBJECT_FILTERING_MODE |
| Lists supported bounding box preprocessing. More... | |
| enum class | OBJECT_ACCELERATION_PRESET |
| Lists of supported presets for maximum acceleration allowed for a given tracked object. More... | |
Functions | |
| AI_Model_status | checkAIModelStatus (AI_MODELS model, int gpu_id=0) |
| Checks if a corresponding optimized engine is found for the requested Model based on your rig configuration. More... | |
| ERROR_CODE | downloadAIModel (sl::AI_MODELS model, int gpu_id=0) |
| Downloads the requested model. More... | |
| ERROR_CODE | optimizeAIModel (sl::AI_MODELS model, int gpu_id=0) |
| Optimizes the requested model (and download the model if it is not present on the host). More... | |
| ERROR_CODE | optimizeCustomAIModel (const String &custom_onnx_file, Resolution custom_onnx_dynamic_input_shape=Resolution(512, 512), int gpu_id=0) |
| Optimizes a custom object detection model ahead of time, so that Camera::enableObjectDetection() can start using it right away. More... | |
| String | generate_unique_id () |
| Generate a UUID like unique id to help identify and track AI detections. More... | |
|
strong |
Lists available models for the object detection module.
| Enumerator | |
|---|---|
| MULTI_CLASS_BOX_FAST | Any objects, bounding box based. |
| MULTI_CLASS_BOX_MEDIUM | Any objects, bounding box based, compromise between accuracy and speed. |
| MULTI_CLASS_BOX_ACCURATE | Any objects, bounding box based, more accurate but slower than the base model. |
| PERSON_HEAD_BOX_FAST | Bounding box detector specialized in person heads particularly well suited for crowded environments. The person localization is also improved. |
| PERSON_HEAD_BOX_ACCURATE | Bounding box detector specialized in person heads, particularly well suited for crowded environments. The person localization is also improved, more accurate but slower than the base model. |
| CUSTOM_BOX_OBJECTS | For external inference, using your own custom model and/or frameworks. This mode disables the internal inference engine, the 2D bounding box detection must be provided. |
| CUSTOM_YOLOLIKE_BOX_OBJECTS | For internal inference using your own custom YOLO-like model. This mode requires a onnx file to be passed in the ObjectDetectionParameters. This model will be used for inference. |
| CUSTOM_RFDETRLIKE_BOX_OBJECTS | For internal inference using your own custom RF-DETR / DETR-like model (two outputs: boxes + class logits, NMS-free). Requires a onnx file in the ObjectDetectionParameters. |
| CUSTOM_BOX_OBJECTS_AUTODETECT | For internal inference using your own custom ONNX model, auto-detecting whether it is YOLO-like or RF-DETR/DETR-like from the model output structure. Requires a onnx file. Recommended default for custom models. |
|
strong |
Lists available AI models.
| Enumerator | |
|---|---|
| MULTI_CLASS_DETECTION | |
| MULTI_CLASS_MEDIUM_DETECTION | Related to sl::OBJECT_DETECTION_MODEL::MULTI_CLASS_BOX_MEDIUM |
| MULTI_CLASS_ACCURATE_DETECTION | Related to [sl::OBJECT_DETECTION_MODEL::MULTI_CLASS_BOX_ACCURATE](OBJECT_DETECTION_MODEL) |
| HUMAN_BODY_FAST_DETECTION | Related to sl::BODY_TRACKING_MODEL::HUMAN_BODY_FAST |
| HUMAN_BODY_MEDIUM_DETECTION | Related to sl::BODY_TRACKING_MODEL::HUMAN_BODY_MEDIUM |
| HUMAN_BODY_ACCURATE_DETECTION | Related to sl::BODY_TRACKING_MODEL::HUMAN_BODY_ACCURATE |
| HUMAN_BODY_38_FAST_DETECTION | Related to sl::BODY_TRACKING_MODEL::HUMAN_BODY_FAST |
| HUMAN_BODY_38_MEDIUM_DETECTION | Related to sl::BODY_TRACKING_MODEL::HUMAN_BODY_FAST |
| HUMAN_BODY_38_ACCURATE_DETECTION | Related to sl::BODY_TRACKING_MODEL::HUMAN_BODY_FAST |
| PERSON_HEAD_DETECTION | |
| PERSON_HEAD_ACCURATE_DETECTION | Related to [sl::OBJECT_DETECTION_MODEL::PERSON_HEAD_BOX_ACCURATE](OBJECT_DETECTION_MODEL) |
| REID_ASSOCIATION | Related to sl::BatchParameters.enable |
| NEURAL_LIGHT_DEPTH | Related to sl::DEPTH_MODE::NEURAL_LIGHT |
| NEURAL_DEPTH | Related to sl::DEPTH_MODE::NEURAL |
| NEURAL_PLUS_DEPTH | Related to sl::DEPTH_MODE::NEURAL_PLUS |
| NEURAL_DEPTH_INT8 | Related to sl::DEPTH_MODE::NEURAL with sl::DEPTH_PRECISION::INT8.
|
|
strong |
Lists available object classes.
|
strong |
List available object subclasses.
Given as hint, when using object tracking an object can change of sl::OBJECT_SUBCLASS while keeping the same sl::OBJECT_CLASS (i.e.: frame n: MOTORBIKE, frame n+1: BICYCLE).
|
strong |
Lists the different states of object tracking.
| Enumerator | |
|---|---|
| OFF | The tracking is not yet initialized. |
| OK | The object is tracked. |
| SEARCHING | The object could not be detected in the image and is potentially occluded. |
| TERMINATE | This is the last searching state of the track. |
|
strong |
|
strong |
Lists supported bounding box preprocessing.
|
strong |
Lists of supported presets for maximum acceleration allowed for a given tracked object.
| AI_Model_status sl::checkAIModelStatus | ( | AI_MODELS | model, |
| int | gpu_id = 0 |
||
| ) |
Checks if a corresponding optimized engine is found for the requested Model based on your rig configuration.
| ERROR_CODE sl::downloadAIModel | ( | sl::AI_MODELS | model, |
| int | gpu_id = 0 |
||
| ) |
Downloads the requested model.
| ERROR_CODE sl::optimizeAIModel | ( | sl::AI_MODELS | model, |
| int | gpu_id = 0 |
||
| ) |
Optimizes the requested model (and download the model if it is not present on the host).
| ERROR_CODE sl::optimizeCustomAIModel | ( | const String & | custom_onnx_file, |
| Resolution | custom_onnx_dynamic_input_shape = Resolution(512, 512), |
||
| int | gpu_id = 0 |
||
| ) |
Optimizes a custom object detection model ahead of time, so that Camera::enableObjectDetection() can start using it right away.
This optimizes the given ONNX file exactly as Camera::enableObjectDetection() does when ObjectDetectionParameters::detection_model is set to OBJECT_DETECTION_MODEL::CUSTOM_YOLOLIKE_BOX_OBJECTS, OBJECT_DETECTION_MODEL::CUSTOM_RFDETRLIKE_BOX_OBJECTS or OBJECT_DETECTION_MODEL::CUSTOM_BOX_OBJECTS_AUTODETECT, and saves the result for re-use. Optimizing a model can take several minutes, so this is meant to be called once when installing or deploying your application, rather than on its critical path.
| custom_onnx_file | : Path to the ONNX file to optimize. Use the same value as ObjectDetectionParameters::custom_onnx_file. |
| custom_onnx_dynamic_input_shape | : Input resolution to optimize the model for. Use the same value as ObjectDetectionParameters::custom_onnx_dynamic_input_shape, otherwise the optimized model cannot be re-used and the model is optimized again at runtime. |
| gpu_id | : ID of the GPU on which the model will run. The optimized model is specific to it. |
| String sl::generate_unique_id | ( | ) |
Generate a UUID like unique id to help identify and track AI detections.