All Classes Namespaces Functions Variables Typedefs Enumerations Enumerator Modules Pages
Depth Sensing Module

Classes

struct  RuntimeParameters
 Structure containing parameters that defines the behavior of sl::Camera::grab(). More...
 
struct  CameraParameters
 Structure containing the intrinsic parameters of a camera. More...
 
struct  CalibrationParameters
 Structure containing intrinsic and extrinsic parameters of the camera (translation and rotation). More...
 

Enumerations

enum class  DEPTH_MODE
 Lists available depth computation modes. More...
 
enum class  MEASURE
 Lists retrievable measures. More...
 
enum class  REGION_OF_INTEREST_AUTO_DETECTION_STATE
 Lists the different states of region of interest auto detection. More...
 

Enumeration Type Documentation

◆ DEPTH_MODE

enum DEPTH_MODE
strong

Lists available depth computation modes.

Enumerator
NONE 

No depth map computation.
Only rectified stereo images will be available.

PERFORMANCE 

Computation mode optimized for speed.

QUALITY 

Computation mode designed for challenging areas with untextured surfaces.

ULTRA 

Computation mode that favors edges and sharpness.
Requires more GPU memory and computation power.

NEURAL 

End to End Neural disparity estimation.
Requires AI module.

NEURAL_PLUS 

More accurate Neural disparity estimation.
Requires AI module.

◆ MEASURE

enum MEASURE
strong

Lists retrievable measures.

Enumerator
DISPARITY 

Disparity map. Each pixel contains 1 float.
Type: sl::MAT_TYPE::F32_C1

DEPTH 

Depth map in sl::UNIT defined in sl::InitParameters.coordinate_units. Each pixel contains 1 float.
Type: sl::MAT_TYPE::F32_C1.

CONFIDENCE 

Certainty/confidence of the depth map. Each pixel contains 1 float.
Type: sl::MAT_TYPE::F32_C1

XYZ 

Point cloud. Each pixel contains 4 float (X, Y, Z, not used).
Type: sl::MAT_TYPE::F32_C4

XYZRGBA 

Colored point cloud. Each pixel contains 4 float (X, Y, Z, color).
The color should to be read as an unsigned char[4] representing the RGBA color.
Type: sl::MAT_TYPE::F32_C4

XYZBGRA 

Colored point cloud. Each pixel contains 4 float (X, Y, Z, color).
The color should to be read as an unsigned char[4] representing the BGRA color.
Type: sl::MAT_TYPE::F32_C4

XYZARGB 

Colored point cloud. Each pixel contains 4 float (X, Y, Z, color).
The color should to be read as an unsigned char[4] representing the ARGB color.
Type: sl::MAT_TYPE::F32_C4

XYZABGR 

Colored point cloud. Each pixel contains 4 float (X, Y, Z, color).
The color should to be read as an unsigned char[4] representing the ABGR color.
Type: sl::MAT_TYPE::F32_C4

NORMALS 

Normal vectors map. Each pixel contains 4 float (X, Y, Z, 0).
Type: sl::MAT_TYPE::F32_C4.

DISPARITY_RIGHT 

Disparity map for right sensor. Each pixel contains 1 float.
Type: sl::MAT_TYPE::F32_C1.

DEPTH_RIGHT 

Depth map for right sensor. Each pixel contains 1 float.
Type: sl::MAT_TYPE::F32_C1.

XYZ_RIGHT 

Point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, not used).
Type: sl::MAT_TYPE::F32_C4

XYZRGBA_RIGHT 

Colored point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, color).
The color should to be read as an unsigned char[4] representing the RGBA color.
Type: sl::MAT_TYPE::F32_C4

XYZBGRA_RIGHT 

Colored point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, color).
The color should to be read as an unsigned char[4] representing the BGRA color.
Type: sl::MAT_TYPE::F32_C4

XYZARGB_RIGHT 

Colored point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, color).
The color should to be read as an unsigned char[4] representing the ARGB color.
Type: sl::MAT_TYPE::F32_C4

XYZABGR_RIGHT 

Colored point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, color).
The color should to be read as an unsigned char[4] representing the ABGR color.
Type: sl::MAT_TYPE::F32_C4

NORMALS_RIGHT 

Normal vectors map for right view. Each pixel contains 4 float (X, Y, Z, 0).
Type: sl::MAT_TYPE::F32_C4.

DEPTH_U16_MM 

Depth map in millimeter whatever the sl::UNIT defined in sl::InitParameters.coordinate_units.
Invalid values are set to 0 and depth values are clamped at 65000.
Each pixel contains 1 unsigned short.
Type: sl::MAT_TYPE::U16_C1.

DEPTH_U16_MM_RIGHT 

Depth map in millimeter for right sensor. Each pixel contains 1 unsigned short.
Type: sl::MAT_TYPE::U16_C1.

◆ REGION_OF_INTEREST_AUTO_DETECTION_STATE

Lists the different states of region of interest auto detection.

Enumerator
RUNNING 

The region of interest auto detection is initializing.

READY 

The region of interest mask is ready, if auto_apply was enabled, the region of interest mask is being used

NOT_ENABLED 

The region of interest auto detection is not enabled