Video Module

Classes

class  MODEL
 Lists compatible ZED Camera model. More...
 
class  INPUT_TYPE
 Lists available input type in SDK. More...
 
class  CAMERA_STATE
 List of possible camera states. More...
 
class  DeviceProperties
 Properties of a camera. More...
 
class  SIDE
 Defines left, right, both to distinguish between left and right or both sides. More...
 
class  VIDEO_SETTINGS
 Lists available camera settings for the ZED camera (contrast, hue, saturation, gain...). More...
 
class  VIEW
 Lists available views. More...
 
class  TIME_REFERENCE
 Lists specific and particular timestamps. More...
 
class  SVO_COMPRESSION_MODE
 Lists available compression modes for SVO recording. More...
 
class  FLIP_MODE
 Gives the camera flip mode. More...
 
class  CameraInformation
 Structure containing information of a single camera (serial number, model, calibration, etc.)That information about the camera will be returned by Camera.get_camera_information() More...
 
class  InputType
 Defines the input type used in the ZED SDK. More...
 
class  InitParameters
 Holds the options used to initialize the Camera object. More...
 
class  STREAMING_CODEC
 List of possible camera states. More...
 
class  StreamingProperties
 Properties of all streaming devices. More...
 
class  StreamingParameters
 Sets the streaming parameters. More...
 
class  RecordingParameters
 Sets the recording parameters. More...
 
class  RecordingStatus
 Recording structure that contains information about SVO. More...
 
class  Camera
 This class is the main interface with the camera and the SDK features, such as: video, depth, tracking, mapping, and more. More...
 

Functions

def get_resolution (resolution)
 Returns the actual size of the given RESOLUTION as a sl.Resolution object. More...
 

Function Documentation

◆ get_resolution()

def pyzed.sl.get_resolution (   resolution)

Returns the actual size of the given RESOLUTION as a sl.Resolution object.

Parameters
resolution: the given RESOLUTION