Classes | |
| class | RuntimeParameters | 
| Parameters that defines the behavior of the grab.  More... | |
| struct | CameraParameters | 
| Intrinsic parameters of a camera.  More... | |
| struct | CalibrationParameters | 
| Intrinsic and Extrinsic parameters of the camera (translation and rotation).  More... | |
Enumerations | |
| enum class | DEPTH_MODE | 
| Lists available depth computation modes.  More... | |
| enum class | SENSING_MODE | 
| Lists available depth sensing modes.  More... | |
| enum class | MEASURE | 
| Lists retrievable measures.  More... | |
      
  | 
  strong | 
Lists available depth computation modes.
      
  | 
  strong | 
Lists available depth sensing modes.
      
  | 
  strong | 
Lists retrievable measures.
| Enumerator | |
|---|---|
| DISPARITY | Disparity map. Each pixel contains 1 float. sl::MAT_TYPE::F32_C1.  | 
| DEPTH | Depth map. In sl::UNIT defined in sl::InitParameters. Each pixel contains 1 float. sl::MAT_TYPE::F32_C1.  | 
| CONFIDENCE | Certainty/confidence of the depth map. Each pixel contains 1 float. sl::MAT_TYPE::F32_C1.  | 
| XYZ | Point cloud. Each pixel contains 4 float (X, Y, Z, not used). sl::MAT_TYPE::F32_C4.  | 
| XYZRGBA | Colored point cloud. Each pixel contains 4 float (X, Y, Z, color). The color need to be read as an unsigned char[4] representing the RGBA color. sl::MAT_TYPE::F32_C4.  | 
| XYZBGRA | Colored point cloud. Each pixel contains 4 float (X, Y, Z, color). The color need to be read as an unsigned char[4] representing the BGRA color. sl::MAT_TYPE::F32_C4.  | 
| XYZARGB | Colored point cloud. Each pixel contains 4 float (X, Y, Z, color). The color need to be read as an unsigned char[4] representing the ARGB color. sl::MAT_TYPE::F32_C4.  | 
| XYZABGR | Colored point cloud. Each pixel contains 4 float (X, Y, Z, color). The color need to be read as an unsigned char[4] representing the ABGR color. sl::MAT_TYPE::F32_C4.  | 
| NORMALS | Normals vector. Each pixel contains 4 float (X, Y, Z, 0). sl::MAT_TYPE::F32_C4.  | 
| DISPARITY_RIGHT | Disparity map for right sensor. Each pixel contains 1 float. sl::MAT_TYPE::F32_C1.  | 
| DEPTH_RIGHT | Depth map for right sensor. Each pixel contains 1 float. sl::MAT_TYPE::F32_C1.  | 
| XYZ_RIGHT | Point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, not used). sl::MAT_TYPE::F32_C4.  | 
| XYZRGBA_RIGHT | Colored point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, color). The color need to be read as an unsigned char[4] representing the RGBA color. sl::MAT_TYPE::F32_C4.  | 
| XYZBGRA_RIGHT | Colored point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, color). The color need to be read as an unsigned char[4] representing the BGRA color. sl::MAT_TYPE::F32_C4.  | 
| XYZARGB_RIGHT | Colored point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, color). The color need to be read as an unsigned char[4] representing the ARGB color. sl::MAT_TYPE::F32_C4.  | 
| XYZABGR_RIGHT | Colored point cloud for right sensor. Each pixel contains 4 float (X, Y, Z, color). The color need to be read as an unsigned char[4] representing the ABGR color. sl::MAT_TYPE::F32_C4.  | 
| NORMALS_RIGHT | Normals vector for right view. Each pixel contains 4 float (X, Y, Z, 0). sl::MAT_TYPE::F32_C4.  | 
| DEPTH_U16_MM | Depth map in millimeter whatever the sl::UNIT defined in sl::InitParameters. Invalid values are set to 0, depth values are clamped at 65000. Each pixel contains 1 unsigned short. sl::MAT_TYPE::U16_C1.  | 
| DEPTH_U16_MM_RIGHT | Depth map in millimeter for right sensor. Each pixel contains 1 unsigned short. sl::MAT_TYPE::U16_C1.  |