Classes | |
| struct | SensorsData |
| Structure containing all sensors data (except image sensors) to be used for positional tracking or environment study. More... | |
| struct | SensorsData::BarometerData |
| Structure containing data from the barometer sensor. More... | |
| struct | SensorsData::TemperatureData |
| Structure containing data from the temperature sensors. More... | |
| struct | SensorsData::MagnetometerData |
| Structure containing data from the magnetometer sensor. More... | |
| struct | SensorsData::IMUData |
| Structure containing data from the IMU sensor. More... | |
| struct | SensorParameters |
| Structure containing information about a single sensor available in the current device. More... | |
| struct | SensorsConfiguration |
| Structure containing information about all the sensors available in the current device. More... | |
| class | GNSSData |
| Class containing GNSS data to be used for positional tracking as prior. More... | |
| class | FusedPositionalTrackingStatus |
| Class containing the overall position fusion status. More... | |
Enumerations | |
| enum class | SENSOR_TYPE |
| Lists available sensor types. More... | |
| enum class | SENSORS_UNIT |
| Lists available measurement units of onboard sensors. More... | |
| enum class | CAMERA_MOTION_STATE |
| Lists different states of the camera motion. More... | |
| enum class | GNSS_STATUS |
| Class representing the status of the of GNSS signal. More... | |
| enum class | GNSS_MODE |
| Class representing the mode of GNSS signal. More... | |
| enum class | GNSS_FUSION_STATUS |
| Class containing the current GNSS fusion status. More... | |
|
strong |
Lists available sensor types.
|
strong |
Lists available measurement units of onboard sensors.
| Enumerator | |
|---|---|
| M_SEC_2 | m/s² (acceleration) |
| DEG_SEC | deg/s (angular velocity) |
| U_T | μT (magnetic field) |
| HPA | hPa (atmospheric pressure) |
| CELSIUS | °C (temperature) |
| HERTZ | Hz (frequency) |
|
strong |
|
strong |
|
strong |
Class representing the mode of GNSS signal.
|
strong |
Class containing the current GNSS fusion status.