Classes | |
| class | SpatialMappingParameters |
| Sets the spatial mapping parameters. More... | |
| class | MeshFilterParameters |
| Defines the behavior of the sl::Mesh::filter function. More... | |
| class | Chunk |
| Represents a sub-mesh, it contains local vertices and triangles. More... | |
| class | Mesh |
| A mesh contains the geometric (and optionally texture) data of the scene captured by spatial mapping. More... | |
| class | PointCloudChunk |
| Represents a sub fused point cloud, it contains local vertices and colors. More... | |
| class | FusedPointCloud |
| A fused point cloud contains both geometric and color data of the scene captured by spatial mapping. More... | |
Enumerations | |
| enum class | AREA_EXPORTING_STATE |
| Lists the different states of spatial memory area export. More... | |
| enum class | SPATIAL_MAPPING_STATE |
| Gives the spatial mapping state. More... | |
| enum class | SPATIAL_MAP_TYPE |
| Lists the types of spatial maps that can be created. More... | |
| enum class | MAPPING_RESOLUTION |
| Lists the spatial mapping resolution presets. More... | |
| enum class | MAPPING_RANGE |
| Lists the spatial mapping depth range presets. More... | |
| enum class | MESH_FILE_FORMAT |
| Lists available mesh file formats. More... | |
| enum class | MESH_TEXTURE_FORMAT |
| Lists available mesh texture formats. More... | |
|
strong |
Lists the different states of spatial memory area export.
|
strong |
Gives the spatial mapping state.
| Enumerator | |
|---|---|
| INITIALIZING | The spatial mapping is initializing. |
| OK | The depth and tracking data were correctly integrated in the fusion algorithm. |
| NOT_ENOUGH_MEMORY | The maximum memory dedicated to the scanning has been reach, the mesh will no longer be updated. |
| NOT_ENABLED | Camera::enableSpatialMapping() wasn't called (or the scanning was stopped and not relaunched). |
| FPS_TOO_LOW | Effective FPS is too low to give proper results for spatial mapping. Consider using PERFORMANCES parameters (DEPTH_MODE_PERFORMANCE, low camera resolution (VGA,HD720), spatial mapping low resolution) |
|
strong |
|
strong |
|
strong |
Lists the spatial mapping depth range presets.
| Enumerator | |
|---|---|
| SHORT | Only depth close to the camera will be used during spatial mapping. |
| MEDIUM | Medium depth range. |
| LONG | Takes into account objects that are far, useful for outdoor purposes. |
| AUTO | Depth range will be computed based on current Camera states and parameters. |
|
strong |
|
strong |