Structure containing all sensors data (except image sensors) to be used for positional tracking or environment study. More...
Data Fields | |
| struct SL_IMUData | imu |
| IMU data. | |
| struct SL_BarometerData | barometer |
| Barometer data. | |
| struct SL_MagnetometerData | magnetometer |
| Magnetometer data. | |
| struct SL_TemperatureData | temperature |
| Temperature data. | |
| int | camera_moving_state |
| Motion state of the camera. More... | |
| int | image_sync_trigger |
| Indicates if the Sensors data has been taken during a frame capture on sensor. More... | |
Structure containing all sensors data (except image sensors) to be used for positional tracking or environment study.
| int SL_SensorsData::camera_moving_state |
Motion state of the camera.
| int SL_SensorsData::image_sync_trigger |
Indicates if the Sensors data has been taken during a frame capture on sensor.
If the value is 1, the data has been taken during the same time than a frame has been acquired by the left sensor (the time precision is linked to the IMU rate, therefore 800Hz == 1.3ms).
If the value is 0, the data has not been taken during a frame acquisition.