Structure containing data from the IMU sensor. More...
Data Fields | |
| bool | is_available |
| Whether the IMU sensor is available in your camera. | |
| uint64_t | timestamp_ns |
| Data acquisition timestamp in nanoseconds. | |
| struct SL_Vector3 | angular_velocity |
| Gets the angular velocity vector of the gyroscope in deg/s. More... | |
| struct SL_Vector3 | linear_acceleration |
| Linear acceleration vector (3x1) of the gyroscope in m/s². More... | |
| struct SL_Vector3 | angular_velocity_unc |
| Angular velocity vector of the gyroscope in deg/s (uncorrected from the IMU calibration). More... | |
| struct SL_Vector3 | linear_acceleration_unc |
| Linear acceleration vector of the gyroscope in m/s² (uncorrected from the IMU calibration). More... | |
| struct SL_Quaternion | orientation |
| Orientation from the IMU sensor. | |
| struct SL_Matrix3f | orientation_covariance |
| Covariance matrix of the orientation from the IMU sensor (orientation). | |
| struct SL_Matrix3f | angular_velocity_convariance |
| Covariance matrix of the angular velocity of the gyroscope in deg/s (angular_velocity). More... | |
| struct SL_Matrix3f | linear_acceleration_convariance |
| Covariance matrix of the linear acceleration of the gyroscope in m/s² (linear_acceleration). More... | |
Structure containing data from the IMU sensor.
| struct SL_Vector3 SL_IMUData::angular_velocity |
Gets the angular velocity vector of the gyroscope in deg/s.
The value is corrected from bias, scale and misalignment.
| struct SL_Vector3 SL_IMUData::linear_acceleration |
Linear acceleration vector (3x1) of the gyroscope in m/s².
The value is corrected from bias, scale and misalignment.
| struct SL_Vector3 SL_IMUData::angular_velocity_unc |
Angular velocity vector of the gyroscope in deg/s (uncorrected from the IMU calibration).
| struct SL_Vector3 SL_IMUData::linear_acceleration_unc |
Linear acceleration vector of the gyroscope in m/s² (uncorrected from the IMU calibration).
| struct SL_Matrix3f SL_IMUData::angular_velocity_convariance |
Covariance matrix of the angular velocity of the gyroscope in deg/s (angular_velocity).
| struct SL_Matrix3f SL_IMUData::linear_acceleration_convariance |
Covariance matrix of the linear acceleration of the gyroscope in m/s² (linear_acceleration).