Structure containing data from the magnetometer sensor. More...
Data Fields | |
| bool | is_available | 
| Whether the magnetometer sensor is available in your camera.  | |
| uint64_t | timestamp_ns | 
| Data acquisition timestamp in nanoseconds.  | |
| struct SL_Vector3 | magnetic_field_c | 
| Magnetic field local vector in microtesla (μT).  More... | |
| struct SL_Vector3 | magnetic_field_unc | 
| Uncalibrated magnetic field local vector in microtesla (μT).  More... | |
| float | magnetic_heading | 
| Camera heading in degrees relative to the magnetic North Pole.  More... | |
| enum SL_HEADING_STATE | magnetic_heading_state | 
| State of magnetic_heading.  | |
| float | magnetic_heading_accuracy | 
| Accuracy of magnetic_heading measure in the range [0.0, 1.0].  More... | |
| float | effective_rate | 
| Realtime data acquisition rate in hertz (Hz).  | |
Structure containing data from the magnetometer sensor.
| struct SL_Vector3 SL_MagnetometerData::magnetic_field_c | 
Magnetic field local vector in microtesla (μT).
| struct SL_Vector3 SL_MagnetometerData::magnetic_field_unc | 
Uncalibrated magnetic field local vector in microtesla (μT).
| float SL_MagnetometerData::magnetic_heading | 
Camera heading in degrees relative to the magnetic North Pole.
| float SL_MagnetometerData::magnetic_heading_accuracy | 
Accuracy of magnetic_heading measure in the range [0.0, 1.0].