Using the Sensors API
The Sensors API lets you access sensors available on ZED depth cameras and perform a wide variety of sensor-related tasks explained below.
Getting Sensors Data #
The data from the different sensors are accessible with the SensorsData
class. The class contains raw and calibrated values of each sensor.
To retrieve sensor values synchronized with the image frames, you will need to:
- Open the camera and grab the current image.
- Get sensor data corresponding to this image using
TIME_REFERENCE::IMAGE
. - Retrieve data from the different sensors.
// Create and open the camera
Camera zed;
zed.open();
SensorsData sensors_data;
// Grab new frames and retrieve sensors data
while (zed.grab() == ERROR_CODE::SUCCESS) {
zed.getSensorsData(sensors_data, TIME_REFERENCE::IMAGE); // Get frame synchronized sensor data
// Extract multi-sensor data
imu_data = sensors_data.imu;
barometer_data = sensors_data.barometer;
magnetometer_data = sensors_data.magnetometer;
// Retrieve linear acceleration and angular velocity
float3 linear_acceleration = imu_data.linear_acceleration;
float3 angular_velocity = imu_data.angular_velocity;
// Retrieve pressure and relative altitude
float pressure = barometer_data.pressure;
float relative_altitude = barometer_data.relative_altitude;
// Retrieve magnetic field
float3 magnetic_field = magnetometer_data.magnetic_field_uncalibrated;
}
# Create and open the camera
zed = sl.Camera()
zed.open()
sensors_data = sl.SensorsData()
# Grab new frames and retrieve sensors data
while zed.grab() == sl.ERROR_CODE.SUCESS :
zed.get_sensors_data(sensors_data, sl.TIME_REFERENCE.IMAGE) # Get frame synchronized sensor data
# Extract multi-sensor data
imu_data = sensors_data.get_imu_data()
barometer_data = sensors_data.get_barometer_data()
magnetometer_data = sensors_data.get_magnetometer_data()
# Retrieve linear acceleration and angular velocity
linear_acceleration = imu_data.get_linear_acceleration()
angular_velocity = imu_data.get_angular_velocity()
# Retrieve pressure and relative altitude
pressure = barometer_data.pressure
relative_altitude = barometer_data.relative_altitude
# Retrieve magnetic field
magnetic_field = magnetometer_data.get_magnetic_field_uncalibrated()
// Create and open the camera
Camera zed = new Camera();
InitParameters init_parameters = new InitParameters();
zed.Open(ref init_parameters);
SensorsData sensors_data = new SensorsData();
RuntimeParameters runtimeParameters = new RuntimeParameters();
// Grab new frames and retrieve sensors data
while (zed.Grab(ref runtimeParameters) == ERROR_CODE.SUCCESS) {
zed.GetSensorsData(ref sensors_data, TIME_REFERENCE.IMAGE); // Get frame synchronized sensor data
// Extract multi-sensor data
imu_data = sensors_data.imu;
barometer_data = sensors_data.barometer;
magnetometer_data = sensors_data.magnetometer;
// Retrieve linear acceleration and angular velocity
float3 linear_acceleration = imu_data.linearAcceleration;
float3 angular_velocity = imu_data.angularVelocity;
// Retrieve pressure and relative altitude
float pressure = barometer_data.pressure;
float relative_altitude = barometer_data.relativeAltitude;
// Retrieve magnetic field
float3 magnetic_field = magnetometer_data.magneticFieldUncalibrated;
}
Time Reference #
The function getSensorsData
can be called with a TIME_REFERENCE
. For example, you can use TIME_REFERENCE::CURRENT
to get the sensor data corresponding to the timestamp of the function call, or TIME_REFERENCE::IMAGE
to get the data synchronized with the current camera image.
For more information on sensor time reference, read the Sensors Time Synchronization section.
Retrieve New Sensor Data #
To retrieve updated sensor data, getSensorsData
must be called at a frequency superior to or equal to the sensor data rate.
Since sensors have different frequencies and their data is stored in the same sensors_data
structure, some sensor data might not be updated between two calls to getSensorsData
.
To know if a given sensor data has been updated, we compare their timestamps which are used as unique identifiers. If they are the same, then the sensor data has not been updated.
Timestamp last_imu_ts = 0;
while (zed.grab() == ERROR_CODE::SUCCESS) {
zed.getSensorsData(sensors_data, TIME_REFERENCE::IMAGE);
// Check if a new IMU sample is available
if (sensors_data.imu.timestamp > last_imu_ts) {
cout << "Linear Acceleration: " << sensors_data.imu.linear_acceleration << endl;
cout << "Angular Velocity: " << sensors_data.imu.angular_velocity << endl;
last_imu_ts = sensors_data.imu.timestamp;
}
}
last_imu_ts = sl.Timestamp()
while zed.grab() == sl.ERROR_CODE.SUCCESS:
zed.get_sensors_data(sensors_data, sl.TIME_REFERENCE.IMAGE)
# Check if a new IMU sample is available
if sensors_data.get_imu_data().timestamp.get_seconds() > last_imu_ts.get_seconds():
print("Linear Acceleration: {}".format(sensors_data.get_imu_data().get_linear_acceleration()))
print("Angular Velocity : {}".format(sensors_data.get_imu_data().get_angular_velocity()))
last_imu_ts = sensors_data.get_imu_data().timestamp
ulong last_imu_ts = 0;
RuntimeParameters runtimeParameters = new RuntimeParameters();
while (zed.Grab(ref runtimeParameters) == ERROR_CODE.SUCCESS) {
zed.GetSensorsData(sensors_data, TIME_REFERENCE.IMAGE);
// Check if a new IMU sample is available
if (sensors_data.imu.timestamp > last_imu_ts) {
Console.WriteLine("Linear Acceleration: " + sensors_data.imu.linearAcceleration);
Console.WriteLine("Angular Velocity: " + sensors_data.imu.angularVelocity);
last_imu_ts = sensors_data.imu.timestamp;
}
}
Accessing Raw Sensor Data #
The Sensors API lets you read raw data from the depth camera’s built-in motion and position sensors. To retrieve raw data, use the uncalibrated
values present in sensors_data
structure.
Identifying Sensors Capabilities #
Sensors factory parameters can be accessed through the API. They cannot be changed as they are fixed in the microcontroller firmware of the cameras. You can access the following parameters:
- Sensor Type
- Sampling Rate
- Range
- Resolution
- Noise Density
- Random Walk (if applicable)
- Sensor Units
// Display camera information (model, serial number, firmware version)
auto info = zed.getCameraInformation();
cout << "Camera Model: " << info.camera_model << endl;
cout << "Serial Number: " << info.serial_number << endl;
cout << "Camera Firmware: " << info.camera_configuration.firmware_version << endl;
cout << "Sensors Firmware: " << info.sensors_configuration.firmware_version << endl;
// Display accelerometer sensor configuration
SensorParameters& sensor_parameters = info.sensors_configuration.accelerometer_parameters;
cout << "Sensor Type: " << sensor_parameters.type << endl;
cout << "Sampling Rate: " << sensor_parameters.sampling_rate << endl;
cout << "Range: " << sensor_parameters.range << endl;
cout << "Resolution: " << sensor_parameters.resolution << endl;
if (isfinite(sensor_parameters.noise_density)) cout << "Noise Density: " << sensor_parameters.noise_density << endl;
if (isfinite(sensor_parameters.random_walk)) cout << "Random Walk: " << sensor_parameters.random_walk << endl;
# Display camera information (model, serial number, firmware version)
info = zed.get_camera_information()
print("Camera model: {}".format(info.camera_model))
print("Serial Number: {}".format(info.serial_number))
print("Camera Firmware: {}".format(info.camera_configuration.firmware_version))
print("Sensors Firmware: {}".format(info.sensors_configuration.firmware_version))
# Display accelerometer sensor configuration
sensor_parameters = info.sensors_configuration.accelerometer_parameters
print("Sensor Type: {}".format(sensor_parameters.sensor_type))
print("Sampling Rate: {}".format(sensor_parameters.sampling_rate))
print("Range: {}".format(sensor_parameters.sensor_range))
print("Resolution: {}".format(sensor_parameters.resolution))
import math
if math.isfinite(sensor_parameters.noise_density):
print("Noise Density: {}".format(sensor_parameters.noise_density))
if math.isfinite(sensor_parameters.random_walk):
print("Random Walk: {}".format(sensor_parameters.random_walk))
// Display camera information (model, serial number, firmware version)
Console.WriteLine("Camera Model: " + zed.GetCameraModel());
Console.WriteLine("Serial Number: " + zed.GetZEDSerialNumber());
Console.WriteLine("Camera Firmware: " + zed.GetCameraFirmwareVersion());
Console.WriteLine("Sensors Firmware: " + zed.GetSensorsFirmwareVersion());
// Display accelerometer sensor configuration
SensorParameters sensorParams = new SensorParameters();
sensorParams = zed.GetSensorsConfiguration().accelerometer_parameters;
Console.WriteLine("Sensor type: " + sensorParams.type);
Console.WriteLine("Sampling Rate: " + sensorParams.sampling_rate);
Console.WriteLine("Range:" + sensorParams.range.x + " / " + sensorParams.range.y);
Console.WriteLine("Resolution: " + sensorParams.resolution);
if (!float.IsInfinity(sensorParams.noise_density)) Console.WriteLine("Noise Density: " + sensorParams.noise_density);
if (!float.IsInfinity(sensorParams.random_walk)) Console.WriteLine("Random Walk: " + sensorParams.random_walk);
Code Example #
For a code example, check out the Getting Sensor Data tutorial.