GStreamer - ZED Object Detection Overlay

Open in ClaudeOpen in ChatGPT

The ZED Object Detection Overlay, zedodoverlay GStreamer element, is a transform filter that allows drawing object detection bounding boxes on a ZED left color video stream. The incoming data stream must contain ZED Metadata. You can use the zeddatamux element to add back metadata to a ZED video stream in case a GStreamer filter removes them.

OD Multi class overlay road

The source code of this plugin is a complete example of how to process the ZED metadata in a GStreamer element to retrieve object detection data.

Properties

No properties

Example pipelines

Display Object Detection bounding boxes

The following is a pipeline to acquire a stream at 720p resolution with RGB and MULTI CLASS Object Detection information and display the results on screen:

gst-launch-1.0 zedsrc stream-type=0 od-enabled=true od-detection-model=0 camera-resolution=3 camera-fps=30 ! queue ! \
zedodoverlay ! queue ! autovideoconvert ! fpsdisplaysink

image

OD Multi class overlay bridge

Display Skeleton Tracking results

The same pipeline of the previous example can be used to display Skeleton Tracking results by simply changing the bt-detection-model property of the zedsrc element

gst-launch-1.0 zedsrc stream-type=0 bt-enabled=true bt-detection-model=2 camera-resolution=3 camera-fps=30 ! queue ! \
zedodoverlay ! queue ! autovideoconvert ! fpsdisplaysink

image

OD Skeleton overlay