Classes | |
class | DETECTION_MODEL |
Lists available models for detection. More... | |
class | OBJECT_FILTERING_MODE |
Lists available filtering mode for object detection/tracking. More... | |
class | OBJECT_CLASS |
Lists available object classes. More... | |
class | OBJECT_SUBCLASS |
Available object subclass, given as hint, when using object tracking an object can change of OBJECT_SUBCLASS while keeping the same OBJECT_CLASS (i.e: frame M: MOTORBIKE, frame N:BICYCLE) More... | |
class | OBJECT_TRACKING_STATE |
Lists available object tracking states. More... | |
class | OBJECT_ACTION_STATE |
Lists available object action states. More... | |
class | ObjectData |
Contains data of a detected object such as its bounding_box, label, id and its 3D position. More... | |
class | CustomBoxObjectData |
Container to store the externally detected objects. More... | |
class | BODY_PARTS |
Semantic of human body parts and order of sl.ObjectData.keypoint for sl.BODY_FORMAT.POSE_18. More... | |
class | BODY_PARTS_POSE_34 |
Semantic of human body parts and order of sl.ObjectData.keypoint for sl.BODY_FORMAT.POSE_32. More... | |
class | BODY_FORMAT |
List of supported skeleton body model. More... | |
class | ObjectsBatch |
Contains batched data of a detected object. More... | |
class | Objects |
Contains the result of the object detection module. More... | |
class | BatchParameters |
Sets batch trajectory parametersThe default constructor sets all parameters to their default settings. More... | |
class | ObjectDetectionParameters |
Sets the object detection parameters. More... | |
class | ObjectDetectionRuntimeParameters |
Sets the object detection runtime parameters. More... | |
Functions | |
def | generate_unique_id () |
Generates a UUID like unique ID to help identify and track AI detections. | |
def | get_idx (BODY_PARTS part) |
Returns the associated index for a given BODY_PARTS. | |
def | get_idx_34 (BODY_PARTS_POSE_34 part) |
Returns the associated index for a given BODY_PARTS_POSE_34. | |
Variables | |
BODY_PARTS_POSE_18 = BODY_PARTS | |
Equivalent to BODY_PARTS. More... | |
list | BODY_BONES |
Links of human body keypoints for sl.BODY_FORMAT.POSE_18, useful for display. | |
list | BODY_BONES_POSE_34 |
Links of human body keypoints for sl.BODY_FORMAT.POSE_34, useful for display. | |
BODY_PARTS_POSE_18 = BODY_PARTS |
Equivalent to BODY_PARTS.
Added in SDK 3.6 for compatibility with previous versions.