Data Fields | |
| unsigned char | ip [16] |
| unsigned short | port |
| unsigned int | serial_number |
| int | current_bitrate |
| enum SL_STREAMING_CODEC | codec |
| unsigned char SL_StreamingProperties::ip[16] |
the streaming IP of the device
| unsigned short SL_StreamingProperties::port |
the streaming port
| unsigned int SL_StreamingProperties::serial_number |
the serial number of the streaming device
| int SL_StreamingProperties::current_bitrate |
the current bitrate of encoding of the streaming device
| enum SL_STREAMING_CODEC SL_StreamingProperties::codec |
the current codec used for compression in streaming device