Sets the recording parameters. More...
Data Fields | |
unsigned char | video_filename [256] |
filename of the SVO file. | |
enum SL_SVO_COMPRESSION_MODE | compression_mode |
can be one of the SL_SVO_COMPRESSION_MODE enum | |
unsigned int | bitrate |
overrides default bitrate of the SVO file, in KBits/s. Only works if SVO_COMPRESSION_MODE is H264 or H265. default : 0 means default values (depends on the resolution) More... | |
unsigned int | target_framerate |
defines the target framerate for the recording module. More... | |
bool | transcode_streaming_input |
In case of streaming input, if set to false, it will avoid decoding/re-encoding and convert directly streaming input into a SVO file. This saves a encoding session and can be especially useful on NVIDIA Geforce cards where the number of encoding session is limited. More... | |
Sets the recording parameters.
unsigned int SL_RecordingParameters::bitrate |
overrides default bitrate of the SVO file, in KBits/s. Only works if SVO_COMPRESSION_MODE is H264 or H265.
default : 0 means default values (depends on the resolution)
unsigned int SL_RecordingParameters::target_framerate |
defines the target framerate for the recording module.
bool SL_RecordingParameters::transcode_streaming_input |
In case of streaming input, if set to false, it will avoid decoding/re-encoding and convert directly streaming input into a SVO file. This saves a encoding session and can be especially useful on NVIDIA Geforce cards where the number of encoding session is limited.