Classes | |
class | GNSS_STATUS |
Lists that represents the status of the of GNSS signal. More... | |
class | GNSS_MODE |
Lists that represents the mode of GNSS signal. More... | |
class | GNSS_FUSION_STATUS |
Lists that represents the current GNSS fusion status. More... | |
class | SENSOR_TYPE |
Lists available sensor types. More... | |
class | SENSORS_UNIT |
Lists available measurement units of onboard sensors. More... | |
class | SensorParameters |
Class containing information about a single sensor available in the current device. More... | |
class | SensorsConfiguration |
Class containing information about all the sensors available in the current device. More... | |
class | CAMERA_MOTION_STATE |
Lists different states of the camera motion. More... | |
class | SENSOR_LOCATION |
Lists possible locations of temperature sensors. More... | |
class | BarometerData |
Class containing data from the barometer sensor. More... | |
class | TemperatureData |
Class containing data from the temperature sensors. More... | |
class | HEADING_STATE |
Lists the different states of the magnetic heading. More... | |
class | MagnetometerData |
Class containing data from the magnetometer sensor. More... | |
class | SensorsData |
Class containing all sensors data (except image sensors) to be used for positional tracking or environment study. More... | |
class | IMUData |
Class containing data from the IMU sensor. More... | |
class | GNSSData |
Class containing GNSS data to be used for positional tracking as prior. More... | |