Positional Tracking Module

Classes

class  PositionalTrackingParameters
 Structure containing a set of parameters for the positional tracking module initialization. More...
 
class  Rotation
 Class representing a rotation for the positional tracking module. More...
 
class  Translation
 Class representing a translation for the positional tracking module. More...
 
class  Orientation
 Class representing an orientation/quaternion for the positional tracking module. More...
 
class  Transform
 Class representing a transformation (translation and rotation) for the positional tracking module. More...
 
class  Pose
 Class containing positional tracking data giving the position and orientation of the camera in 3D space. More...
 
class  Landmark
 Represents a 3d landmark. More...
 
class  Landmark2D
 Represents the projection of a 3d landmark in the image. More...
 
class  KeyFrame
 Represents a keyframe in the tracking system. More...
 
class  PositionalTrackingStatus
 Lists the different status of positional tracking. More...
 
class  GNSSData
 Class containing GNSS data to be used for positional tracking as prior. More...
 
class  FusedPositionalTrackingStatus
 Class containing the overall position fusion status. More...
 

Enumerations

enum class  POSITIONAL_TRACKING_MODE
 Lists the mode of positional tracking that can be used. More...
 
enum class  AREA_EXPORTING_STATE
 Lists the different states of spatial memory area export. More...
 
enum class  REFERENCE_FRAME
 Lists possible types of position matrix used to store camera path and pose. More...
 
enum class  POSITIONAL_TRACKING_STATE
 Lists the different states of positional tracking. More...
 
enum class  ODOMETRY_STATUS
 Report the status of current odom tracking. More...
 
enum class  SPATIAL_MEMORY_STATUS
 Report the status of current map tracking. More...
 
enum class  POSITIONAL_TRACKING_FUSION_STATUS
 Report the status of the positional tracking fusion. More...
 
enum class  GNSS_STATUS
 Class representing the status of the of GNSS signal. More...
 
enum class  GNSS_MODE
 Class representing the mode of GNSS signal. More...
 
enum class  GNSS_FUSION_STATUS
 Class containing the current GNSS fusion status. More...
 

Enumeration Type Documentation

◆ POSITIONAL_TRACKING_MODE

Lists the mode of positional tracking that can be used.

Enumerator
GEN_1 

Default mode. Fast and stable mode. Requires depth computation. Less robust than GEN_3

GEN_2 
Deprecated:
GEN_3 

Fast and accurate, in both exploratory mode and mapped environments.\Note Can be used even if depth_mode is set to DEPTH_MODE::NONE.

◆ AREA_EXPORTING_STATE

enum AREA_EXPORTING_STATE
strong

Lists the different states of spatial memory area export.

Enumerator
SUCCESS 

The spatial memory file has been successfully created.

RUNNING 

The spatial memory is currently being written.

NOT_STARTED 

The spatial memory file exportation has not been called.

FILE_EMPTY 

The spatial memory contains no data, the file is empty.

FILE_ERROR 

The spatial memory file has not been written because of a wrong file name.

SPATIAL_MEMORY_DISABLED 

The spatial memory learning is disabled. No file can be created.

◆ REFERENCE_FRAME

enum REFERENCE_FRAME
strong

Lists possible types of position matrix used to store camera path and pose.

Enumerator
WORLD 

The transform of sl::Pose will contain the motion with reference to the world frame (previously called PATH).

CAMERA 

The transform of sl::Pose will contain the motion with reference to the previous camera frame (previously called POSE).

◆ POSITIONAL_TRACKING_STATE

Lists the different states of positional tracking.

Enumerator
SEARCHING 

\warn DEPRECATED: This state is no longer in use.

OK 

The positional tracking is functioning normally.

OFF 

The positional tracking is currently disabled.

FPS_TOO_LOW 

The effective FPS is too low to provide accurate motion tracking results. Consider adjusting performance parameters (e.g., depth mode, camera resolution) to improve tracking quality.

SEARCHING_FLOOR_PLANE 

The camera is currently searching for the floor plane to establish its position relative to it. The world reference frame will be set afterward.

UNAVAILABLE 

The tracking module was unable to perform tracking from the previous frame to the current frame.

◆ ODOMETRY_STATUS

enum ODOMETRY_STATUS
strong

Report the status of current odom tracking.

Enumerator
OK 

The positional tracking module successfully tracked from the previous frame to the current frame.

UNAVAILABLE 

The positional tracking module cannot track the current frame.

INSUFFICIENT_FEATURES 

The positional tracking failed to track the current frame because it could not find enought features.

LAST 

◆ SPATIAL_MEMORY_STATUS

enum SPATIAL_MEMORY_STATUS
strong

Report the status of current map tracking.

Enumerator
OK 

Deprecated: This state is no longer in use for GEN_3.

LOOP_CLOSED 

Displayed whenever the system has found a loop closure, relocalized within the area map or corrected after a sudden localization loss.

SEARCHING 

Deprecated: This state is no longer in use for GEN_3.

OFF 

Displayed when the spatial memory is turned off.

INITIALIZING 

Displayed until the cameras has acquired enough memory (Initial Area Mapping) or has found its first loop closure and is localized in the loaded area map (Lifelong Mapping/Localization). Users need to keep moving the camera for it to get updated.

KNOWN_MAP 

Displayed when the camera is localized within the loaded area map.

MAP_UPDATE 

Displayed when the robot is mapping (Initial Area Mapping) or when the robot is getting out of the area map bounds (Lifelong Mapping). Displayed as “Tracking” when in exploratory mode with SLAM engaged.

LOST 

Displayed when localization cannot operate anymore (camera completely obstructed, sudden localization jumps after being localized) in Mapping/ Localization modes. It can also include the case where the camera jumps or is located out of map bounds in Localization mode. This should be an indicator for users to stop the robot.

NOT_ENOUGH_MEMORY_FOR_TRACKING 

Displayed when there is not enough memory to continue tracking.

LAST 

◆ POSITIONAL_TRACKING_FUSION_STATUS

Report the status of the positional tracking fusion.

Enumerator
VISUAL_INERTIAL 
VISUAL 
INERTIAL 
GNSS 
VISUAL_INERTIAL_GNSS 
VISUAL_GNSS 
INERTIAL_GNSS 
UNAVAILABLE 
LAST 

◆ GNSS_STATUS

enum GNSS_STATUS
strong

Class representing the status of the of GNSS signal.

Enumerator
UNKNOWN 

No GNSS fix data is available.

SINGLE 

Single Point Positioning.

DGNSS 

Differential GNSS.

PPS 

Precise Positioning Service.

RTK_FLOAT 

Real Time Kinematic Float.

RTK_FIX 

Real Time Kinematic Fixed.

LAST 

◆ GNSS_MODE

enum GNSS_MODE
strong

Class representing the mode of GNSS signal.

Enumerator
UNKNOWN 

No GNSS fix data is available.

NO_FIX 

No GNSS fix is available.

FIX_2D 

2D GNSS fix, providing latitude and longitude coordinates but without altitude information.

FIX_3D 

3D GNSS fix, providing latitude, longitude, and altitude coordinates.

LAST 

◆ GNSS_FUSION_STATUS

enum GNSS_FUSION_STATUS
strong

Class containing the current GNSS fusion status.

Enumerator
OK 

The GNSS fusion module is calibrated and working successfully.

OFF 

The GNSS fusion module is not enabled.

CALIBRATION_IN_PROGRESS 

Calibration of the GNSS/VIO fusion module is in progress.

RECALIBRATION_IN_PROGRESS 

Re-alignment of GNSS/VIO data is in progress, leading to potentially inaccurate global position.

LAST