Structure containing a set of parameters for the spatial mapping module. More...
Data Fields | |
| float | resolution_meter |
| Spatial mapping resolution in meters. More... | |
| float | range_meter |
| Depth range in meters. More... | |
| bool | save_texture |
| Whether to save the texture. More... | |
| bool | use_chunk_only |
| Whether to only use chunks. More... | |
| int | max_memory_usage |
| The maximum CPU memory (in MB) allocated for the meshing process. More... | |
| bool | reverse_vertex_order |
| Whether to inverse the order of the vertices of the triangles. More... | |
| enum SL_SPATIAL_MAP_TYPE | map_type |
| The type of spatial map to be created. More... | |
| int | stability_counter |
| Control the integration rate of the current depth into the mapping process. More... | |
| float | disparity_std |
| Control the disparity noise (standard deviation) in px. set a very small value (<0.1) if the depth map of the scene is accurate. set a big value (>0.5) if the depth map is noisy. | |
| float | decay |
| Adjust the weighting factor for the current depth during the integration process. By default, the value is set to 1, which results in the complete integration and fusion of the current depth with the previously integrated depth. Setting it to 0 discards all previous data and solely integrates the current depth. | |
| bool | enable_forget_past |
| This parameter enables the forgetting of the previous map to limit memory and drift issues. It enables a local spatial mapping that only keeps a mapped scene around the current camera position. The distance threshold is set to be equal to 1.5 x the range of the spatial mapping. | |
Structure containing a set of parameters for the spatial mapping module.
The default constructor sets all parameters to their default settings.
| float SL_SpatialMappingParameters::resolution_meter |
Spatial mapping resolution in meters.
Default: 0.05f
| float SL_SpatialMappingParameters::range_meter |
Depth range in meters.
Can be different from the value set by SL_InitParameters.depth_maximum_distance.
| bool SL_SpatialMappingParameters::save_texture |
Whether to save the texture.
If set to true, you will be able to apply the texture to your mesh after it is created.
Default: false
| bool SL_SpatialMappingParameters::use_chunk_only |
Whether to only use chunks.
If set to false, you will ensure consistency between the mesh and its inner chunk data.
Default: false
| int SL_SpatialMappingParameters::max_memory_usage |
The maximum CPU memory (in MB) allocated for the meshing process.
Default: 2048
| bool SL_SpatialMappingParameters::reverse_vertex_order |
Whether to inverse the order of the vertices of the triangles.
If your display process does not handle front and back face culling, you can use this to correct it.
Default: false
| enum SL_SPATIAL_MAP_TYPE SL_SpatialMappingParameters::map_type |
The type of spatial map to be created.
This dictates the format that will be used for the mapping (e.g. mesh, point cloud).
See SL_SPATIAL_MAP_TYPE.
| int SL_SpatialMappingParameters::stability_counter |
Control the integration rate of the current depth into the mapping process.
This parameter controls how many times a stable 3D points should be seen before it is integrated into the spatial mapping.
Default: 0 (this will define the stability counter based on the mesh resolution, the higher the resolution, the higher the stability counter)