Structure containing a set of parameters for the body tracking module. More...
Data Fields | |
unsigned int | instance_module_id |
Id of the module instance. More... | |
bool | enable_tracking |
Whether the body tracking system includes body/person tracking capabilities across a sequence of images. More... | |
bool | enable_segmentation |
Whether the body/person masks will be computed. More... | |
enum SL_BODY_TRACKING_MODEL | detection_model |
SL_BODY_TRACKING_MODEL to use. More... | |
bool | enable_body_fitting |
Whether to apply the body fitting. More... | |
enum SL_BODY_FORMAT | body_format |
Body format to be outputted by the ZED SDK with sl_retrieve_bodies(). More... | |
enum SL_BODY_KEYPOINTS_SELECTION | body_selection |
Selection of keypoints to be outputted by the ZED SDK with sl_retrieve_bodies(). More... | |
float | max_range |
Upper depth range for detections. More... | |
float | prediction_timeout_s |
Prediction duration of the ZED SDK when an object is not detected anymore before switching its state to SL_OBJECT_TRACKING_STATE_SEARCHING. More... | |
bool | allow_reduced_precision_inference |
Whether to allow inference to run at a lower precision to improve runtime and memory usage. More... | |
Structure containing a set of parameters for the body tracking module.
The default constructor sets all parameters to their default settings.
unsigned int SL_BodyTrackingParameters::instance_module_id |
Id of the module instance.
This is used to identify which body tracking module instance is used.
bool SL_BodyTrackingParameters::enable_tracking |
Whether the body tracking system includes body/person tracking capabilities across a sequence of images.
Default: true
bool SL_BodyTrackingParameters::enable_segmentation |
Whether the body/person masks will be computed.
Default: false
enum SL_BODY_TRACKING_MODEL SL_BodyTrackingParameters::detection_model |
SL_BODY_TRACKING_MODEL to use.
bool SL_BodyTrackingParameters::enable_body_fitting |
Whether to apply the body fitting.
Default: false
enum SL_BODY_FORMAT SL_BodyTrackingParameters::body_format |
Body format to be outputted by the ZED SDK with sl_retrieve_bodies().
Default: SL_BODY_FORMAT_BODY_18
enum SL_BODY_KEYPOINTS_SELECTION SL_BodyTrackingParameters::body_selection |
Selection of keypoints to be outputted by the ZED SDK with sl_retrieve_bodies().
Default: SL_BODY_KEYPOINTS_SELECTION_FULL
float SL_BodyTrackingParameters::max_range |
Upper depth range for detections.
Default: -1.f (value set in SL_InitParameters.depth_maximum_distance)
float SL_BodyTrackingParameters::prediction_timeout_s |
Prediction duration of the ZED SDK when an object is not detected anymore before switching its state to SL_OBJECT_TRACKING_STATE_SEARCHING.
It prevents the jittering of the object state when there is a short misdetection.
The user can define their own prediction time duration.
Default: 0.2f
bool SL_BodyTrackingParameters::allow_reduced_precision_inference |
Whether to allow inference to run at a lower precision to improve runtime and memory usage.
It might increase the initial optimization time and could include downloading calibration data or calibration cache and slightly reduce the accuracy.