Recording structure that contains information about SVO. More...
Data Fields | |
bool | is_recording |
bool | is_paused |
bool | status |
double | current_compression_time |
double | current_compression_ratio |
double | average_compression_time |
double | average_compression_ratio |
Recording structure that contains information about SVO.
bool SL_RecordingStatus::is_recording |
< Recorder status, true if enabled Recorder status, true if the pause is enabled
bool SL_RecordingStatus::is_paused |
Status of current frame. True for success or false if the frame couldn't be written in the SVO file.
bool SL_RecordingStatus::status |
Compression time for the current frame in ms.
double SL_RecordingStatus::current_compression_time |
Compression ratio (% of raw size) for the current frame.
double SL_RecordingStatus::current_compression_ratio |
Average compression time in ms since beginning of recording.
double SL_RecordingStatus::average_compression_time |
Average compression ratio (% of raw size) since beginning of recording.