SL_BatchParameters Struct Reference

Data Fields

bool enable
 Defines if the Batch option in the object detection module is enabled. Batch queueing system provides: More...
 
float id_retention_time
 Max retention time in seconds of a detected object. After this time, the same object will mostly have a different ID.
 
float latency
 Trajectories will be output in batch with the desired latency in seconds. During this waiting time, re-identification of objects is done in the background. Specifying a short latency will limit the search ( falling in timeout) for previously seen object IDs but will be closer to real time output. Specifying a long latency will reduce the change of timeout in Re-ID but increase difference with live output.
 

Detailed Description

Set the batch trajectory parameters

Field Documentation

◆ enable

bool SL_BatchParameters::enable

Defines if the Batch option in the object detection module is enabled. Batch queueing system provides:

  • Deep-Learning based re-identification
  • Trajectory smoothing and filtering
    Note
    To activate this option, enable must be set to true.