Structure containing information about the properties of a streaming device. More...
Data Fields | |
| unsigned char | ip [16] |
| IP address of the streaming device. | |
| unsigned short | port |
| Streaming port of the streaming device. More... | |
| unsigned int | serial_number |
| Serial number of the streaming camera. More... | |
| int | current_bitrate |
| Current bitrate of encoding of the streaming device. More... | |
| enum SL_STREAMING_CODEC | codec |
| Current codec used for compression in streaming device. More... | |
Structure containing information about the properties of a streaming device.
| unsigned short SL_StreamingProperties::port |
Streaming port of the streaming device.
Default: 0
| unsigned int SL_StreamingProperties::serial_number |
Serial number of the streaming camera.
Default: 0
| int SL_StreamingProperties::current_bitrate |
Current bitrate of encoding of the streaming device.
Default: 0
| enum SL_STREAMING_CODEC SL_StreamingProperties::codec |
Current codec used for compression in streaming device.
Default: SL_STREAMING_CODEC_H265