Structure containing information about a single sensor available in the current device. More...
Data Fields | |
| enum SL_SENSOR_TYPE | type |
| Type of the sensor. | |
| float | resolution |
| Resolution of the sensor. | |
| float | sampling_rate |
| Sampling rate (or ODR) of the sensor. | |
| struct SL_Vector2 | range |
Range of the sensor (minimum: range.x, maximum: range.y). | |
| float | noise_density |
| White noise density given as continuous (frequency-independent). More... | |
| float | random_walk |
| Random walk derived from the Allan Variance given as continuous (frequency-independent). More... | |
| enum SL_SENSORS_UNIT | sensor_unit |
| Unit of the sensor. | |
| bool | is_available |
| Whether the sensor is available in your camera. | |
Structure containing information about a single sensor available in the current device.
Information about the camera sensors is available in the SL_CameraInformation struct returned by sl_get_camera_information().
| float SL_SensorParameters::noise_density |
White noise density given as continuous (frequency-independent).
sensor_unit / √(Hz).NAN if the information is not available. | float SL_SensorParameters::random_walk |
Random walk derived from the Allan Variance given as continuous (frequency-independent).
sensor_unit / √(Hz).NAN if the information is not available.