Structure containing information about the status of the recording. More...
Data Fields | |
bool | is_recording |
Report if the recording has been enabled. | |
bool | is_paused |
Report if the recording has been paused. | |
bool | status |
Status of current frame. More... | |
double | current_compression_time |
Compression time for the current frame in milliseconds. | |
double | current_compression_ratio |
Compression ratio (% of raw size) for the current frame. | |
double | average_compression_time |
Average compression time in milliseconds since beginning of recording. | |
double | average_compression_ratio |
Average compression ratio (% of raw size) since beginning of recording. | |
Structure containing information about the status of the recording.
bool SL_RecordingStatus::status |
Status of current frame.
True for success or false if the frame could not be written in the SVO file.