Structure representing a plane defined by a point and a normal, or a plane equation. More...
Data Fields | |
| int | error_code |
| SL_ERROR_CODE returned by the ZED SDK when the plane detection was attempted. | |
| enum UNITY_PLAN_TYPE | type |
| Type of the plane defined by its orientation. More... | |
| struct SL_Vector3 | plane_normal |
| Plane normalized normal vector. | |
| struct SL_Vector3 | plane_center |
| Plane center point. | |
| struct SL_Vector3 | plane_transform_position |
| Plane position relative to the global reference frame. | |
| struct SL_Quaternion | plane_transform_orientation |
| Plane orientation relative to the global reference frame. | |
| struct SL_Vector4 | plane_equation |
Plane equation coefficients {a, b, c, d}. More... | |
| struct SL_Vector2 | extents |
| Width and height of the bounding rectangle around the plane contours. | |
| int | bounds_size |
| Size of bounds. | |
| struct SL_Vector3 | bounds [256] |
| Array of 3D points forming a polygon bounds corresponding to the current visible limits of the plane. | |
Structure representing a plane defined by a point and a normal, or a plane equation.
| enum UNITY_PLAN_TYPE SL_PlaneData::type |
Type of the plane defined by its orientation.
| struct SL_Vector4 SL_PlaneData::plane_equation |
Plane equation coefficients {a, b, c, d}.
ax + by + cz = d.