Structure containing the results of the object detection module. More...
Data Fields | |
| int | nb_objects | 
| Number of detected objects.  More... | |
| uint64_t | timestamp | 
| Timestamp corresponding to the frame acquisition.  More... | |
| int | is_new | 
| Whether object_list has already been retrieved or not.  | |
| int | is_tracked | 
| Whether both the object tracking and the world orientation has been setup.  | |
| enum SL_OBJECT_DETECTION_MODEL | detection_model | 
| Current SL_OBJECT_DETECTION_MODEL used.  | |
| struct SL_ObjectData | object_list [MAX_NUMBER_OBJECT] | 
| Array of detected objects.  More... | |
Structure containing the results of the object detection module.
The detected objects are listed in object_list.
| int SL_Objects::nb_objects | 
Number of detected objects.
| uint64_t SL_Objects::timestamp | 
Timestamp corresponding to the frame acquisition.
This value is especially useful for the async mode to synchronize the data.
| struct SL_ObjectData SL_Objects::object_list[MAX_NUMBER_OBJECT] | 
Array of detected objects.