Structure defining the input type used in the ZED SDK. More...
Data Fields | |
enum SL_INPUT_TYPE | input_type |
Current input type. | |
unsigned int | serial_number |
Serial number of the camera. | |
unsigned int | id |
Id of the camera. | |
char | svo_input_filename [256] |
Path to the SVO file. | |
char | stream_input_ip [128] |
IP address of the streaming camera. | |
unsigned short | stream_input_port |
Port of the streaming camera. | |
Structure defining the input type used in the ZED SDK.
It can be used to select a specific camera with an id or serial number, or from a SVO file.