Structure containing a set of runtime parameters for the body tracking module. More...
Data Fields | |
| float | detection_confidence_threshold |
| Confidence threshold. More... | |
| int | minimum_keypoints_threshold |
| Minimum threshold for the keypoints. More... | |
| float | skeleton_smoothing |
| Control of the smoothing of the fitted fused skeleton. More... | |
Structure containing a set of runtime parameters for the body tracking module.
The default constructor sets all parameters to their default settings.
| float SL_BodyTrackingRuntimeParameters::detection_confidence_threshold |
Confidence threshold.
From 1 to 100, with 1 meaning a low threshold, more uncertain objects and 99 very few but very precise objects.
Default: 20.f
| int SL_BodyTrackingRuntimeParameters::minimum_keypoints_threshold |
Minimum threshold for the keypoints.
The ZED SDK will only output the keypoints of the skeletons with threshold greater than this value.
Default: 0
| float SL_BodyTrackingRuntimeParameters::skeleton_smoothing |
Control of the smoothing of the fitted fused skeleton.
It is ranged from 0 (low smoothing) and 1 (high smoothing). Default: 0