Getting Started with GStreamer and ZED
GStreamer is a popular framework used to create custom media pipelines by combining modular plugins. The ZED GStreamer plugins greatly simplifies the use of ZED camera and SDK in a GStreamer media pipeline.
The ZED GStreamer package is composed of five plugins providing five elements, a metadata library and a Linux RTSP Server application.
Plugins
Name |
Classification |
Source Code |
Description |
---|---|---|---|
zedsrc | Source | Github | acquires camera color image, depth map, sensors data and object detection information and pushes them in a GStreamer pipeline. |
zeddemux | Stream Demuxer | Github | receives a composite zedsrc stream (color left + color right + metadata or color left + depth map + metadata ), processes the eventual depth data and pushes them in two separated new streams named src_left and src_aux . A third source pad is optionally created for metadata to be externally processed. |
zeddatamux | Metadata Muxer | Github | receives a video stream compatible with ZED caps and a ZED Data Stream generated by the zeddemux and adds metadata to the video stream. This is useful if metadata are removed by a filter that does not automatically propagate them. |
zeddatacsvsink | File Sink | Github | sink plugin that receives ZED metadata, extracts the Positional Tracking and the Sensors Data information and save them in a CSV file. Demonstrates how to retrieve and parse Positional Tracking and the Sensors metadata. |
zedodoverlay | Filter Effect Video | Github | transform filter plugin that receives ZED combined stream with metadata, extracts object detection information and draws the overlays on the oncoming image frames. Demonstrates how to retrieve and parse Object Detection metadata. |
Library
Name |
Classification |
Source Code |
Description |
---|---|---|---|
zedmeta | Metadata Library | Github | GStreamer library to define and handle the ZED metadata (Positional Tracking data, Sensors data, Detected Object data, Detected Skeletons data). |
Application
Name |
Classification |
Source Code |
Description |
---|---|---|---|
RTSP Server | Server application | Github | Linux application that instantiates an RTSP server from a text launch pipeline “gst-launch” like.Detected Skeletons data). |
Installation
Prerequisites
Windows installation
-
Install the latest ZED SDK from the official download page [Optional to compile the
zedsrc
plugin to acquire data from a ZED camera device] -
Install Git
-
Install CMake
-
Install a GStreamer distribution (both
runtime
anddevelopment
installers). -
The installer should set the installation path via the
GSTREAMER_1_0_ROOT_X86_64
environment variable. -
Add the path
%GSTREAMER_1_0_ROOT_X86_64%\bin
to the system variablePATH
-
[Optional] Install OpenCV to build the
zedodverlay
filter -
Run the following commands from a terminal or command prompt, assuming CMake and Git are in your
PATH
.git clone https://github.com/stereolabs/zed-gstreamer.git cd zed-gstreamer mkdir build cd build cmake -G "Visual Studio 16 2019" .. cmake --build . --target INSTALL --config Release
Linux installation
Install prerequisites
-
Install the latest ZED SDK from the official download page
-
Update list of
apt
available packagessudo apt update
-
Install GCC compiler and build tools
sudo apt install build-essential
-
Install CMake build system
sudo apt install cmake
-
Install GStreamer, the development packages and useful tools:
sudo apt install libgstreamer1.0-0 gstreamer1.0-plugins-base gstreamer1.0-plugins-good gstreamer1.0-plugins-bad gstreamer1.0-plugins-ugly gstreamer1.0-libav libgstrtspserver-1.0-0 gstreamer1.0-doc gstreamer1.0-tools gstreamer1.0-x gstreamer1.0-alsa gstreamer1.0-gl gstreamer1.0-gtk3 gstreamer1.0-qt5 gstreamer1.0-pulseaudio libgstreamer1.0-dev libgstreamer-plugins-base1.0-dev libgstrtspserver-1.0-dev
-
[Optional] Install OpenCV to build the
zedodverlay
filtersudo apt install libopencv-dev libopencv-contrib-dev
Clone the repository
git clone https://github.com/stereolabs/zed-gstreamer.git
cd zed-gstreamer
Build
mkdir build
cd build
cmake -DCMAKE_BUILD_TYPE=Release ..
make # Note: do not use the `-j` flag because parallel build is not supported
sudo make install
Installation test
Open a command line console and try the following commands to verify that everything is correctly installed:
-
Check
ZED Video Source Plugin
installation inspecting its properties:gst-inspect-1.0 zedsrc
-
Check
ZED Video Demuxer
installation inspecting its properties:gst-inspect-1.0 zeddemux
-
Check
ZED Data Mux Plugin
installation inspecting its properties:gst-inspect-1.0 zeddatamux
-
Check
ZED CSV Sink Plugin
installation inspecting its properties:`gst-inspect-1.0 zeddatacsvsink`
-
Check
ZED Object Detection Overlay Plugin
installation inspecting its properties:`gst-inspect-1.0 zedodoverlay`
Use cases
Following a list of use case examples, linked to the relative documentation page:
- DISPLAY LEFT IMAGE ON SCREEN
- DISPLAY COLOR STEREO COUPLE WITH VGA RESOLUTION AT 100 FPS
- DISPLAY DEPTH MAP WITH HD720 RESOLUTION AT 60 FPS
- H264 STREAMING OVER UDP ON LOCAL NETWORK
- SPLIT THE STEREO COUPLE AND DISPLAY SINGLE STREAMS
- SPLIT THE RGB/LEFT SYNCHRONIZED STREAM AND DISPLAY SINGLE STREAMS
- SENSORS DATA LOGGING TO CSV FILE
- DISPLAY OBJECT DETECTION BOUNDING BOXES
- DISPLAY SKELETON TRACKING RESULTS
- INJECT ZED METADATA INFORMATION IN A STREAM
- CREATE AN RTSP SERVER TO STREAM ZED DATA