Using ZED and OpenCV in a Docker Container This tutorial shows how to use ZED SDK applications along with the OpenCV library in a Docker container. This section gives you an overview of using ZED cameras and OpenCV in a Docker Container, it demonstrates how to build and run an OpenCV application. In the next section you will learn how to create a Docker image with ZED SDK and OpenCV. However, the present tutorial presumes that you are running a Docker container with all the necessary libraries to present an overview of using OpenCV in Docker. Download and run the Docker Image To build an application using OpenCV you need to pull and run a Docker image with ZED SDK and OpenCV capabilities. If you wish to run applications that use display window make sure your container also supports OpenGL. $ docker pull <container_tag> # pull a docker container with ZED SDK , OpenCV and OpenGL support $ xhost +si:localuser:root # allows container to communicate with X server $ docker run --gpus all --runtime nvidia --privileged -e DISPLAY -v /tmp/.X11-unix:/=tmp/.X11-unix <container_tag> # Run the Docker container #Remember: Replace <container tag> with the tag of your container image --gpus all command adds all the available GPUs --privileged grants permission to the container to access the camera connected on USB --runtime nvidia will use the NVIDIA container runtime. -v /tmp/.X11-unix:/tmp/.X11-unix is required for the container to access the display. -e DISPLAY makes your DISPLAY environment variable available in the container. To know more about docker run usage and command options,read docker run description here. Run a sample OpenCV application Once there is a container running you are good to get started. Download a sample OpenCV example, [zed-opencv] (https://github.com/stereolabs/zed-opencv) is sample is the perfect place to get started. The sample implements the following tasks: Adjust several parameters: depth sensing mode, image resolution, units. Capture image, depth and point cloud from the ZED. Convert image and depth map to compatible 32-bits float OpenCV matrix. Display video and depth with OpenCV. Save side by side image, depth image and point cloud in various formats. For further explanation of the code refer to the ZED OpenCV documentation. Install the zed-opencv sample code from GitHub (https://github.com/stereolabs/zed-opencv). git clone https://github.com/stereolabs/zed-opencv.git Compile the code and run the application Build the C++ code and run the application cd zed-opencv/cpp mkdir build && cd build cmake .. make ./ZED_with_OpenCV Congratulations! You have built your first ZED OpenCV application using Docker. You can now go ahead and build other examples that use openCV in a similar way explained above. Program specific explanation and build instructions can be found in their respective GitHub repository. Next Steps Read the next section to learn how to actually Create Docker images with OpenCV.