Using the Body Tracking API
Object detection API extension
Body Tracking API is an extension of the Object detection API. Almost all functions are shared by these two modules. New functions are added for Body Tracking usage only. See Using Object Detection API for more details on the overall API usage.
Body Tracking Configuration
Body Tracking configuration shares a lot of parameters with Object detection configuration.
Opening the ZED Camera
Some parameters are set when opening the camera.
In the above example, the ZED camera is opened with 2K resolution, all 3D data are expressed with respect to the RIGHT_HANDED_Y_UP
coordinate frame. Moreover, each 3D position is expressed in METER
.
// Set camera configuration parameters
InitParameters init_parameters;
init_parameters.camera_resolution = sl::RESOLUTION::HD2K;
init_parameters.coordinate_system = sl::COORDINATE_SYSTEM::RIGHT_HANDED_Y_UP;
init_parameters.coordinate_units = sl::UNIT::METER;
// Open the camera
auto returned_state = zed.open(init_parameters);
if (returned_state != ERROR_CODE::SUCCESS) {
print("Camera Open", returned_state, "Exit program.");
return EXIT_FAILURE;
}
# Set camera configuration parameters
InitParameters init_parameters;
init_params = sl.InitParameters()
init_params.camera_resolution = sl.RESOLUTION.HD2K
init_params.coordinate_units = sl.UNIT.METER
init_params.coordinate_system = sl.COORDINATE_SYSTEM.RIGHT_HANDED_Y_UP
# Open the camera
status = zed.open(init_params)
if status != sl.ERROR_CODE.SUCCESS:
print(repr(status))
exit()
// Set camera configuration parameters
InitParameters init_params = new InitParameters();
init_params.resolution = RESOLUTION.HD2K;
init_params.coordinateUnits = UNIT.METER;
init_params.coordinateSystem = COORDINATE_SYSTEM.RIGHT_HANDED_Y_UP;
// Open the camera
zedCamera = new Camera(0);
ERROR_CODE err = zedCamera.Open(ref init_params);
if (err != ERROR_CODE.SUCCESS)
Environment.Exit(-1);
Enable Body Tracking module
Initial Body tracking configuration can be set using ObjectDetectionParameters
and runtime configuration can be set using ObjectDetectionRuntimeParameters
. Note that initial configuration must be set only once when enabling the module and runtime configuration can be changed at runtime. See Object Detection Configuration for more details on these parameters.
We will focus only on new attributes and options introduced by Body Tracking module :
-
new detection model
ObjectDetectionParameters::detection_model
that enables human body detection. These new preset configure the runtime and accuracy of the human body detector :-
DETECTION_MODEL::HUMAN_BODY_FAST
: real time performance even on Jetson or low end GPU cards-
DETECTION_MODEL::HUMAN_BODY_MEDIUM
: this is a compromise between accuracy and speed-
DETECTION_MODEL::HUMAN_BODY_ACCURATE
: state of the art accuracy, requires powerful GPU -
ObjectDetectionParameters::enable_body_fitting
: this enables the fitting process of each detected person. -
ObjectDetectionParameters::body_format
is the Body format outputed by the ZED SDK. The currently supported body format are :-
BODY_FORMAT::POSE_18
: a 18 keypoints body model. This is a COCO18 format and is not directly compatible with public software like Unreal or Unity. For this reason, all local keypoint rotation and translation are not available with this format. -
BODY_FORMAT::POSE_34
: a 34 keypoints body model. This model is compatible with public software and all available data for body can be extracted with this format.
-
The code below shows how to set these new attributes.
// Set initialization parameters
ObjectDetectionParameters detection_parameters;
detection_parameters.detection_model = DETECTION_MODEL::HUMAN_BODY_ACCURATE; //specific to human skeleton detection
detection_parameters.enable_tracking = true; // Objects will keep the same ID between frames
detection_parameters.enable_body_fitting = true; // Fitting process is called, user have access to all available data for a person processed by SDK
detection_parameters.body_format = BODY_FORMAT::POSE_34; // selects the 34 keypoints body model for SDK outputs
// Set runtime parameters
ObjectDetectionRuntimeParameters detection_parameters_rt;
detection_parameters_rt.detection_confidence_threshold = 40;
# Set initialization parameters
detection_parameters.detection_model = sl.DETECTION_MODEL.HUMAN_BODY_ACCURATE
detection_parameters = sl.ObjectDetectionParameters()
detection_parameters.enable_tracking = true
detection_parameters.enable_body_fitting = True
# Set runtime parameters
detection_parameters_rt = sl.ObjectDetectionRuntimeParameters()
detection_parameters_rt.detection_confidence_threshold = 40
// Set initialization parameters
ObjectDetectionParameters detection_parameters = new ObjectDetectionParameters();
detection_parameters.enableObjectTracking = true; // Objects will keep the same ID between frames
detection_parameters.detectionModel = sl.DETECTION_MODEL.HUMAN_BODY_ACCURATE;
detection_parameters.enableBodyFitting = true;
detection_parameters.bodyFormat = sl.BODY_FORMAT.POSE_34;
// Set runtime parameters
ObjectDetectionRuntimeParameters detection_parameters_rt = new ObjectDetectionRuntimeParameters();
detection_parameters_rt.detectionConfidenceThreshold = 40;
If you want to track persons' motion within their environment, you will first need to activate the positional tracking module. Then, set detection_parameters.enable_tracking
to true
.
if (detection_parameters.enable_tracking) {
// Set positional tracking parameters
PositionalTrackingParameters positional_tracking_parameters;
// Enable positional tracking
zed.enablePositionalTracking(positional_tracking_parameters);
}
if detection_parameters.enable_tracking :
# Set positional tracking parameters
positional_tracking_parameters = sl.PositionalTrackingParameters()
# Enable positional tracking
zed.enable_positional_tracking(positional_tracking_parameters)
if (detection_parameters.enableObjectTracking ) {
// Set positional tracking parameters
PositionalTrackingParameters trackingParams = new PositionalTrackingParameters();
// Enable positional tracking
zed.EnablePositionalTracking(ref trackingParams);
}
With these parameters configured, you can enable the Body Tracking module in exactly the same way as Object detection module :
// Enable object detection with initialization parameters
zed_error = zed.enableObjectDetection(detection_parameters);
if (zed_error != ERROR_CODE::SUCCESS) {
cout << "enableObjectDetection: " << zed_error << "\nExit program.";
zed.close();
exit(-1);
}
# Enable object detection with initialization parameters
zed_error = zed.enable_object_detection(detection_parameters)
if zed_error != sl.ERROR_CODE.SUCCESS :
print("enable_object_detection", zed_error, "\nExit program.")
zed.close()
exit(-1)
// Enable object detection with initialization parameters
zed_error = zedCamera.EnableObjectDetection(ref detection_parameters);
if (zed_error != ERROR_CODE.SUCCESS) {
Console.WriteLine("enableObjectDetection: " + zed_error + "\nExit program.";
zed.Close();
Environment.Exit(-1);
}
Note: Body tracking has been optimized for ZED 2 wide angle field of view and uses the camera motion sensors for improved reliability. Therefore the Body Tracking module requires ZED 2, and sensors cannot be disabled when using the module.
Getting Human Body Data
To get the detected person in a scene, get a new image with grab(...)
and extract the detected person with retrieveObjects()
. This process is exactly the same as getting new objects with Object detection module.
sl::Objects objects; // Structure containing all the detected objects
// grab runtime parameters
RuntimeParameters runtime_parameters;
runtime_parameters.measure3D_reference_frame = sl::REFERENCE_FRAME::WORLD;
if (zed.grab(runtime_parameters) == ERROR_CODE::SUCCESS) {
zed.retrieveObjects(objects, detection_parameters_rt); // Retrieve the detected objects
}
objects = sl.Objects() # Structure containing all the detected objects
# grab runtime parameters
runtime_params = sl.RuntimeParameters()
runtime_params.measure3D_reference_frame = sl.REFERENCE_FRAME.WORLD;
if zed.grab(runtime_params) == sl.ERROR_CODE.SUCCESS :
zed.retrieve_objects(objects, obj_runtime_param) # Retrieve the detected objects
sl.Objects objects = new sl.Objects(); // Structure containing all the detected objects
// grab runtime parameters
RuntimeParameters runtimeParameters = new RuntimeParamters();
runtimeParameters.measure3DReferenceFrame = sl.REFERENCE_FRAME.WORLD;
if (zed.Grab(ref runtimeParameters) == ERROR_CODE.SUCCESS) {
zed.RetrieveObjects(ref objects, ref detection_parameters_rt); // Retrieve the detected objects
}
sl::Objects
class stores all data regarding the different persons present in the scene in its vector<sl::ObjectData> object_list
attribute. Each person data are stored as a sl::ObjectData
. sl::Objects
also contains the timestamp of the detection, which can help connect the objects to the images.
All 2D data are related to the left image, while the 3D data are either in the CAMERA
or WORLD
referential depending on RuntimeParameters.measure3D_reference_frame
(given to the grab()
function). The 2D data are expressed in the initial camera resolution RESOLUTION
. A scaling can be applied if the value is needed in another resolution.
For 3D data, the coordinate frame and units can be set by user with using COORDINATE_SYSTEM
and UNIT
respectively. These setting are accessible using InitParameters
when opening the ZED camera with open function.
Accessing Human Body Data
Once a sl::ObjectData
is retrieved from the object vector, all data available with respect to the initial configuration can be accessed. All Object detection datas are accessible. See Getting Object Data for shared datas between Object detection and Body tracking module.
Getting 2D and 3D human keypoints
2D and 3D keypoint data of a detected person are accessible in a vector of pixel keypoint keypoint_2d
and a vector of 3d position keypoint
which are new attributes of sl::ObjectData
.
From a sl::ObjectData
object obj
, these new attributes can be accessible :
// collect all 2d keypoints
for (auto& kp_2d : obj.keypoint_2d) {
// user code using each kp_2d point
}
// collect all 3d keypoints
for (auto& kp_3d : obj.keypoint)
{
// user code using each kp_3d point
}
# collect all 2d keypoints
for kp_2d in obj.keypoint_2d:
# user code using each kp_2d point
# collect all 3d keypoints
for kp_3d in obj.keypoint:
# user code using each kp_3d point
// collect all 2d keypoints
foreach (var kp_2d in obj.keypoints2D)
{
// user code using each kp_2d point
}
// collect all 3d keypoints
foreach (var kp_3d in obj.keypoints)
{
// user code using each kp_3d point
}
See the keypoint index and name correspondence as well as the output skeleton format here.
Getting more results
When fitting is enable at initial configuration, more results are available according to the chosen BODY_FORMAT
. All local rotation and translation of each keypoint become available to user with BODY_FORMAT::POSE_34
format.
From a sl::ObjectData
object obj
, these datas can be accessed as below:
// collect local rotation for each keypoint
for (auto &kp : obj.local_orientation_per_joint)
{
// kp is the local keypoint rotation represented by a quaternion
// user code
}
// collect local translation for each keypoint
for (auto &kp : obj.local_position_per_joint)
// kp is the local keypoint translation
// user code
}
// get global root orientation
auto global_root_orientation = obj.global_root_orientation
// note that global root translation is available in obj.keypoint[root_index] where root_index is the root index of the body model
# collect local rotation for each keypoint
for kp in obj.local_orientation_per_joint:
# kp is the local keypoint rotation represented by a quaternion
# user code
# collect local translation for each keypoint
for kp in obj.local_position_per_joint:
# kp is the local keypoint translation
# user code
# get global root orientation
global_root_orientation = obj.global_root_orientation
# note that global root translation is available in obj.keypoint[root_index] where root_index is the root index of the body model
// collect local rotation for each keypoint
foreach (var kp in obj.localOrientationPerJoint)
{
// kp is the local keypoint rotation represented by a quaternion
// user code
}
// collect local translation for each keypoint
foreach (var kp in obj.localPositionPerJoint)
// kp is the local keypoint translation
// user code
}
// get global root orientation
Quaternion globalRootOrientation = obj.globalRootOrientation;
Note that all these data are expressed in the chosen COORDINATE_SYSTEM
and UNITS
.
Code Example
For code examples, check out the Tutorial and Sample on GitHub.