Adding Video Capture in ROS 2
Video with RVIZ 2 #
In this tutorial, you will learn how to configure your own RVIZ 2 session to see only the video data that you require.
To visualize the video stream published by the ZED node, you can use two different plugins:
Camera
: Displays an image from a camera, with the visualized world rendered behind itImage
: Displays an image from a topic of typesensor_msgs/Image
Camera #
The Camera
plugin allows you to visualize an image from a topic of type sensor_msgs/Image
. It acts as if the source of the image is placed on its virtual frame and renders all virtual objects in front of it.
Key parameters:
Topic
: Selects the image topic to visualize from the list of available images in the combo boxDepth
: The depth of the incoming message queueHistory policy
: Set the QoS history policy.Keep Last
is suggested for performance and compatibilityReliability Policy
: Set the QoS reliability policy.Best Effort
is suggested for performances,Reliable
is used for compatibilityDurability Policy
: Set the QoS durability policy.Volatile
is suggested for compatibility
By expanding Visibility
, you can select/deselect what will be visible in the camera view
. Only active plugins can be selected.
Image #
The Image
plugin allows you to visualize an image from a topic of type sensor_msgs/Image
.
Key parameters:
Topic
: Selects the image topic to visualize from the list of available images in the combo boxDepth
: The depth of the incoming message queueHistory policy
: Set the QoS history policy.Keep Last
is suggested for performance and compatibilityReliability Policy
: Set the QoS reliability policy.Best Effort
is suggested for performances,Reliable
is used for compatibilityDurability Policy
: Set the QoS durability policy.Volatile
is suggested for compatibility
Video subscribing in C++ #
In this tutorial, you will learn how to write a simple C++ node that subscribes to messages of type
sensor_msgs/Image
. This lets you retrieve the Left and Right rectified images published by the ZED node.
Introduction #
Open a new console and use this command to connect the camera to the ROS 2 network:
ros2 launch zed_display_rviz2 display_zed_cam.launch.py camera_model:=<camera model>
📌 Note: the old launch command
ros2 launch zed_display_rviz2 display_<camera model>.launch.py
is now obsolete and will be removed in a future release of the wrapper.
The ZED node will start to publish image data in the network only if there is another node that subscribes to the relative topic.
Running the tutorial #
If you properly followed the ROS 2 Examples Installation Guide, the executable of this tutorial has been compiled and you can run the subscriber node using this command:
ros2 run stereolabs_zed_tutorial_video stereolabs_zed_tutorial_video
The tutorial node subscribes generic left_image
and right_image
topics, so a remapping is required to connect to the correct topics published by the ZED node:
ZED:
ros2 run zed_tutorial_video zed_tutorial_video --ros-args -r left_image:=/zed/zed_node/left/image_rect_color -r right_image:=/zed/zed_node/right/image_rect_color
If the ZED node is running and a camera is connected or you have loaded an SVO file, you will receive the following stream of messages confirming that you have correctly subscribed to the ZED image topics:
[INFO] [zed_video_tutorial]: Left Rectified image received from ZED Size: 1280x720 - Timestamp: 1602576933.791896880 sec
[INFO] [zed_video_tutorial]: Right Rectified image received from ZED Size: 1280x720 - Timestamp: 1602576933.891931106 sec
[INFO] [zed_video_tutorial]: Left Rectified image received from ZED Size: 1280x720 - Timestamp: 1602576934.91928857 sec
[INFO] [zed_video_tutorial]: Right Rectified image received from ZED Size: 1280x720 - Timestamp: 1602576934.91928857 sec
[INFO] [zed_video_tutorial]: Left Rectified image received from ZED Size: 1280x720 - Timestamp: 1602576934.191911460 sec
[INFO] [zed_video_tutorial]: Right Rectified image received from ZED Size: 1280x720 - Timestamp: 1602576934.191911460 sec
[...]
The code #
The source code of the subscriber node zed_video_sub_tutorial.cpp:
#include <rclcpp/rclcpp.hpp>
#include <rclcpp/qos.hpp>
#include <sensor_msgs/msg/image.hpp>
rclcpp::Node::SharedPtr g_node = nullptr;
/**
* Subscriber callbacks. The argument of the callback is a constant pointer to the received message
*/
void imageRightRectifiedCallback(const sensor_msgs::msg::Image::SharedPtr msg) {
RCLCPP_INFO(g_node->get_logger(),
"Right Rectified image received from ZED\tSize: %dx%d - Timestamp: %u.%u sec ",
msg->width, msg->height,
msg->header.stamp.sec,msg->header.stamp.nanosec);
}
void imageLeftRectifiedCallback(const sensor_msgs::msg::Image::SharedPtr msg) {
RCLCPP_INFO(g_node->get_logger(),
"Left Rectified image received from ZED\tSize: %dx%d - Timestamp: %u.%u sec ",
msg->width, msg->height,
msg->header.stamp.sec,msg->header.stamp.nanosec);
}
int main(int argc, char* argv[]) {
rclcpp::init(argc, argv);
// Create the node
g_node = rclcpp::Node::make_shared("zed_video_tutorial");
/* Note: it is very important to use a QOS profile for the subscriber that is compatible
* with the QOS profile of the publisher.
* The ZED component node uses a default QoS profile with reliability set as "RELIABLE"
* and durability set as "VOLATILE".
* To be able to receive the subscribed topic the subscriber must use compatible
* parameters.
*/
// https://github.com/ros2/ros2/wiki/About-Quality-of-Service-Settings
rclcpp::QoS video_qos(10);
video_qos.keep_last(10);
video_qos.best_effort();
video_qos.durability_volatile();
// Create right image subscriber
auto right_sub = g_node->create_subscription<sensor_msgs::msg::Image>(
"right_image", video_qos, imageRightRectifiedCallback );
// Create left image subscriber
auto left_sub = g_node->create_subscription<sensor_msgs::msg::Image>
("left_image", video_qos, imageLeftRectifiedCallback );
// Let the node run
rclcpp::spin(g_node);
// Shutdown when the node is stopped using Ctrl+C
rclcpp::shutdown();
return 0;
}
The code explained #
The following is a brief explanation of the source code above:
void imageRightRectifiedCallback(const sensor_msgs::msg::Image::SharedPtr msg) {
RCLCPP_INFO(g_node->get_logger(),
"Right Rectified image received from ZED\tSize: %dx%d - Timestamp: %u.%u sec ",
msg->width, msg->height,
msg->header.stamp.sec,msg->header.stamp.nanosec);
}
void imageLeftRectifiedCallback(const sensor_msgs::msg::Image::SharedPtr msg) {
RCLCPP_INFO(g_node->get_logger(),
"Left Rectified image received from ZED\tSize: %dx%d - Timestamp: %u.%u sec ",
msg->width, msg->height,
msg->header.stamp.sec,msg->header.stamp.nanosec);
}
These callbacks are executed when the subscriber node receives a message of type sensor_msgs/Image
that matches the subscribed topic.
The parameter of the callback is a std::shared_ptr
to the received message. This means you don’t have to worry
about memory management.
The callback code is very simple and demonstrates how to access the fields in a message;
in this case, the height
and width
of the image and the topic timestamp.
The main
function is divided in two main parts:
Node declaration:
rclcpp::init(argc, argv);
// Create the node
g_node = rclcpp::Node::make_shared("zed_video_tutorial");
First, the ROS 2 environment is initialized with the rclcpp::init
command. Then, the zed_video_tutorial
node is created and a shared pointer g_node
to it is initialized.
The most important lesson of the above code is how the subscribers are defined:
rclcpp::QoS video_qos(10);
video_qos.keep_last(10);
video_qos.best_effort();
video_qos.durability_volatile();
// Create right image subscriber
auto right_sub = g_node->create_subscription<sensor_msgs::msg::Image>(
"right_image", video_qos, imageRightRectifiedCallback );
// Create left image subscriber
auto left_sub = g_node->create_subscription<sensor_msgs::msg::Image>(
"left_image", video_qos, imageLeftRectifiedCallback );
The two auto
variables right_sub
and left_sub
are two rclcpp::Subscription
objects.
A rclcpp::Subscription
is a ROS object that listens to the network and waits for its own topic message to be available.
When a message is received, it executes the callback assigned to it.
We declared two subscribers: one for the left rectified image and one for the right rectified image.
- The subscriber to the
right_image
topic calls theimageRightRectCallback
function when it receives a message of typesensor_msgs/Image
that matches that topic - The subscriber to the
left_image
topic calls theimageLeftRectCallback
function when it receives a message of typesensor_msgs/Image
that matches that topic
It is important that the two subscriptions use a QOS profile compatible with the QOS profile of the publisher of the topics.
In this case, the QOS profile is configured to keep the last received 10 messages with “best effort” reliability and “volatile” durability. This configuration is highly compatible with many possible publisher configurations.
For more information about QoS compatibility, refer to the ZED node guide
📌 Note: The code of this tutorial instantiates a
rclcpp::Node
without subclassing it. This was the typical usage model in the original **ROS, but unfortunately, this style of coding is not compatible with composing multiple nodes into a single process. Thus, it is no longer the recommended style for ROS 2. Please refer to the “Depth sensing” tutorial for C++ tutorials written with a coding style more targeted to ROS 2.
Conclusion #
The full source code of this tutorial is available on GitHub in the zed_video_tutorial sub-package.
Along with the node source code are the package.xml
and CMakeLists.txt
files that complete the tutorial package.