Adding Depth Perception in ROS 2
Depth with RVIZ 2 #
In this tutorial, you will learn in detail how toconfigure your own RVIZ session to see only the depth data that you require.
Depth information can be visualized in many different ways: 2D depth images, 3D point clouds, 3D registered depth clouds, and the confidence image to name a few.
Depth image #
To visualize a depth image
, you can use the simple Image plugin
since the depth data are published on topics of type sensor_msgs/Image
. It differs from a “normal” image in that the data is encoded in 32-bit (floating point) not 8-bit.
The parameters are the same as for Image
(see the Video tutorial) with three additions:
Normalize range
: Since a floating point image is not directly rendered, it is converted to an 8-bit grayscale image. Enabling this field means the normalization range is automatically calculatedMin value
: IfNormalize range
is unchecked, you can manually set the minimum depth range in metersMax value
: IfNormalize range
is unchecked, you can manually set the maximum depth range in meters
Manually setting the normalization range is useful if you know the maximum value measured for the depth and you want to keep the image scale static.
Pointcloud #
To directly visualize a topic of type sensor_msgs/Pointcloud2
you can use the Pointcloud2
plugin.
Key parameters:
Topic
: Selects the topic to visualize from the list of available point cloud messagesDepth
: The depth of the incoming message queueHistory policy
: Set the QoS history policy.Keep Last
is suggested for performance and compatibilityReliability Policy
: Set the QoS reliability policy.Best Effort
is suggested for performances,Reliable
is used for compatibilityDurability Policy
: Set the QoS durability policy.Volatile
is suggested for compatibilityStyle
: The style used to render each point. UsePoints
andSize=1
to maximize FPSColor transformer
: Selects how points are colored. UseRGB8
to match the color image pixels to the corresponding depth pixels. UseAxis color
to use a color proportional to the value of theAxis
value (e.g.Z
to use a color scale proportional to the distance from the floor orX
to use a color proportional to the distance from the camera)
📌 Note: if mapping is enabled (see mapping/mapping_enabled parameter), the Pointcloud2 plugin is used also to visualize the fused point cloud result of the mapping elaboration, subscribing to the topic /zed/zed_node/point_cloud/fused_cloud_registered.
Confidence #
To visualize the Confidence Map
as an image, you can use the Image
plugin subscribing to the topic ~/confidence/confidence_image
.
The lighter a pixel, the more reliable its corresponding depth value is.
Depth subscribing in C++ #
In this tutorial, you will learn how to write a simple C++ node that subscribes to messages of type
sensor_msgs/Image
in order to retrieve depth images published by the ZED node and to get the measured distance at the center of the image.
Introduction #
Open a new console and use this command to connect the camera to the ROS 2 network:
ros2 launch zed_display_rviz2 display_zed_cam.launch.py camera_model:=<camera model>
📌 Note: the old launch command
ros2 launch zed_display_rviz2 display_<camera model>.launch.py
is now obsolete and will be removed in a future release of the wrapper.
The ZED node will start to publish image data in the network only if there is another node that subscribes to the relative topic.
Running the tutorial #
If you properly followed the ROS 2 Examples Installation Guide, the executable of this tutorial has been compiled and you can run the subscriber node using this command:
ros2 run zed_tutorial_depth zed_tutorial_depth
The tutorial node subscribes generic depth
topic, so a remapping is required to connect to the correct topic published by the ZED node:
ros2 run zed_tutorial_depth zed_tutorial_depth --ros-args -r depth:=/zed/zed_node/depth/depth_registered
If the ZED node is running and a camera is connected or you have loaded an SVO file, you will receive the following stream of messages confirming that you are correctly subscribing to the ZED image topics:
[INFO] [zed_depth_tutorial]: Center distance : 0.981005 m
[INFO] [zed_depth_tutorial]: Center distance : nan m
[INFO] [zed_depth_tutorial]: Center distance : nan m
[INFO] [zed_depth_tutorial]: Center distance : 1.20664 m
[INFO] [zed_depth_tutorial]: Center distance : 1.16232 m
[INFO] [zed_depth_tutorial]: Center distance : 1.15096 m
[INFO] [zed_depth_tutorial]: Center distance : 1.15708 m
[INFO] [zed_depth_tutorial]: Center distance : 1.14709 m
[INFO] [zed_depth_tutorial]: Center distance : 1.15806 m
[INFO] [zed_depth_tutorial]: Center distance : 1.16716 m
[INFO] [zed_depth_tutorial]: Center distance : 1.17654 m
[INFO] [zed_depth_tutorial]: Center distance : 1.16571 m
[INFO] [zed_depth_tutorial]: Center distance : 1.16145 m
[...]
📌 Note:
nan
values for depths are reported if the central pixel of the image does not contain a valid depth measure (occlusion, flare, low textured surface, …).
The code #
The source code of the subscriber node zed_depth_sub_tutorial.cpp
:
#include "rclcpp/rclcpp.hpp"
#include "sensor_msgs/msg/image.hpp"
using namespace std::placeholders;
class MinimalDepthSubscriber : public rclcpp::Node {
public:
MinimalDepthSubscriber()
: Node("zed_depth_tutorial") {
/* Note: it is very important to use a QOS profile for the subscriber that is compatible
* with the QOS profile of the publisher.
* The ZED component node uses a default QoS profile with reliability set as "RELIABLE"
* and durability set as "VOLATILE".
* To be able to receive the subscribed topic the subscriber must use compatible
* parameters.
*/
// https://github.com/ros2/ros2/wiki/About-Quality-of-Service-Settings
rclcpp::QoS depth_qos(10);
depth_qos.keep_last(10);
depth_qos.best_effort();
depth_qos.durability_volatile();
// Create depth map subscriber
mDepthSub = create_subscription<sensor_msgs::msg::Image>(
"depth", depth_qos,
std::bind(&MinimalDepthSubscriber::depthCallback, this, _1) );
}
protected:
void depthCallback(const sensor_msgs::msg::Image::SharedPtr msg) {
// Get a pointer to the depth values casting the data
// pointer to floating point
float* depths = (float*)(&msg->data[0]);
// Image coordinates of the center pixel
int u = msg->width / 2;
int v = msg->height / 2;
// Linear index of the center pixel
int centerIdx = u + msg->width * v;
// Output the measure
RCLCPP_INFO(get_logger(), "Center distance : %g m", depths[centerIdx]);
}
private:
rclcpp::Subscription<sensor_msgs::msg::Image>::SharedPtr mDepthSub;
};
// The main function
int main(int argc, char* argv[]) {
rclcpp::init(argc, argv);
auto depth_node = std::make_shared<MinimalDepthSubscriber>();
rclcpp::spin(depth_node);
rclcpp::shutdown();
return 0;
}
The code explained #
The tutorial is written using the new concept of Component
introduced in ROS 2 in order to take advantage of the node composition capabilities.
A component named MinimalDepthSubscriber
is created subclassing the ROS 2 object rclcpp::Node
.
In the constructor, we initialize the parent class Node
with the name of our node new zed_depth_sub
:
MinimalDepthSubscriber()
: Node("zed_depth_tutorial") {
rclcpp::QoS depth_qos(10);
depth_qos.keep_last(10);
depth_qos.best_effort();
depth_qos.durability_volatile();
// Create depth map subscriber
mDepthSub = create_subscription<sensor_msgs::msg::Image>(
"depth", depth_qos,
std::bind(&MinimalDepthSubscriber::depthCallback, this, _1) );
}
The constructor mainly defines mDepthSub
, a std::SharedPtr
to an object that creates a subscriber in the node. The subscriber checks for topics of type depth
and recalls the callback function MinimalDepthSubscriber::depthCallback
every time it receives one of them.
ROS 2 uses the new constructs available with C++11 and C++14, so to bind the callback (a class method in this case) to the mDepthSub
object we use the form
std::bind(&MinimalDepthSubscriber::depthCallback, this, _1)
.
It is important that the subscription use a QOS profile compatible with the QOS profile of the publisher of the topics.
In this case, the QOS profile is configured to keep the last received 10 messages with “best effort” reliability and “volatile” durability. This configuration is highly compatible with many possible publisher configurations.
For more information about QoS compatibility, refer to the ZED node guide
Now we must define the callback to execute when one of the subscribed topics is received:
void depthCallback(const sensor_msgs::msg::Image::SharedPtr msg) {
// Get a pointer to the depth values casting the data
// pointer to floating point
float* depths = (float*)(&msg->data[0]);
// Image coordinates of the center pixel
int u = msg->width / 2;
int v = msg->height / 2;
// Linear index of the center pixel
int centerIdx = u + msg->width * v;
// Output the measure
RCLCPP_INFO(get_logger(), "Center distance : %g m", depths[centerIdx]);
}
This callback is executed when the subscriber node receives a message of type sensor_msgs/Image
that matches the subscribed topic depth
.
The parameter of the callback is a std::shared_ptr
to the received message. This means that you don’t have to worry about memory management for it.
The callback demonstrates how to access the message data:
- The pointer to the
data
field is cast tofloat*
as it is declared as a pointer to an array ofchar
values - The image coordinates [u,v] of the center of the depth image are calculated
- Since the data are organized in a linear vector, the index of the central pixel is calculated from the image coordinates
- The measure in meters of the center point is printed on the screen
Finally, the main
function is standard for a ROS 2 node that executes a single component:
int main(int argc, char* argv[]) {
rclcpp::init(argc, argv);
auto depth_node = std::make_shared<MinimalDepthSubscriber>();
rclcpp::spin(depth_node);
rclcpp::shutdown();
return 0;
}
The ROS 2 environment is initialized using the rclcpp::init
command. Then we create a depth_node
Component as a std::shared_ptr
.
to the MinimalDepthSubscriber
class that we defined above.
Then the code of the node is executed in the main thread using the rclcpp::spin(depth_node);
command. The node will run until the user presses Ctrl+C to stop it, shut it down, and exit.
Conclusions #
The full source code of this tutorial is available on GitHub in the zed_depth_tutorial sub-package.
Along with the node source code, you can find the package.xml
and CMakeLists.txt
files that complete the tutorial package.