Getting Started with ROS and ZED
The ZED ROS wrapper lets you use the ZED stereo cameras with ROS. It provides access to the following data:
- Left and right rectified/unrectified images
- Depth map
- Colored 3D point cloud
- Visual odometry: Position and orientation of the camera
- Pose tracking: Position and orientation of the camera fixed and fused with IMU data
- Spatial mapping: Fused 3d point cloud
- Sensors data: accelerometer, gyroscope, barometer, magnetometer, internal temperature sensors
Installation #
Prerequisites #
- Ubuntu 20.04
- ZED SDK ≥ 3.5 and its dependency CUDA
- ROS Noetic
or
- Ubuntu 18.04
- ZED SDK ≥ 3.5 and its dependency CUDA
- ROS Melodic
Build the packages #
The ZED ROS wrapper is available on GitHub and subdivided in three repositories:
- zed-ros-wrapper: the main package that provides the ZED ROS Wrapper node
- zed-ros-interfaces: the package declaring custom topics, services and actions
- zed-ros-examples: a support package that contains examples and tutorials about how to use the ZED ROS Wrapper We suggest installing the main package on the robot and using the examples on a desktop PC to take confidence with the many features provided by the ROS wrapper. In this way, the robot installation will be clean and the many dependencies required by the examples will not be installed on it.
The zed-ros-interfaces
repository is automatically integrated by zed-ros-wrapper
as a git submodule to satisfy all the required dependencies.
You must instead install the zed-ros-interfaces
repository on a remote system that must retrieve the topics sent by the ZED Wrapper (e.g. the list of detected objects obtained with the Object Detection module) or call services and actions to control the status of the ZED Wrapper.
zed-ros-wrapper #
zed-ros-wrapper is a catkin package that depends on the following ROS packages:
- nav_msgs
- tf2_geometry_msgs
- message_runtime
- catkin
- roscpp
- stereo_msgs
- rosconsole
- robot_state_publisher
- urdf
- sensor_msgs
- image_transport
- roslint
- diagnostic_updater
- dynamic_reconfigure
- tf2_ros
- message_generation
- nodelet
📌 Note: If you haven’t set up your catkin workspace yet, please follow this short tutorial. To install the zed-ros-wrapper, open a bash terminal, clone the repository, update the dependencies and build the packages:
cd ~/catkin_ws/src
git clone --recursive https://github.com/stereolabs/zed-ros-wrapper.git
cd ../
rosdep install --from-paths src --ignore-src -r -y
catkin_make -DCMAKE_BUILD_TYPE=Release
source ./devel/setup.bash
📌 Note: If you are using a different console interface like
zsh
, you have to change thesource
command as follows:echo source $(pwd)/devel/setup.zsh >> ~/.zshrc
andsource ~/.zshrc
.
Error: If an error mentioning
/usr/lib/x86_64-linux-gnu/libEGL.so
blocks compilation, use the following command to repair the libEGl symlink before restarting thecatkin_make
command:
# Only on libEGL error
sudo rm /usr/lib/x86_64-linux-gnu/libEGL.so
sudo ln /usr/lib/x86_64-linux-gnu/libEGL.so.1 /usr/lib/x86_64-linux-gnu/libEGL.so
zed-ros-interfaces #
The zed_interfaces
is a catkin package. It depends on the following ROS packages:
- catkin
- std_msgs
- sensor_msgs
- actionlib_msgs
- geometry_msgs
- message_generation
Open a terminal, clone the repository, update the dependencies and build the packages:
cd ~/catkin_ws/src
git clone https://github.com/stereolabs/zed-ros-interfaces.git
cd ../
rosdep install --from-paths src --ignore-src -r -y
catkin_make -DCMAKE_BUILD_TYPE=Release
source ./devel/setup.bash
📌 Note: this package does not require CUDA, hence it can be used to receive the ZED data also on machines not equipped with an NVIDIA® GPU.
Custom Topics
- BoundingBox2Df
- BoundingBox2Di
- BoundingBox3D
- Keypoint2Df
- Keypoint2Di
- Keypoint3D
- Object
- ObjectsStamped
- RGBDSensors
- Skeleton2D
- Skeleton3D
Custom Services
- reset_odometry
- reset_tracking
- set_led_status
- set_pose
- save_3d_map
- save_area_memory
- start_3d_mapping
- start_object_detection
- start_remote_stream
- start_svo_recording
- stop_3d_mapping
- stop_object_detection
- stop_remote_stream
- stop_svo_recording
- toggle_led
zed-ros-examples #
The zed-ros-examples
repository is a collection of catkin packages. They depend on the following ROS packages:
- catkin
- zed_wrapper
- sensor_msgs
- roscpp
- nav_msgs
- geometry_msgs
- ar_track_alvar
- ar_track_alvar_msgs
- nodelet
- depthimage_to_laserscan
- rtabmap
- rtabmap_ros
- rviz_imu_plugin
- rviz
To install all the packages open a terminal, clone the repository, update the dependencies and build the packages:
cd ~/catkin_ws/src
git clone https://github.com/stereolabs/zed-ros-examples.git
cd ../
rosdep install --from-paths src --ignore-src -r -y
catkin_make -DCMAKE_BUILD_TYPE=Release
source ./devel/setup.bash
Starting the ZED node #
The ZED is available in ROS as a node that publishes its data to topics. You can read the full list of available topics here.
Open a terminal and use roslaunch
to start the ZED node:
- ZED camera:
roslaunch zed_wrapper zed.launch
- ZED Mini camera:
roslaunch zed_wrapper zedm.launch
- ZED 2 camera:
roslaunch zed_wrapper zed2.launch
- ZED 2i camera:
roslaunch zed_wrapper zed2i.launch
📌 Note: You can set your own configuration parameters modifying the file
param/common.yaml
,param/zed.yaml
,param/zedm.yaml
andparam/zed2.yaml
as described in the parameter documentation.
Displaying ZED data #
Using RVIZ #
RVIZ is a useful visualization tool in ROS. Using RVIZ, you can visualize the ZED left and right images, depth, point cloud, and 3D trajectory.
Launch the ZED wrapper along with RVIZ using the following commands available if you installed the zed-ros-examples
repository:
roslaunch zed_display_rviz display_zed.launch
If you are using a ZED Mini camera, you can visualize additional information about IMU data using the following command:
roslaunch zed_display_rviz display_zedm.launch
If you are using a ZED 2 camera, you can visualize additional information about environmental sensors:
roslaunch zed_display_rviz display_zed2.launch
If you are using a ZED 2i camera, you can visualize additional information about environmental sensors:
roslaunch zed_display_rviz display_zed2i.launch
📌 Note: If you haven’t yet configured your own RVIZ interface, you can find detailed tutorials here.
Displaying Images #
The ZED node publishes both original and stereo rectified (aligned) left and right images. In RVIZ, use the image
preview mode and select one of the available image topics. Following the list of the main image topics:
- rgb/image_rect_color: Color rectified image (left sensor by default)
- rgb/camera_info: Color camera calibration data
- rgb_raw/image_raw_color: Color unrectified image (left sensor by default)
- rgb_raw/camera_info: Unrectified color camera calibration data
- right/image_rect_color: Right camera rectified image
- right/camera_info: Right sensor calibration data
- right_raw/image_raw_color: Right camera unrectified image
- right_raw/camera_info: Unrectified right sensor calibration data
- confidence/confidence_image: Confidence map as image
📌 Note: The Confidence Map is also available as a 32bit floating point image subscribing to the confidence/confidence_map topic.
Displaying Depth #
The depth map can be displayed in RVIZ with the following topic:
- depth/depth_registered: 32-bit depth values in meters. RVIZ will normalize the depth map on 8-bit and display it as a grayscale depth image.
📌 Note: An OpenNI compatibility mode is available in the
launch/zed_camera.launch
file. Setopenni_depth_mode
to1
to get depth in millimeters and in 16-bit precision, and restart the ZED node.
Displaying Disparity #
The Disparity Image is available by subscribing to the disparity/disparity_image topics.
Launch the Disparity Viewer to visualize it:
rosrun image_view disparity_view image:=disparity/disparity_image
Displaying the Point cloud #
A 3D colored point cloud can be displayed in RVIZ with the zed/zed_node/point_cloud/cloud_registered topic.
Add it in RVIZ with point_cloud -> cloud -> PointCloud2. Note that displaying point clouds slows down RVIZ, so open a new instance if you want to display other topics.
Displaying position and path #
The ZED position and orientation in space over time are published on the following topics:
- odom: Odometry pose referred to odometry frame (only visual odometry is applied for ZED, visual-inertial for ZED Mini)
- pose: Camera pose referred to Map frame (complete data fusion algorithm is applied)
- pose_with_covariance: Camera pose referred to Map frame with covariance
- path_odom: The sequence of camera odometry poses in Map frame
- path_map: The sequence of camera poses in Map frame
Important: By default, RVIZ does not display odometry data correctly. Open the newly created Odometry object in the left list, and set Position Tolerance and Angle Tolerance to 0, and Keep to 1.
Launching with recorded SVO video #
With the ZED, you can record and play back stereo video using the .svo file format. To record a sequence, open the ZED Explorer app and click on the REC button.
To launch the ROS wrapper with an SVO file, set an svo_file path launch parameter in the command line when starting the package:
ZED:
roslaunch zed_wrapper zed.launch svo_file:=/path/to/file.svo
ZED Mini:
roslaunch zed_wrapper zedm.launch svo_file:=/path/to/file.svo
ZED 2:
roslaunch zed_wrapper zed2.launch svo_file:=/path/to/file.svo
ZED 2i:
roslaunch zed_wrapper zed2i.launch svo_file:=/path/to/file.svo
Dynamic reconfigure #
You can dynamically change many configuration parameters during the execution of the ZED node.
You can set the parameters using the command dynparam set, e.g.:
rosrun dynamic_reconfigure dynparam set depth_confidence 80
or you can use the GUI provided by the rqt
stack:
rosrun rqt_reconfigure rqt_reconfigure
The full list of available dynamic parameters is available here