ZED Link Duo on Xavier AGX
This tutorial will help you set up the ZED Link Duo GMSL2 capture card, and use the Stereolabs GMSL2 cameras with the NVIDIA® Jetson™ Xavier AGX Developer Kit.
Prerequisites #
Make sure that you have the following items before starting this guide:
- 1x NVIDIA® Jetson™ AGX Xavier Developer Kit
- 1x ZED Link Duo GMSL2 capture card
- 1x 1-to-4 GMSL2 Fakra Male to Female cable (included in the box)
- 1x NVIDIA® Power supplier to power the DevKit (included with the devkit)
📌 Note: the ZED Link Duo card does not need external power when connected to an NVIDIA® Jetson™ AGX devkit
If you encounter any issues during the installation process, please refer to the GMSL2 troubleshooting page, or contact support@stereolabs.com.
Install the GMSL2 Capture Card #
Please make sure the AGX DevKit is powered off and not connected to a power source before installing the capture card.
Plug in the capture card in the ‘Camera connector’ slot and fix it by using the three provided screws, as shown in the following diagrams:
📌 Note: The capture card is powered by the Dev Kit, therefore you do not need to use an additional power supply for the card.
The final setup should look as such:

Connect the camera #
Connect the GMSL2 Fakra cable female end to your GMSL2. When you hear a click, the cable is securely connected to the camera.
With the DevKit still powered off, connect the male end of the cable to the capture card’s GMSL2 input. Again, a click informs you that the cable is secured.
Now that the Developer Kit has been correctly set up, we can install the associated software and drivers for the ZED X.
Setting up the software #
Install the ZED Link #
After setting up your ZED Link capture card, please follow this guide to Install the ZED Link Driver.
Install the ZED SDK #
After installing the ZED Link driver, please follow this guide to Install the ZED SDK on NVIDIA® Jetson.
🎉 Congratulations! You have successfully set up your Stereolabs GMSL2 Capture Card and started exploring its features. Now that you have the camera up and running, it is time to start experimenting and building your projects.
Whether you are using the camera for robotics, computer vision, or something else entirely, the ZED GMSL2 cameras are a powerful tool that can help you achieve your goals. Happy coding!