Depth Settings
sl::InitParameters Depth Parameters
For more information on these parameters, see the API documentation page.
Depth Mode
Check this page to get more insights about the currently available depth modes for the ZED cameras.
Depth Precision
For the NEURAL depth mode, InitParameters::depth_precision selects the numerical precision of the neural network inference. DEPTH_PRECISION::FP16 is the default. DEPTH_PRECISION::INT8 runs the network at a lower precision, reducing GPU memory usage and increasing speed for a small (typically 1-2%) accuracy cost.
INT8 is only available for the NEURAL depth mode; other depth modes always run in FP16. It is always safe to set: the ZED SDK falls back to FP16, and logs it, when the depth mode or the GPU does not support INT8.
Depth Range
Depth range corresponds to the minimum and maximum distance at which the depth of an object can be estimated.
Depth Range by Camera Model
Below are the typical depth ranges and focal lengths for each ZED camera model:
ZED Mini
ZED 2i
ZED X
ZED X Mini
ZED X Nano
Minimum Range
You can adjust the minimum detectable depth by setting depth_minimum_distance in InitParameters. Lowering this value allows the camera to estimate depth for objects closer to the lens, within the hardware’s supported range.
Maximum Range
You can increase the maximum detectable depth by setting depth_maximum_distance in InitParameters. Raising this value allows the camera to estimate depth for objects farther from the lens, up to the hardware’s supported maximum range.
This is useful for applications that require depth information at longer distances.
Depth accuracy decreases with distance, so it’s important to consider the trade-off between range and accuracy. Read more about depth accuracy to understand how it affects your application.
- The maximum depth range can be reduced to clamp values above a certain distance. This is useful to reduce depth jitter at long distances.
- Increasing the maximum range has no impact on memory or FPS.
Depth Stabilization
Depth stabilization is a feature that reduces depth map jitter and enhances accuracy by temporally filtering depth data across multiple frames. It leverages the ZED SDK’s positional tracking to maintain stable depth estimates even when the camera is in motion. The system intelligently distinguishes between static and dynamic regions, ensuring that moving objects are not incorrectly fused, which preserves the integrity of depth information in dynamic scenes.
Depth stabilization is enabled by default. Since it enables positional tracking in the background, you can disable depth stabilization by setting init_parameters.depth_stabilization = 0 to improve computational performance. The value sets the stabilization strength, from 0 (disabled) to 100.
- For fixed cameras, we recommend enabling
PositionalTrackingParameters::set_as_staticwhile using depth stabilization. This allows the depth stabilizer module to know the camera is static so it can disable visual tracking and reduce the computational load. - For applications requiring the Positional Tracking module to be disabled, the depth stabilization parameter must be set to 0; otherwise, the Positional Tracking module is automatically activated in the background.
- Enabling depth stabilization uses temporal tracking to smooth depth over time. However, if the stabilization strength is set too high and objects or the camera move quickly, the system may fail to keep up, causing “ghosting” or motion trails around fast-moving objects. By default, the Depth Stabilization parameter is set to 30.
sl::RuntimeParameters Depth Parameters
For more information on these parameters, see the API documentation page.
Depth Confidence Filtering
Depth estimation can introduce some uncertainty, resulting in points with varying reliability. While a small number of inaccurate points may not impact most applications, scenarios requiring high precision benefit from filtering out less reliable depth data.
To help with this, the ZED SDK provides a confidence map. Each pixel in the confidence map is assigned a value from 0 (high confidence) to 100 (low confidence). Pixels with higher values are less trustworthy and can be excluded or handled differently to improve the overall quality of your depth data.
To filter out unreliable points from the depth map or point cloud, you can either implement your own filtering function using the retrieved confidence data, or simply set the sl::RuntimeParameters::confidence_threshold parameter. When you set this threshold, the ZED SDK automatically removes all points with a confidence value higher than the specified limit, streamlining the process and ensuring only reliable depth data is used.
Two different types of confidence thresholds are available:
confidence_threshold: Filters out depth points with low confidence, primarily removing unreliable measurements around object edges. This helps prevent objects that are close together from appearing “linked” in the depth map.texture_confidence_threshold: Filters out depth points in regions with low image texture (uniform or featureless areas), where depth estimation is less reliable due to insufficient visual information.