Logs Introduction Access Token Access tokens are the secret passwords that gives access to your resources through the APIs. You can create an API token from the Cloud as described in the introduction. Make sure to keep your tokens secret and to not publish them publicly to prevent any security breach. API in use The Cloud API centralizes all your teams, workspaces, devices, applications, logs and telemetries. hub.stereolabs.com/api/v1 List and query logs List logs stored in the specified workspace identified by workspaceId. Multiple parameters are available to customize the output of this endpoint. :workspaceId integer Id of the target workspace. fields string_list optional Log's fields that should be returned by the request. This can be used to reduce amount of data retrieved by only selecting the needed fields. ?fields=timestamp,label,payload Available fields: id, device_id, timestamp, payload, retention, level, label, application_name, deployment_id, reference, reference_list, processed Payload fields: A field can also be taken from the payload with the following notation ?fields=payload.temperature,payload.humidity ids integer_list optional Filter the logs from their Id. ?ids=125,356,542 devices integer_list optional Filter logs based on the devices that emitted them. ?devices=1,5 labels string_list optional Filter logs based on their label. ?labels=detections,environment startend timestamp optional Only target the logs published within the specified the time-range. ?start=1567413071229&end=1567419371229 start and end can be used independently. Timestamps can be provided in the following formats: start=1567419371229 A milliseconds UTC EPOCH UNIX timestamp. start=2019-09-02T11:21:11,229+02:00 An ISO8601 datetime string. (must be url-encoded) levels string_list optional Filter logs based on their level. ?labels=INFO,WARNING,ERROR application_names string_list optional Only targets logs produced by applications matching the listed names (url-encoded). ?application_names=webserver,people counter deployment_ids integer_list optional Only targets logs produced by applications instances matching the listed deployment ids. ?deployment_ids=434445,684650 processed boolean optional Only targets logs that have been marked as read true or not false. ?processed=false sortsort_direction field_liststring_list optional Sort the returned logs by the specified key. ?sort=timestamp&sort_direction=DESC The order can be specified with the sort_direction parameter that can be DESC or ASC whether you are using descending or ascending sorting. If more than one key is given, the next fields will be used when sorting with the previous key reported an equality. ?sort=label,payload.humidity&sort_direction=ASC,DESC filter_opfilter_fieldfilter_value stringfieldvalue optional Filter out logs that doesn't match the specified condition. ?filter_field=payload.temperature&filter_op=gt&filter_value=30 Only return log with a reported temperature over 30° (where temperature is a custom field in the payload) Available filter operations are: gt: is greater than gte: is greater than or equal lt: is lower than lte: is lower than of equal eq: is equal neq: is different contains: is containing the value (string) To avoid type ambiguity when filtering on a payload key, use the filter_value_type parameter and set it to number or string. To use more than one filter, append from _1 to _10 at the end of each filter_* parameter. ?filter_field_2=payload.humidity&filter_op_2=eq&filter_value_2=95 aggagg_fieldagg_step stringfieldtimestamp optional This parameter will change the output format by returning aggregates of logs in time-intervals rather than a log list. ?agg=mean&agg_field=payload.temperature&start=1567413071229&end=1567419371229 Returns the average temperature in a time-range (where payload.temperature is a custom field). Available aggregations are: count: Count the number of logs matching the provided parameters sum: Sum of the values found in the queried logs for the agg_field avg: Average of the values found in the queried logs for the agg_field min: Minimum value found in the queried logs for the agg_field max: Maximum value found in the queried logs for the agg_field If an agg_step is provided, result will be split in multiple time ranges, starting from start and incrementing by agg_step up to the end. An additional agg_identifier can be used to split result in groups based on key's value. ?agg=count&agg_identifier=device_id&start=1567413071229&end=1567419371229&agg_step=36000000 Count the number of logs reported by each device in 10 minutes intervals. per_pagepageafter integerinteger_or_fieldvalue optional Controls the pagination of the returned log list. ?per_page=25 By default, the logs's timestamp is used to sort the returned page, providing the latest logs first. Keyset pagination By using page to select the sorting key, and after to specify the position of the page, pagination will return per_page logs starting right after after value. ?per_page=25&page=timestamp&after=1567413071229 Offset pagination By using page as a number, pagination will return per_page logs starting from the most recent one. ?per_page=25&page=1 limitoffset integerinteger optional Skip some logs (offset) and limits the number of logs returned by the request. ?offset=50&limit=25 logs array List of logs matching the specified parameters. /workspaces/:workspaceId/logs curl -s \ -H "Content-Type:application/json" \ -H "Authorization:Bearer ${access_token}" \ https://hub.stereolabs.com/api/v1/workspaces/:workspaceId/logs \ -G \ -d 'labels=storage' \ -d 'fields=id,device_id,level,timestamp,payload.message' \ -d 'start=1580201472695' \ -d 'filter_field=payload.space_left_percent' \ -d 'filter_op=lt' \ -d 'filter_value=5' \ -d 'filter_value_type=number' HTTP/1.1 200 OK { "logs": [ { "id": "343536", "device_id": "67890", "level": "WARNING", "timestamp": "1580205472695", "payload": { "message": "Storage space is running low" } }, ... ] } Publish log Publish a new log from the specified device. :workspaceId integer Id of the target workspace. :deviceNameOrId integer Id or url-encoded name of the associated device. label string A string representing the type of log sent. This field is later used during data consultation to filter relevant logs. level string The reported log level in the following list: INFO, WARNING, ERROR. payload object The actual log data in a json format. If the payload contains a "message":"" field, this message will be displayed in the interface on the log page. timestamp timestamp optional The time at which the log has been generated. Default value is the timestamp at which the request is sent. Timestamp can be provided in the following formats: start=1567419371229 A milliseconds UTC EPOCH UNIX timestamp start=2019-09-02T11:21:11,229+02:00 An ISO8601 datetime string (must be url-encoded) retention number optional The retention time of this log in days. If not set, the default value of 1 month (30 days) will be used. application_name string optional The name of the application sending the log message. This can be used to identify the application at the origin of the log. deployment_id integer optional The deployment id of the application instance sending the log message. This can be used to identify a specific installation and version of an application. referencereference_to stringstring optional Can be used to associate logs to a parent one. reference and reference_to CANNOT be used at the same time. reference: a unique string used as a root reference for yet-to-publish logs reference_to: the reference string used in a previously-published log Child-logs with a message in their payload will be displayed as a console output in the parent log on the web interface. id integer ID of the created log. /workspaces/:workspaceId/devices/:deviceNameOrId/logs curl -s \ -H "Content-Type:application/json" \ -H "Authorization:Bearer ${access_token}" \ -X POST \ https://hub.stereolabs.com/api/v1/workspaces/:workspaceId/devices/:deviceNameOrId/logs \ -d '{ "timestamp": 1567416071229, "label": "storage", "level": "WARNING", "payload": { "message":"Storage space is running low", "space_left_percent": 4.25 } }' HTTP/1.1 200 OK { "id": "313233" } Delete logs Delete logs matching the parameters. :workspaceId integer Id of the target workspace. ids integer_list optional Filter the logs from their Id. ?ids=125,356,542 devices integer_list optional Filter logs based on the devices that emitted them. ?devices=1,5 labels string_list optional Filter logs based on their label. ?labels=detections,environment levels string_list optional Filter logs based on their level. ?levels=INFO,WARNING,ERROR application_names string_list optional Only targets logs produced by applications matching the listed names (url-encoded). ?application_names=webserver,people counter deployment_ids integer_list optional Only targets logs produced by applications instances matching the listed deployment ids. ?deployment_ids=434445,684650 processed boolean optional Only targets read logs true or unread ones false. ?processed=true startend timestamp optional Only target the logs published within the specified the time-range. ?start=1567413071229&end=1567419371229 start and end can be used independently. Timestamps can be provided in the following formats: start=1567419371229 A milliseconds UTC EPOCH UNIX timestamp. start=2019-09-02T11:21:11,229+02:00 An ISO8601 datetime string. (must be url-encoded) /workspaces/:workspaceId/logs curl -s \ -H "Content-Type:application/json" \ -H "Authorization:Bearer ${access_token}" \ -X DELETE \ https://hub.stereolabs.com/api/v1/workspaces/:workspaceId/logs \ -G \ -d 'labels=environment' \ -d 'levels=ERROR' \ -d 'start=1580201472695' \ -d 'end=1580312563849' HTTP/1.1 200 OK {}