Overview ZED Hub comes with multiple samples that can be deployed as applications on your devices to experience all of the platform features. The code can be written in C++ or Python. Tutorial Description Camera Viewer This sample is a basic example which displays a ZED live view in the ZED Hub Video Panel. It also allows you to continuously record the video. This sample showcases the following ZED Hub features : - Logs which informs you about the application's status - Live Stream which displays the live video from your ZED camera in the Video Panel - Recordings which are listed hour by hour in the Video Panel Object Detection This sample is a complete example that shows you how to perform Object detection in a ZED Hub App. It also shows how to generate: - Logs which inform you about the application's status - Telemetries which store data linked to the detections - Video Events which capture videos when people are detected - A Custom Stream which shows you the live video, with bounding boxes around detected people GPS Tracker This sample is an example that shows you how to send GPS data in a ZED Hub App to display them in the Map page. It also shows how to use it to generate: - Logs which inform you about the application's status - Telemetries which store data linked to the detections