Building a C++ Application on Linux and NVIDIA® Jetson
This section explains how to build an application with the ZED SDK on Linux platforms.
Setting Up a Project #
We will build a simple tutorial application Hello ZED using the ZED SDK and CMake. CMake is a cross-platform project generation tool. It provides an easy way to build project files that can be used in the compiler environment of your choice. For example, a CMake script can produce Visual Studio projects and solution files.
- Download and install the latest ZED SDK.
- Download the ZED Examples sample code available on our GitHub page. You can also browse our GitHub for additional plugins and sample codes.
- Open the Tutorials/Tutorial - Hello ZED folder to find the code we will build. The following files should be in the directory:
- CMakeLists.txt
- main.cpp
- README.md
Building on Linux and NVIDIA® Jetson #
On Linux, compiling an application with the ZED SDK requires a toolchain with GCC (5, 6) and CMake (3.5.0 minimum). To install both, type:
sudo apt-get install build-essential cmake
Now let’s build the Hello ZED tutorial.
- Open your terminal and go to the tutorial folder.
cd path/to/your/project/ZED_Tutorial_1
- Create a build folder.
mkdir build && cd build
- Generate your project with CMake by pointing to the CMakeLists.txt folder (the parent folder).
cmake ..
...
-- Configuring done
-- Generating done
-- Build files have been written to: path/to/your/project/ZED_Tutorial_1/build
- Use the
ls
command to check the content of the build directory:
ls
CMakeCache.txt CMakeFiles cmake_install.cmake Makefile
- Compile the application using the
make
command.
make
- The application is now compiled. To launch it, run this command:
./ZED_Tutorial_1
The application will display your camera serial number in the terminal.
Dynamic/static linking #
On Linux, the ZED SDK is available as static and dynamic libraries. The default is dynamic, reducing the application size but forcing the application user to install all the dependencies.
The static linking will package all the dependencies into the final executable.
To switch between the mode simply enables this option when running the CMake configuration :
cmake -DLINK_SHARED_ZED=OFF ..
Then rebuilt the program :
make
The size will significantly increase but the ease of deployment will be greatly improved!